43 #ifndef ti_drivers_adc_ADCCC26XX__include 44 #define ti_drivers_adc_ADCCC26XX__include 55 #include <ti/devices/DeviceFamily.h> 56 #include DeviceFamily_constructPath(driverlib/aux_adc.h) ADCCC26XX_Trigger_Source triggerSource
Definition: ADCCC26XX.h:157
Definition: ADCCC26XX.h:84
Definition: ADCCC26XX.h:77
ADCCC26XX_Reference_Source refSource
Definition: ADCCC26XX.h:153
ADCCC26XX Object.
Definition: ADCCC26XX.h:165
Definition: ADCCC26XX.h:120
bool returnAdjustedVal
Definition: ADCCC26XX.h:149
bool isProtected
Definition: ADCCC26XX.h:173
Power manager interface for CC26XX/CC13XX.
ADCCC26XX_Sampling_Duration
Amount of time the ADC spends sampling the analogue input.
Definition: ADCCC26XX.h:71
const ADC_FxnTable ADCCC26XX_fxnTable
ADCCC26XX_Trigger_Source
List of sources the ADC can be configured to trigger off of.
Definition: ADCCC26XX.h:130
Definition: ADCCC26XX.h:83
Device-specific pin & GPIO driver for CC26xx family [def].
Analog to Digital Conversion (ADC) Input Driver.
Definition: ADCCC26XX.h:78
Definition: ADCCC26XX.h:81
Definition: ADCCC26XX.h:82
uint8_t adcCompBInput
Definition: ADCCC26XX.h:147
The definition of an ADC function table that contains the required set of functions to control a spec...
Definition: ADC.h:319
Definition: ADCCC26XX.h:73
underlying data structure for type PIN_State
Definition: PIN.h:708
uint8_t adcDIO
Definition: ADCCC26XX.h:145
bool isOpen
Definition: ADCCC26XX.h:171
ADCCC26XX Hardware attributes These fields are used by driverlib APIs and therefore must be populated...
Definition: ADCCC26XX.h:143
Definition: ADCCC26XX.h:76
Definition: ADCCC26XX.h:72
PIN_Handle pinHandle
Definition: ADCCC26XX.h:169
PIN_State pinState
Definition: ADCCC26XX.h:167
Definition: ADCCC26XX.h:79
Definition: ADCCC26XX.h:74
bool inputScalingEnabled
Definition: ADCCC26XX.h:151
ADCCC26XX_Sampling_Duration samplingDuration
Definition: ADCCC26XX.h:155
Definition: ADCCC26XX.h:131
Definition: ADCCC26XX.h:75
Generic PIN & GPIO driver.
Definition: ADCCC26XX.h:80
ADCCC26XX_Reference_Source
Specifies whether the internal reference of the ADC is sourced from the battery voltage or a fixed in...
Definition: ADCCC26XX.h:119
Definition: ADCCC26XX.h:121