Go to the documentation of this file. 37 #ifndef _PROP_MAILBOX_H 38 #define _PROP_MAILBOX_H 44 #define PROP_DONE_OK 0x3400 45 #define PROP_DONE_RXTIMEOUT 0x3401 46 #define PROP_DONE_BREAK 0x3402 47 #define PROP_DONE_ENDED 0x3403 48 #define PROP_DONE_STOPPED 0x3404 49 #define PROP_DONE_ABORT 0x3405 50 #define PROP_DONE_RXERR 0x3406 51 #define PROP_DONE_IDLE 0x3407 52 #define PROP_DONE_BUSY 0x3408 53 #define PROP_DONE_IDLETIMEOUT 0x3409 54 #define PROP_DONE_BUSYTIMEOUT 0x340A 56 #define PROP_ERROR_PAR 0x3800 60 #define PROP_ERROR_RXBUF 0x3801 61 #define PROP_ERROR_RXFULL 0x3802 62 #define PROP_ERROR_NO_SETUP 0x3803 63 #define PROP_ERROR_NO_FS 0x3804 64 #define PROP_ERROR_RXOVF 0x3805 65 #define PROP_ERROR_TXUNF 0x3806
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale