Go to the documentation of this file. 37 #ifndef _BLE_MAILBOX_H 38 #define _BLE_MAILBOX_H 44 #define BLE_DONE_OK 0x1400 45 #define BLE_DONE_RXTIMEOUT 0x1401 46 #define BLE_DONE_NOSYNC 0x1402 47 #define BLE_DONE_RXERR 0x1403 48 #define BLE_DONE_CONNECT 0x1404 49 #define BLE_DONE_MAXNACK 0x1405 50 #define BLE_DONE_ENDED 0x1406 51 #define BLE_DONE_ABORT 0x1407 52 #define BLE_DONE_STOPPED 0x1408 53 #define BLE_DONE_AUX 0x1409 54 #define BLE_DONE_CONNECT_CHSEL0 0x140A 55 #define BLE_DONE_SCAN_RSP 0x140B 56 #define BLE_ERROR_PAR 0x1800 60 #define BLE_ERROR_RXBUF 0x1801 61 #define BLE_ERROR_NO_SETUP 0x1802 62 #define BLE_ERROR_NO_FS 0x1803 63 #define BLE_ERROR_SYNTH_PROG 0x1804 64 #define BLE_ERROR_RXOVF 0x1805 65 #define BLE_ERROR_TXUNF 0x1806 66 #define BLE_ERROR_AUX 0x1807 72 #define BLE_TRIG_REL_SYNC 15
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale