Go to the source code of this file.
|
#define | ANT1 (28) |
|
#define | ANT2 (29) |
|
#define | ANT3 (30) |
|
#define | ANT_ARRAY (27) |
|
#define | AOA_NUM_ANTENNAS 3 |
| Number of antennas in antenna array.
|
|
#define | AOA_PIN(x) (1 << (x&0xff)) |
| Relevant only for RTLS Passive.
|
|
#define | AOA_RES_MAX_CTE_TIME 20 |
| CTE Time at maximum resolution.
|
|
#define | AOA_RES_MAX_SIZE 512 |
| Relevent only for RTLS Passive. More...
|
|
|
uint16_t | AOA_calcNumOfCteSamples (uint8_t cteTime, uint8_t cteScanOvs, uint8_t cteOffset) |
| This function calculate the number of IQ samples based on the cte parameters from the CTEInfo header and our patch params. More...
|
|
void | AOA_cteCapEnable (uint8_t cteTime, uint8_t cteScanOvs, uint8_t cteOffset) |
| This function enables the CTE capture in the rf core. More...
|
|
uint8_t | AOA_getActiveAnt (void) |
| Returns active antenna id. More...
|
|
AoA_IQSampleState_t | AOA_getSampleState (void) |
| Returns active antenna id. More...
|
|
void | AOA_init (uint8_t startAntenna) |
| Initialize AoA for the defined role. More...
|
|
void | AOA_postProcess (int8_t rssi, uint8_t channel, AoA_IQSample_t *samplesBuff) |
| This function will update the final result report with rssi and channel For RTLS Passive it will also send a command to enable RF RAM so we can read the samples that we captured (if any) More...
|
|