174 #ifndef ti_drivers_watchdog_WatchdogCC26XX__include 175 #define ti_drivers_watchdog_WatchdogCC26XX__include 180 #include <ti/drivers/dpl/HwiP.h> void(* Watchdog_Callback)(uintptr_t handle)
Watchdog callback pointer.
Definition: Watchdog.h:289
unsigned int baseAddr
Definition: WatchdogCC26XX.h:221
Watchdog driver interface.
Watchdog hardware attributes for CC26XX.
Definition: WatchdogCC26XX.h:220
Watchdog_Callback callbackFxn
Definition: WatchdogCC26XX.h:232
bool isOpen
Definition: WatchdogCC26XX.h:231
Watchdog_DebugMode
Watchdog debug stall settings.
Definition: Watchdog.h:264
Watchdog Object for CC26XX.
Definition: WatchdogCC26XX.h:230
unsigned long reloadValue
Definition: WatchdogCC26XX.h:222
Watchdog_ResetMode resetMode
Definition: WatchdogCC26XX.h:234
const Watchdog_FxnTable WatchdogCC26XX_fxnTable
Watchdog function table for CC26XX.
Watchdog_DebugMode debugStallMode
Definition: WatchdogCC26XX.h:236
The definition of a Watchdog function table that contains the required set of functions to control a ...
Definition: Watchdog.h:362
Watchdog_ResetMode
Watchdog reset mode settings.
Definition: Watchdog.h:276
HwiP_Struct hwi
Definition: WatchdogCC26XX.h:239