341 #ifndef ti_drivers_uart_UARTCC26X2__include 342 #define ti_drivers_uart_UARTCC26X2__include 347 #include <ti/drivers/dpl/ClockP.h> 348 #include <ti/drivers/dpl/HwiP.h> 349 #include <ti/drivers/dpl/SemaphoreP.h> 350 #include <ti/drivers/dpl/SwiP.h> 363 #define UARTCC26X2_FLOWCTRL_NONE 0 368 #define UARTCC26X2_FLOWCTRL_HARDWARE 1 401 #define UARTCC26X2_CMD_RETURN_PARTIAL_ENABLE (UART_CMD_RESERVED + 0) 410 #define UARTCC26X2_CMD_RETURN_PARTIAL_DISABLE (UART_CMD_RESERVED + 1) 418 #define UARTCC26X2_CMD_RX_FIFO_FLUSH (UART_CMD_RESERVED + 2) 424 #define UARTCC26X2_FIFO_SIZE 32 599 bool ctrlRxEnabled:1;
UART_STOP
UART stop bit settings.
Definition: UART.h:523
size_t readSize
Definition: UARTCC26X2.h:619
UARTCC26X2 Object.
Definition: UARTCC26X2.h:573
Definition: UARTCC26X2.h:440
UARTCC26X2_FifoThreshold rxIntFifoThr
Definition: UARTCC26X2.h:563
UARTCC26X2_ErrorCallback errorFxn
Definition: UARTCC26X2.h:565
The definition of a UART function table that contains the required set of functions to control a spec...
Definition: UART.h:635
size_t readCount
Definition: UARTCC26X2.h:620
Definition: UARTCC26X2.h:439
size_t ringBufSize
Definition: UARTCC26X2.h:551
struct UARTCC26X2_Object * UARTCC26X2_Handle
UART_PAR
UART parity type settings.
Definition: UART.h:533
uint8_t rxPin
Definition: UARTCC26X2.h:553
UART_Mode
UART mode settings.
Definition: UART.h:428
unsigned int powerMgrId
Definition: UARTCC26X2.h:640
HwiP_Struct hwi
Definition: UARTCC26X2.h:606
UART_DataMode
UART data mode settings.
Definition: UART.h:483
UARTCC26X2 Hardware attributes.
Definition: UARTCC26X2.h:533
UART_ReturnMode
UART return mode settings.
Definition: UART.h:461
UART_LEN dataLength
Definition: UARTCC26X2.h:611
unsigned char * ringBufPtr
Definition: UARTCC26X2.h:549
UART_Echo
UART echo settings.
Definition: UART.h:501
PIN_Handle hPin
Definition: UARTCC26X2.h:636
uint32_t status
Definition: UARTCC26X2.h:614
void(* UARTCC26X2_ErrorCallback)(UART_Handle handle, uint32_t error)
The definition of an optional callback function used by the UART driver to notify the application whe...
Definition: UARTCC26X2.h:456
UART Global configuration.
Definition: UART.h:678
uint8_t rtsPin
Definition: UARTCC26X2.h:559
SemaphoreP_Struct writeSem
Definition: UARTCC26X2.h:630
Definition: UARTCC26X2.h:438
size_t writeCount
Definition: UARTCC26X2.h:629
UART_STOP stopBits
Definition: UARTCC26X2.h:612
Device-specific pin & GPIO driver for CC26xx family [def].
unsigned int readTimeout
Definition: UARTCC26X2.h:622
RingBuf_Object ringBuffer
Definition: UARTCC26X2.h:617
UART_Callback writeCallback
Definition: UARTCC26X2.h:632
uint8_t intPriority
Definition: UARTCC26X2.h:539
Definition: UARTCC26X2.h:442
UART_Callback readCallback
Definition: UARTCC26X2.h:623
ClockP_Struct timeoutClk
Definition: UARTCC26X2.h:609
Definition: UARTCC26X2.h:441
Definition: UARTCC26X2.h:443
Power notify object structure.
Definition: Power.h:443
const unsigned char * writeBuf
Definition: UARTCC26X2.h:627
Universal Asynchronous Receiver-Transmitter (UART) Driver.
uint32_t baseAddr
Definition: UARTCC26X2.h:535
int intNum
Definition: UARTCC26X2.h:537
uint32_t swiPriority
Swi priority. The higher the number, the higher the priority. The minimum priority is 0 and the maxim...
Definition: UARTCC26X2.h:545
underlying data structure for type PIN_State
Definition: PIN.h:708
UARTCC26X2_FifoThreshold
UART TX/RX interrupt FIFO threshold select.
Definition: UARTCC26X2.h:437
uint32_t flowControl
Definition: UARTCC26X2.h:547
const UART_FxnTable UARTCC26X2_fxnTable
PIN_State pinState
Definition: UARTCC26X2.h:635
uint32_t baudRate
Definition: UARTCC26X2.h:610
UART_LEN
UART data length settings.
Definition: UART.h:511
SwiP_Struct writeSwi
Definition: UARTCC26X2.h:608
unsigned char * readBuf
Definition: UARTCC26X2.h:618
uint8_t txPin
Definition: UARTCC26X2.h:555
UARTCC26X2_FifoThreshold txIntFifoThr
Definition: UARTCC26X2.h:561
unsigned int writeTimeout
Definition: UARTCC26X2.h:631
size_t writeSize
Definition: UARTCC26X2.h:628
uint8_t ctsPin
Definition: UARTCC26X2.h:557
SemaphoreP_Struct readSem
Definition: UARTCC26X2.h:621
UART_PAR parityType
Definition: UARTCC26X2.h:613
bool readRetPartial
Definition: UARTCC26X2.h:624
void(* UART_Callback)(UART_Handle handle, void *buf, size_t count)
The definition of a callback function used by the UART driver when used in UART_MODE_CALLBACK The cal...
Definition: UART.h:421
Power_NotifyObj postNotify
Definition: UARTCC26X2.h:639
SwiP_Struct readSwi
Definition: UARTCC26X2.h:607