45 #ifndef ti_drivers_timer_TimerCC26XX__include 46 #define ti_drivers_timer_TimerCC26XX__include 52 #include <ti/drivers/dpl/SemaphoreP.h> TimerCC26XX_Object.
Definition: TimerCC26XX.h:118
GPTimer driver implementation for CC26XX/CC13XX.
Definition: TimerCC26XX.h:72
TimerCC26XX_SubTimer subTimer
Definition: TimerCC26XX.h:109
bool isRunning
Definition: TimerCC26XX.h:125
const Timer_FxnTable TimerCC26XX_fxnTable
Timer_CallBackFxn callBack
Definition: TimerCC26XX.h:122
TimerCC26XX_SubTimer
Definition: TimerCC26XX.h:71
Timer_Mode mode
Definition: TimerCC26XX.h:123
SemaphoreP_Handle semHandle
Definition: TimerCC26XX.h:121
bool isOpen
Definition: TimerCC26XX.h:126
TimerCC26XX Hardware Attributes.
Definition: TimerCC26XX.h:104
SemaphoreP_Struct semStruct
Definition: TimerCC26XX.h:120
Definition: TimerCC26XX.h:73
Definition: TimerCC26XX.h:74
GPTimer Global configuration.
Definition: GPTimerCC26XX.h:407
Timer_Mode
Timer mode settings.
Definition: Timer.h:239
The definition of a timer function table that contains the required set of functions to control a spe...
Definition: Timer.h:379
uint32_t period
Definition: TimerCC26XX.h:124
uint8_t gpTimerUnit
Definition: TimerCC26XX.h:106
void(* Timer_CallBackFxn)(Timer_Handle handle)
Timer callback function.
Definition: Timer.h:299
GPTimerCC26XX_Handle gptHandle
Definition: TimerCC26XX.h:119