87 #ifndef ti_drivers_ecdsa_ECDSACC26X2__include 88 #define ti_drivers_ecdsa_ECDSACC26X2__include 100 #include <ti/drivers/dpl/HwiP.h> 101 #include <ti/drivers/dpl/SwiP.h> 102 #include <ti/drivers/dpl/SemaphoreP.h> 109 #define ECDSACC26X2_STATUS_FSM_RUN_PKA_OP ECDSA_STATUS_RESERVED - 0 111 #define ECDSACC26X2_STATUS_FSM_RUN_FSM ECDSA_STATUS_RESERVED - 1 TI Driver for Elliptic Curve Digital Signature Algorithm.
ECDSA_ReturnBehavior
The way in which ECDSA function calls return after performing an encryption + authentication or decry...
Definition: ECDSA.h:505
Definition: ECDSACC26X2.h:144
uint8_t trngIntPriority
Definition: ECDSACC26X2.h:194
Definition: ECDSACC26X2.h:140
The CryptoKey type is an opaque representation of a cryptographic key.
TRNGCC26XX Hardware Attributes.
Definition: TRNGCC26XX.h:119
uint32_t resultAddress
Definition: ECDSACC26X2.h:218
Definition: ECDSACC26X2.h:149
Definition: ECDSACC26X2.h:153
void(* ECDSA_CallbackFxn)(ECDSA_Handle handle, int_fast16_t returnStatus, ECDSA_Operation operation, ECDSA_OperationType operationType)
The definition of a callback function used by the ECDSA driver when used in ECDSA_RETURN_BEHAVIOR_CAL...
Definition: ECDSA.h:608
uint32_t * scratchNumber2
Definition: ECDSACC26X2.h:220
ECDSACC26X2_FsmState
ECDSACC26X2 Sign and Verify states.
Definition: ECDSACC26X2.h:122
TRNG Global configuration.
Definition: TRNG.h:273
uint32_t semaphoreTimeout
Definition: ECDSACC26X2.h:217
bool operationInProgress
Definition: ECDSACC26X2.h:208
CryptoKey datastructure.
Definition: CryptoKey.h:209
Definition: ECDSACC26X2.h:150
Definition: ECDSACC26X2.h:137
Definition: ECDSACC26X2.h:146
ECDSA Global configuration.
Definition: ECDSA.h:470
Definition: ECDSACC26X2.h:152
ECDSA_CallbackFxn callbackFxn
Definition: ECDSACC26X2.h:213
TRNG driver implementation for the CC26XX family.
TRNGCC26XX_Object trngObject
Definition: ECDSACC26X2.h:204
Definition: ECDSACC26X2.h:157
Definition: ECDSACC26X2.h:143
uint32_t * scratchNumber1
Definition: ECDSACC26X2.h:219
Definition: ECDSACC26X2.h:134
ECDSACC26X2 Object.
Definition: ECDSACC26X2.h:202
Definition: ECDSACC26X2.h:128
Definition: ECDSACC26X2.h:125
Definition: ECDSACC26X2.h:132
bool isOpen
Definition: ECDSACC26X2.h:207
ECDSA_OperationType
Enum for the operation types supported by the driver.
Definition: ECDSA.h:584
int_fast16_t(* ECDSACC26X2_stateMachineFxn)(ECDSA_Handle handle)
ECDSACC26X2 state machine function prototype.
Definition: ECDSACC26X2.h:172
Definition: ECDSACC26X2.h:129
Definition: ECDSACC26X2.h:123
Definition: ECDSACC26X2.h:141
Definition: ECDSACC26X2.h:136
Definition: ECDSACC26X2.h:130
ECDSACC26X2_FsmState fsmState
Definition: ECDSACC26X2.h:216
Union containing pointers to all supported operation structs.
Definition: ECDSA.h:576
uint8_t intPriority
PKA Peripheral's interrupt priority.
Definition: ECDSACC26X2.h:193
Definition: ECDSACC26X2.h:160
ECDSA_Operation operation
Definition: ECDSACC26X2.h:211
Definition: ECDSACC26X2.h:131
ECDSACC26X2 Hardware Attributes.
Definition: ECDSACC26X2.h:180
ECDSACC26X2_stateMachineFxn fsmFxn
Definition: ECDSACC26X2.h:214
Definition: ECDSACC26X2.h:159
Definition: ECDSACC26X2.h:148
Definition: ECDSACC26X2.h:156
Definition: ECDSACC26X2.h:154
Definition: ECDSACC26X2.h:147
Definition: ECDSACC26X2.h:142
TRNG_Handle trngHandle
Definition: ECDSACC26X2.h:206
Definition: ECDSACC26X2.h:145
Definition: ECDSACC26X2.h:133
Definition: ECDSACC26X2.h:158
Definition: ECDSACC26X2.h:151
bool operationCanceled
Definition: ECDSACC26X2.h:209
Definition: ECDSACC26X2.h:155
Definition: ECDSACC26X2.h:135
Definition: ECDSACC26X2.h:138
ECDSA_ReturnBehavior returnBehavior
Definition: ECDSACC26X2.h:215
int_fast16_t operationStatus
Definition: ECDSACC26X2.h:210
Definition: ECDSACC26X2.h:127
ECDSA_OperationType operationType
Definition: ECDSACC26X2.h:212
TRNGCC26XX_HWAttrs trngHwAttrs
Definition: ECDSACC26X2.h:205
TRNG_Config trngConfig
Definition: ECDSACC26X2.h:203
Definition: ECDSACC26X2.h:126
CryptoKey pmsnKey
Definition: ECDSACC26X2.h:221