171 #define SCAN_RSSI_MAX 127 172 #define SCAN_RSSI_MIN -128 179 #define SCAN_FLT_RSSI_ALL SCAN_RSSI_MIN 180 #define SCAN_FLT_RSSI_NONE SCAN_RSSI_MAX 187 #define SCAN_PARAM_DFLT_INTERVAL 800 189 #define SCAN_PARAM_DFLT_WINDOW 800 191 #define SCAN_PARAM_DFLT_TYPE SCAN_TYPE_PASSIVE 193 #define SCAN_PARAM_DFLT_RPT_FIELDS (SCAN_ADVRPT_FLD_EVENTTYPE|\ 195 SCAN_ADVRPT_FLD_ADDRTYPE |\ 196 SCAN_ADVRPT_FLD_ADDRESS |\ 197 SCAN_ADVRPT_FLD_ADVSID |\ 198 SCAN_ADVRPT_FLD_RSSI) 199 #define SCAN_PARAM_DFLT_PHYS SCAN_PRIM_PHY_1M 201 #define SCAN_PARAM_DFLT_FLT_POLICY SCAN_FLT_POLICY_ALL 203 #define SCAN_PARAM_DFLT_FLT_PDU SCAN_FLT_PDU_COMPLETE_ONLY 205 #define SCAN_PARAM_DFLT_FLT_RSSI SCAN_FLT_RSSI_ALL 207 #define SCAN_PARAM_DFLT_FLT_DISC SCAN_FLT_DISC_DISABLE 209 #define SCAN_PARAM_DFLT_FLT_DUP SCAN_FLT_DUP_ENABLE 211 #define SCAN_PARAM_DFLT_NUM_ADV_RPT 0 544 uint16_t interval, uint16_t window);
562 uint16_t* pInterval, uint16_t* pWindow);
590 status_t
GapScan_getParam(GapScan_ParamId_t paramId,
void* pValue, uint8_t *pLen);
625 uint8_t maxNumReport);
Definition: gap_scanner.h:428
address field
Definition: gap_scanner.h:149
GAP_Addr_Types_t
Address types used for identifying peer address type.
Definition: gap.h:577
status_t GapScan_discardAdvReportList(void)
Definition: gap_scanner.h:320
Limited discoverable mode.
Definition: gap_scanner.h:450
txPower field
Definition: gap_scanner.h:153
This API allows the software components in the Z-Stack to be written independently of the specifics o...
No PHY is used.
Definition: gap_scanner.h:404
Definition: gap_scanner.h:282
General discoverable mode.
Definition: gap_scanner.h:449
GapScan_FilterDiscMode_t
Choices for GAP Scanner Discoverable Mode Filter.
Definition: gap_scanner.h:447
Truncated.
Definition: gap_scanner.h:106
Scan Response only. Mutually exclusive with SCAN_FLT_PDU_ADV_ONLY.
Definition: gap_scanner.h:134
int8_t txPower
-127 dBm <= TX power <= 126 dBm
Definition: gap_scanner.h:487
Directed only. Mutually exclusive with SCAN_FLT_PDU_UNDIRECTED_ONLY.
Definition: gap_scanner.h:130
Disable discoverable mode filter.
Definition: gap_scanner.h:452
GapScan_EndReason_t
Reason for GapScan_Evt_End_t.
Definition: gap_scanner.h:162
Scannable.
Definition: gap_scanner.h:94
status_t GapScan_enable(uint16_t period, uint16_t duration, uint8_t maxNumReport)
Definition: gap_scanner.h:366
GapScan_ScannedPhy_t
Scanned PHY.
Definition: gap_scanner.h:402
GapScan_ScannedPhy_t secPhy
PHY of the secondary advertising channel.
Definition: gap_scanner.h:483
status_t GapScan_getAdvReport(uint8_t rptIdx, GapScan_Evt_AdvRpt_t *pAdvRpt)
status_t GapScan_registerCb(pfnGapCB_t cb, uintptr_t arg)
uint8_t * pData
Pointer to advertising or scan response data.
Definition: gap_scanner.h:499
GapScan_AdvRptField_t
Fields of Adv Report.
Definition: gap_scanner.h:146
GapScan_ParamId_t
Definition: gap_scanner.h:230
Undirected only. Mutually exclusive with SCAN_FLT_PDU_DIRECTIED_ONLY.
Definition: gap_scanner.h:128
Definition: gap_scanner.h:435
Non-discoverable mode.
Definition: gap_scanner.h:448
dataLen field
Definition: gap_scanner.h:158
Directed.
Definition: gap_scanner.h:96
Truncated only. Mutually exclusive with SCAN_FLT_PDU_COMPLETE_ONLY.
Definition: gap_scanner.h:140
Legacy.
Definition: gap_scanner.h:100
GapScan_ScanType_t
GAP Scanner Scan Type.
Definition: gap_scanner.h:411
void GapScan_setEventMask(GapScan_EventMask_t eventMask)
Scanned on the 2M PHY.
Definition: gap_scanner.h:406
Non-scannable only. Mutually exclusive with SCAN_FLT_PDU_SCANNABLE_ONLY.
Definition: gap_scanner.h:124
uint8_t reason
End reason - GapScan_EndReason_t.
Definition: gap_scanner.h:465
Definition: gap_scanner.h:458
Extended only. Mutually exclusive with SCAN_FLT_PDU_LEGACY_ONLY.
Definition: gap_scanner.h:136
GapScan_FilterPolicy_t
GAP Scanner Filter Policy.
Definition: gap_scanner.h:417
GapScan_AdvRptTypeNStatus_t
Advertising report event types.
Definition: gap_scanner.h:90
uint8_t advSid
SID (0x00-0x0f) of the advertising PDU. 0xFF means no ADI field in the PDU.
Definition: gap_scanner.h:485
Definition: gap_scanner.h:383
status_t GapScan_setPhyParams(uint8_t primPhys, GapScan_ScanType_t type, uint16_t interval, uint16_t window)
status_t GapScan_disable(void)
addrType field
Definition: gap_scanner.h:148
Scanned on the 1M PHY.
Definition: gap_scanner.h:405
void(* pfnGapCB_t)(uint32_t event, void *pBuf, uintptr_t arg)
Definition: gap.h:1188
status_t GapScan_setParam(GapScan_ParamId_t paramId, void *pValue)
Complete.
Definition: gap_scanner.h:102
Definition: gap_scanner.h:348
More Data To Come.
Definition: gap_scanner.h:104
Scanned on the Coded PHY.
Definition: gap_scanner.h:407
advSid field
Definition: gap_scanner.h:152
status_t GapScan_getParam(GapScan_ParamId_t paramId, void *pValue, uint8_t *pLen)
GapScan_ScannedPhy_t primPhy
PHY of the primary advertising channel.
Definition: gap_scanner.h:481
Scan on the 1M PHY.
Definition: gap_scanner.h:113
Scanning ended by user request.
Definition: gap_scanner.h:163
Scan on the Coded PHY.
Definition: gap_scanner.h:114
General or Limited discoverable mode.
Definition: gap_scanner.h:451
Scannable only. Mutually exclusive with SCAN_FLT_PDU_NONSCANNABLE_ONLY.
Definition: gap_scanner.h:126
Event for advertising report.
Definition: gap_scanner.h:470
status_t GapScan_getPhyParams(uint8_t primPhy, GapScan_ScanType_t *pType, uint16_t *pInterval, uint16_t *pWindow)
prdAdvInterval field
Definition: gap_scanner.h:157
Type definitions and macros for BLE stack.
eventType field
Definition: gap_scanner.h:147
Scan for scannable advertisements.
Definition: gap_scanner.h:413
GAP_Addr_Types_t directAddrType
Type of TargetA address in the directed advertising PDU.
Definition: gap_scanner.h:491
GapScan_FilterDuplicate_t
Choices for GAP Scanner Duplicate Filter.
Definition: gap_scanner.h:456
Definition: gap_scanner.h:422
Definition: gap_scanner.h:247
Event for scanning end.
Definition: gap_scanner.h:464
Connectable only. Mutually exclusive with SCAN_FLT_PDU_NONCONNECTABLE_ONLY.
Definition: gap_scanner.h:122
uint16_t periodicAdvInt
Periodic advertising interval. 0 means no periodic advertising.
Definition: gap_scanner.h:495
primPhy field
Definition: gap_scanner.h:150
Definition: gap_scanner.h:265
uint32_t GapScan_EventMask_t
Event Mask.
Definition: gap_scanner.h:503
Legacy only. Mutually exclusive with SCAN_FLT_PDU_EXTENDED_ONLY.
Definition: gap_scanner.h:138
Reserved for Future Use.
Definition: gap_scanner.h:108
Duplicate filtering enabled, reset for each scan period.
Definition: gap_scanner.h:460
#define B_ADDR_LEN
Default Public and Random Address Length.
Definition: bcomdef.h:108
Complete only. Mutually exclusive with SCAN_FLT_PDU_TRUNCATED_ONLY.
Definition: gap_scanner.h:142
GapScan_PrimPhy_t
GAP Scanner Primary PHY.
Definition: gap_scanner.h:112
uint8_t evtType
Definition: gap_scanner.h:475
Advertisement only. Mutually exclusive with SCAN_FLT_PDU_SCANRSP_ONLY.
Definition: gap_scanner.h:132
GapScan_FilterPduType_t
PDU Types for PDU Type Filter.
Definition: gap_scanner.h:118
secPhy field
Definition: gap_scanner.h:151
RSSI field.
Definition: gap_scanner.h:154
dirAddress field
Definition: gap_scanner.h:156
uint16_t dataLen
Length of the data.
Definition: gap_scanner.h:497
int8_t rssi
-127 dBm <= RSSI <= 20 dBm
Definition: gap_scanner.h:489
Definition: gap_scanner.h:443
Non-connectable only. Mutually exclusive with SCAN_FLT_PDU_CONNECTABLE_ONLY.
Definition: gap_scanner.h:120
Connectable.
Definition: gap_scanner.h:92
dirAddrType field
Definition: gap_scanner.h:155
Duplicate filtering disabled.
Definition: gap_scanner.h:457
Scan Response.
Definition: gap_scanner.h:98
Scanning ended by duration expiration.
Definition: gap_scanner.h:164
GAP_Addr_Types_t addrType
Public, random, public ID, random ID, or anonymous.
Definition: gap_scanner.h:477
Definition: gap_scanner.h:334
uint8_t numReport
Number of recorded advertising reports.
Definition: gap_scanner.h:466
Scan for non-scannable advertisements.
Definition: gap_scanner.h:412