22 #ifndef GAP_ADVERTISER_H 23 #define GAP_ADVERTISER_H 52 #define GAPADV_PARAMS_LEGACY_SCANN_CONN { \ 54 .eventProps = GAP_ADV_PROP_CONNECTABLE | GAP_ADV_PROP_SCANNABLE | \ 55 GAP_ADV_PROP_LEGACY, \ 58 .primChanMap = GAP_ADV_CHAN_ALL, \ 59 .peerAddrType = PEER_ADDRTYPE_PUBLIC_OR_PUBLIC_ID, \ 60 .peerAddr = { 0xaa, 0xaa, 0xaa, 0xaa, 0xaa, 0xaa }, \ 61 .filterPolicy = GAP_ADV_WL_POLICY_ANY_REQ, \ 62 .txPower = GAP_ADV_TX_POWER_NO_PREFERENCE, \ 63 .primPhy = GAP_ADV_PRIM_PHY_1_MBPS, \ 64 .secPhy = GAP_ADV_SEC_PHY_1_MBPS, \ 69 #define GAPADV_PARAMS_AE_LONG_RANGE_CONN { \ 70 .eventProps = GAP_ADV_PROP_CONNECTABLE, \ 73 .primChanMap = GAP_ADV_CHAN_ALL, \ 74 .peerAddrType = PEER_ADDRTYPE_PUBLIC_OR_PUBLIC_ID, \ 75 .peerAddr = { 0xaa, 0xaa, 0xaa, 0xaa, 0xaa, 0xaa }, \ 76 .filterPolicy = GAP_ADV_WL_POLICY_ANY_REQ, \ 77 .txPower = GAP_ADV_TX_POWER_NO_PREFERENCE, \ 78 .primPhy = GAP_ADV_PRIM_PHY_CODED_S2, \ 79 .secPhy = GAP_ADV_SEC_PHY_CODED_S2, \ 288 #define GAP_ADV_INVALID_HANDLE 0xFF 379 #define GAP_ADV_TX_POWER_NO_PREFERENCE 127 444 GAP_ADV_EVT_MASK_RESERVED = BV(15)
568 GapAdv_freeBufferOptions_t freeOptions);
605 GapAdv_enableOptions_t enableOptions,
606 uint16 durationOrMaxEvents);
686 void *pValue, uint8_t *pLen);
706 uint16 *pLen, uint8 **ppBuf);
767 GapAdv_freeBufferOptions_t freeOptions);
814 uint16
len, uint8 *pBuf);
Omit advertiser's address from PDU's.
Definition: gap_advertiser.h:299
uint32_t primIntMax
GAP_ADV_PARAM_PRIMARY_INTERVAL_MAX
Definition: gap_advertiser.h:470
This API allows the software components in the Z-Stack to be written independently of the specifics o...
All Channels.
Definition: gap_advertiser.h:349
GAP_Peer_Addr_Types_t
Address types used for specifying peer address type.
Definition: gap.h:591
coded-s2
Definition: gap_advertiser.h:386
Channels 37 & 39.
Definition: gap_advertiser.h:345
bStatus_t GapAdv_setParam(uint8 handle, GapAdv_ParamId_t paramID, void *pValue)
bStatus_t GapAdv_getParam(uint8 handle, GapAdv_ParamId_t paramID, void *pValue, uint8_t *pLen)
Definition: gap_advertiser.h:275
uint32_t primIntMin
GAP_ADV_PARAM_PRIMARY_INTERVAL_MIN
Definition: gap_advertiser.h:469
bStatus_t GapAdv_prepareLoadByHandle(uint8 handle, GapAdv_freeBufferOptions_t freeOptions)
GapAdv_freeBufferOptions_t
Possible free options for Gap Advertiser API's.
Definition: gap_advertiser.h:312
Definition: gap_advertiser.h:434
1 mbps
Definition: gap_advertiser.h:384
Definition: gap_advertiser.h:207
bStatus_t GapAdv_loadByHandle(uint8 handle, GapAdv_dataTypes_t dataType, uint16 len, uint8 *pBuf)
Definition: gap_advertiser.h:300
Directed advertising.
Definition: gap_advertiser.h:296
bStatus_t GapAdv_abortLoad(void)
Definition: gap_advertiser.h:422
bStatus_t GapAdv_enable(uint8 handle, GapAdv_enableOptions_t enableOptions, uint16 durationOrMaxEvents)
Data type returned with GAP_EVT_ADV_DATA_TRUNCATED event.
Definition: gap_advertiser.h:502
int8 rssi
RSSI of the scan req.
Definition: gap_advertiser.h:498
Scannable advertising.
Definition: gap_advertiser.h:295
uint16_t eventProps
GAP_ADV_PARAM_PROPS
Definition: gap_advertiser.h:468
Free the scan response data.
Definition: gap_advertiser.h:316
uint8 channel
Channel when the scan req was received.
Definition: gap_advertiser.h:497
GapAdv_enableOptions_t
Enable options for GapAdv_enable.
Definition: gap_advertiser.h:320
Definition: gap_advertiser.h:410
GapAdv_ParamId_t
Definition: gap_advertiser.h:143
Definition: gap_advertiser.h:361
1 mbps
Definition: gap_advertiser.h:392
uint8 handle
Advertising handle.
Definition: gap_advertiser.h:485
Don't free anything.
Definition: gap_advertiser.h:314
Definition: gap_advertiser.h:261
Channels 38 & 39.
Definition: gap_advertiser.h:347
bStatus_t GapAdv_disable(uint8 handle)
Disable an active advertising set.
void(* pfnGapCB_t)(uint32_t event, void *pBuf, uintptr_t arg)
Definition: gap.h:1188
uint8 handle
Advertising handle.
Definition: gap_advertiser.h:504
Definition: gap_advertiser.h:216
GapAdv_secondaryPHY_t secPhy
GAP_ADV_PARAM_SECONDARY_PHY
Definition: gap_advertiser.h:477
2 mbps
Definition: gap_advertiser.h:393
Scan response data.
Definition: gap_advertiser.h:308
bStatus_t GapAdv_setEventMask(uint8 handle, GapAdv_eventMaskFlags_t mask)
GapAdv_secondaryPHY_t
Gap Advertiser Options for advertising on the secondary PHY.
Definition: gap_advertiser.h:390
bStatus_t GapAdv_create(pfnGapCB_t *cb, GapAdv_params_t *advParam, uint8 *advHandle)
Definition: gap_advertiser.h:430
Definition: gap_advertiser.h:237
GapAdv_advChannels_t
GAP Advertiser Defines for Advertiser Channels.
Definition: gap_advertiser.h:338
Definition: gap_advertiser.h:177
Channels 37 & 38.
Definition: gap_advertiser.h:343
GAP_Peer_Addr_Types_t peerAddrType
GAP_ADV_PARAM_PEER_ADDRESS_TYPE
Definition: gap_advertiser.h:472
GapAdv_eventMaskFlags_t
Definition: gap_advertiser.h:405
Advertising data.
Definition: gap_advertiser.h:307
GapAdv_primaryPHY_t
Gap Advertiser Options for advertising on the primary PHY.
Definition: gap_advertiser.h:382
Definition: gap_advertiser.h:334
Type definitions and macros for BLE stack.
Channel 37.
Definition: gap_advertiser.h:340
Definition: gap_advertiser.h:163
Connectable advertising.
Definition: gap_advertiser.h:294
Free the advertising data.
Definition: gap_advertiser.h:315
Definition: gap_advertiser.h:330
bStatus_t GapAdv_getBuffer(uint8 handle, GapAdv_dataTypes_t dataType, uint16 *pLen, uint8 **ppBuf)
coded-s2
Definition: gap_advertiser.h:395
Definition: gap_advertiser.h:249
Definition: gap_advertiser.h:371
Definition: gap_advertiser.h:418
uint16 connHandle
Connection handle that ended advertising.
Definition: gap_advertiser.h:487
Definition: gap_advertiser.h:414
coded-s8
Definition: gap_advertiser.h:394
GapAdv_filterPolicy_t filterPolicy
GAP_ADV_PARAM_FILTER_POLICY
Definition: gap_advertiser.h:474
GapAdv_advChannels_t primChanMap
GAP_ADV_PARAM_PRIMARY_CHANNEL_MAP
Definition: gap_advertiser.h:471
Use legacy advertising PDU's.
Definition: gap_advertiser.h:298
GapAdv_dataTypes_t
Gap Advertising Data Types.
Definition: gap_advertiser.h:305
Definition: gap_advertiser.h:326
uint8 scanAddrType
Address type of scanning device.
Definition: gap_advertiser.h:495
uint16 advDataLen
Definition: gap_advertiser.h:509
int8_t txPower
NOT CURRENTLY IMPLEMENTED.
Definition: gap_advertiser.h:475
Data type returned with GAP_EVT_ADV_SET_TERMINATED event.
Definition: gap_advertiser.h:483
#define B_ADDR_LEN
Default Public and Random Address Length.
Definition: bcomdef.h:108
Definition: gap_advertiser.h:152
Definition: gap_advertiser.h:466
Definition: gap_advertiser.h:426
High Duty Cycle Directed Advertising.
Definition: gap_advertiser.h:297
Definition: gap_advertiser.h:366
Status_t bStatus_t
BLE Generic Status return.
Definition: bcomdef.h:238
Definition: gap_advertiser.h:375
Definition: gap_advertiser.h:198
GapAdv_filterPolicy_t
GAP Advertiser White List Policy.
Definition: gap_advertiser.h:355
bStatus_t GapAdv_prepareLoadByBuffer(uint8 *pBuf, bool freeOldData)
bStatus_t GapAdv_loadByBuffer(uint16 len, uint8 *pBuf)
Channel 39.
Definition: gap_advertiser.h:342
bStatus_t GapAdv_destroy(uint8 handle, GapAdv_freeBufferOptions_t freeOptions)
uint8 handle
Advertising handle.
Definition: gap_advertiser.h:494
GapAdv_eventProps_t
GAP Advertising Event Param Properties.
Definition: gap_advertiser.h:292
coded-s8
Definition: gap_advertiser.h:385
Data type returned with GAP_EVT_SCAN_REQ_RECEIVED event.
Definition: gap_advertiser.h:492
Channel 38.
Definition: gap_advertiser.h:341
GapAdv_primaryPHY_t primPhy
GAP_ADV_PARAM_PRIMARY_PHY
Definition: gap_advertiser.h:476
uint8_t sid
GAP_ADV_PARAM_SID
Definition: gap_advertiser.h:478
uint8 status
TODO.
Definition: gap_advertiser.h:486
uint8 numCompAdvEvts
Number of completed advertising events.
Definition: gap_advertiser.h:488
Definition: gap_advertiser.h:189
uint8 availAdvDataLen
How many bytes of the advertising data were sent.
Definition: gap_advertiser.h:505