![]() |
![]() |
TI BLE5-Stack API Documentation
2.00.04.00
|
TOF interface.
Go to the source code of this file.
Data Structures | |
struct | rfc_CMD_READ_FS_CAL_s |
RF Read frequency calibration command Structure. More... | |
struct | ToF_BurstStat |
TOF Burst Stats Structure. More... | |
struct | ToF_Params |
TOF Parameters Structure. More... | |
struct | ToF_Status |
TOF Burst Stats Structure. More... | |
Macros | |
#define | CMD_READ_FS_CAL 0x000D |
Read frequency calibration command. | |
#define | FAILURE 0x01 |
Failure. | |
#define | IRQN_DOUBLE_SYNCWORD_BUFFER_SWITCH 11 |
Same as RF_EventTxBufferChange, use with care. | |
#define | IRQN_PARTIAL_READ_READY 15 |
Partial result readout is ready. | |
#define | RF_EventDoubleSyncWordBufferSwitch (1 << IRQN_DOUBLE_SYNCWORD_BUFFER_SWITCH) |
Double syncword buffer switch event bitmap. | |
#define | RF_EventPartialReadReady (1 << IRQN_PARTIAL_READ_READY) |
Partial result readout event bitmap. | |
#define | SUCCESS 0x00 |
SUCCESS. | |
#define | syncWordBufferOneReady 0x01 |
First buffer ready. | |
#define | syncWordBufferTwoReady 0x02 |
Second buffer ready. | |
#define | TICK_TO_METER (6.25 * 3) |
Clock tics to distance in meters conversion. | |
#define | TOF_COMPENSATION_CORRELATOR_COMP 2 |
use correlator compensation | |
#define | TOF_COMPENSATION_NO_COMP 0 |
don't use compensation | |
#define | TOF_COMPENSATION_STIM_COMP 1 |
use STIM compensation (experimental feature) | |
#define | TOF_FILL_1ST_BUFF TOF_SEC_FILL_1ST_BUFF |
Fill first buffers. | |
#define | TOF_FILL_2ND_BUFF TOF_SEC_FILL_2ND_BUFF |
Fill second buffers. | |
#define | TOF_FILL_BOTH_BUFF TOF_SEC_FILL_BOTH_BUFFS |
Fill both buffers. | |
#define | TOF_MAX_NUM_FREQ 20 |
Maximun number of frequencies. | |
#define | TOF_NUM_RFC_BURST_PKTS 32 |
Maximun number of packets in RF burst. | |
#define | TOF_PATCH_LOCATION 0x21000914 |
TOF patch location in memory. | |
#define | TOF_SEEDLEN 32 |
Seed Length in Bytes. | |
#define | TOF_TIMEOUTVAL 0xFFFFFFFF |
TOF Timeout. | |
Typedefs | |
typedef struct __RFC_STRUCT rfc_CMD_READ_FS_CAL_s | rfc_CMD_READ_FS_CAL_t |
RF Read frequency calibration command Structure. | |
typedef void(* | TOF_ApplicationCB) (void) |
Callback to a handler supplied by the application. | |
typedef uint8_t * | ToF_RX_Buf |
Pointer to RX buffer. | |
typedef rfc_CMD_TOF_sample_t | ToF_Sample |
TOF Sample. | |
typedef rfc_CMD_TOF_synthCal_t | ToF_SynthCal |
Pointer to frequency calibration struct, used for the pre-calibration of the synth. | |
typedef uint8_t * | ToF_TX_Buf |
Pointer to TX buffer. | |
Enumerations | |
enum | ToF_Role { ToF_ROLE_SLAVE = 0, ToF_ROLE_MASTER, ToF_ROLE_PASSIVE } |
Enumeration for TOF roles of operation. | |
Functions | |
void | TOF_clearBuffers (ToF_Handle handle) |
Clean buffers for the specified ToF Handle. More... | |
void | TOF_close (ToF_Handle handle) |
Close the ToF and RF drivers. More... | |
uint8_t | TOF_genSeed (void) |
call ToF Security module to generate a true 128-bit random seed More... | |
void | TOF_getBurstStat (ToF_Handle handle, ToF_BurstStat **resultBuffer) |
Get the result for the last ToF burst (run) More... | |
uint8_t | TOF_getSeed (uint8_t *dst) |
copy 32 byte seed into dst More... | |
uint8_t | TOF_initSyncWords (void) |
Init sync words buffer, depends on user configuration. More... | |
ToF_Handle | TOF_open (ToF_Struct *tofStruct, ToF_Params *params) |
Initiate RF ToF params and open RF driver. More... | |
ToF_Status | TOF_run (ToF_Handle handle, uint32_t nextTaskTime) |
Start a ToF run. More... | |
uint8_t | TOF_setSeed (uint8_t *newSeed) |
call ToF Security module to restart the ctr drbg new 128-bit random seed More... | |
void | TOF_skipSyncWords (void) |
Skip some syncwords into the future (for synchronization purposes) More... | |