Green Power Device Application Overview¶
Green Power Device¶
A Green Power Device (GPD) is a special type of Zigbee device different from the three logical devices defined in Zigbee PRO: Coordinator, Router or End Device. These devices are designed for application where the end product has a very strict energy budget, such as an energy-harvesting device or bateryless devices. GPDs follows their own Zigbee specification which defines the possible capabilities of a given GPD implementation, such as security level, commissioning procedures and supported commands per device definition. As GPDs are the most restricted device in terms of functionality, these devices are not part of the Zigbee network unless those are commissioned to a Green Power Sink (GPS) device directly or through a Green Power Proxy (GPP). If the device to which it got commissioned is not present, then the device must be recommissioned as it does not have a means to keep communication with any other device. Once the GPD is commissioned it can send Green Power Data Frames (GPDF) which are converted by the GPP into Green Power Notifications (ZCL frames) that can travel through the Zigbee network until it reaches its GPS destination to be processed by the application. For further details on GPDs and its interactions with the network, please refer to Green Power.
General Application Architecture¶
This section describes how a Green Power Device application task is structured in more detail.
Green Power Configuration¶
gpd_config.h
provides configuration definitions for parameters like
device ID, security level and security keys. To change the Green Power Device
behavior is neccesary to modify the predefined symbols in the project properties.
Green Power Device definitions | ||
---|---|---|
Name | Description | Values |
DEVICE_ID | (uint8) Green Power Device ID | 0x00 - 0xFF, refer to GPD spec |
GPD_APP_ID | Unique identifier of the GPD, either the 4-byte SrcID or the IEEE Addr | 0b00 GPD_APP_TYPE_SRC_ID
0b10 GPD_APP_TYPE_IEEE_ID
|
GPDF_FRAME_DUPLICATES | (uint8) Application-specific. Number of GPDF retries per packet. | 0x00 - 0xFF (recommended to be low, more retries = more power consumption) |
GPD_CHANNEL | IEEE channel, 11 - 26 (in Hex) | 0x0B - 0x1A |
GP_SECURITY_LEVEL | Defines the security level which GPDF packets are encrypted and sent with | 0b00 GP_SECURITY_LVL_NO_SEC
0b01 Reserved
0b10 GP_SECURITY_LVL_4FC_4MIC
0b11 GP_SECURITY_LVL_4FC_4MIC_ENCRYPT
|
AUTO_COMMISSIONING | Defines whether or not the device will automatically start commissioning on power-up | TRUE/FALSE |
RX_AFTER_TX | RxOnCapability commissioning option. Defines whether or not GPD will turn RX on after TXing a frame, i.e. whether or not GPD is expecting a response | TRUE/FALSE |
SEQUENCE_NUMBER_CAP | Sequence Number Capability commissioning option. Defines if GPD will use Seq Num | TRUE/FALSE |
BATTERYLESS_DEVICE | Configures settings base on whether the device operates on battery power or energy harvesting | Defined or not |
Note
Please refer to the preprocessor symbols section of the Z-Stack Quick Start Guide to setup compile options for the project if using IAR.
Non Volatile Memory¶
gpd_memory.c
provides an interface for Non Volatile (NV) memory required for
attribute persistence in some GPD configurations. For example the persistence
of sequence number when SEQUENCE_NUMBER_CAP
is required. Use gp_nv_item_init()
to create a new NV item, then gp_nv_read()
to get the NV value and
gp_nv_write()
to update the NV value when necesary.
Callbacks¶
The application code also likely includes various callbacks from the protocol stack layer and RTOS modules. To ensure thread safety, processing should be minimized in the actual callback, and the bulk of the processing should be done in the application context.
static uint16 gpdSampleSw_process_loop( void )
{
/* Forever loop */
for(;;)
{
if(events & SAMPLEAPP_KEY_EVT)
{
// Process Key Presses
gpdSampleSw_processKey(keys);
keys = 0;
events &= ~SAMPLEAPP_KEY_EVT;
}
ApiMac_processIncoming();
}
}
Send Green Power Data Frames¶
An API to send Green Power Data Frames (GPDF) is provided in gpd.c
. The generic
function GreenPowerDataFrameSend()
sends a frame formated for the Green
Power Device configuration automatically by providing a gpdfReq_t
struct,
the desired channel and a flag to enable frame security.
Additionally GreenPowerCommissioningSend()
and GreenPowerAttributeReportingSend()
functions use GreenPowerDataFrameSend()
to generate the corresponding commands.
Setting Up the Network with GPD and GPS¶
To set up a network with a Green Power Device (GPD) and a Green Power Sink (GPS), you will need 3 devices:
- Green Power Device (
gpd_switch
orgpd_temperaturesensor
)- Green Power Sink (
zc/zr_light_sink
orzc/zr_thermostat_sink
)- Optional: Green Power Proxy (any other Zigbee 3.0 routing device, e.g.
zc/zr_genericapp
)
Select Network Channel¶
First, determine which channel you would like to use for your test. To change the channel mask of the Green Power Sink and Green Power Proxy,
modify DEFAULT_CHANLIST
in zstack_config.h
. To change the channel of the Green Power Device, change GPD_CHANNEL
in the predefined symbols.
Create and Open the Network on the GPS¶
Next, create a network with your coordinator. For example, use zc_light_sink
to create a network, following the
instructions in the Commissioning the Device Into the Network section of this readme:
Join the GPP Device¶
If you would prefer a Green Power Proxy (GPP) to route GP Data Frames, it must be joined to the network formed by the coordinator.
For example, we can use zr_genericapp
as a GPP by simply joining it into the network,
following the instructions Example Usage section of this readme:
-
Note
This step is entirely optional as the GPD can be directly commissioned to the GPS coordinator
Enable Commissioning on the GPS¶
Next, enable GPS Commissioning on the zc_light_sink
by following the instructions in the Interfacing with the GP On/Off Switch Example App
section of this readme:
Commission the GPD into the Network¶
Lastly, commission a GPD like the gpd_switch
into the network by following the instructions in the Interfacing with the Light Sink Example App
section of this readme:
Example Ubiqua Capture of Green Power Traffic¶
Here is an annotated Ubiqua capture of the expected behavior following the instructions above: