Clocks¶
Clock instances are functions that can be scheduled to run after a certain
number of system ticks. Clock instances are either one-shot or periodic. These
instances start immediately upon creation, are configured to start after a
delay, and can be stopped at any time. All clock instances are executed when
they expire in the context of a Swi. The following example shows the
minimum resolution is the TI-RTOS clock tick period set in the TI-RTOS
configuration file (.cfg
).
Note
The default TI-RTOS kernel tick period is 1 millisecond. For CC13x2 or CC26x2
devices, this is reconfigured in the TI-RTOS configuration file (.cfg
):
Clock.tickPeriod = 10;
Each system tick, which is derived from the real-time clock RTC, launches a Clock object that compares the running tick count with the period of each clock to determine if the associated function should run. For higher-resolution timers, TI recommends using a 16-bit hardware timer channel or the sensor controller. See the Clock module in the package ti.sysbios.knl section of the TI-RTOS Kernel User Guide for more information on these functions.
You can use the Kernel’s Clock APIs directly in your application and in addition
the Util
module also contains a set of abstracted TI-RTOS Clock functions as
shown here:
- Util_constructClock() creates a Clock object.
- Util_startClock() starts an existing Clock object.
- Util_restartClock() stops, restarts an existing Clock object.
- Util_isActive() checks if a Clock object is running.
- Util_stopClock() stop an existing Clock object.
- Util_rescheduleClock() reconfigure an existing Clock object.
Functional Example¶
The following example was taken from the simple_peripheral project in BLE5-Stack.
Figure 65. Triggering Clock objects¶
Step 1 in Triggering Clock objects constructs the Clock object via Util_constructClock(). After the example entered a connected state, it will then start the Clock object via a Util_startClock().
// Clock instances for internal periodic events.
static Clock_Struct periodicClock;
// Create one-shot clocks for internal periodic events.
Util_constructClock(&periodicClock, SimplePeripheral_clockHandler,
SP_PERIODIC_EVT_PERIOD, 0, false, SP_PERIODIC_EVT);
Step 2 in Triggering Clock objects, after the Clock object’s timer expired,
it will execute SimplePeripheral_clockHandler()
within a Swi context. As
this call cannot be blocked and blocks all Tasks, it is kept short by invoking
an Event_post(SP_PERIODIC_EVT)
for post processing in simple_peripheral.
static void SimplePeripheral_clockHandler(UArg arg)
{
/* arg is passed in from Clock_construct() */
Event_post(events, arg);
}
Attention
Clock functions must not call blocking kernel APIs or TI-RTOS driver APIs! Executing long routines will impact real-time constraints placed in high priority tasks allocated for wireless protocol stacks!
Step 3 in Triggering Clock objects, the simple_peripheral task is
unblocked due the Event_post(SP_PERIODIC_EVT)
, where it proceeds to invoke
the SimplePeripheral_performPeriodicTask()
function. Afterwards, to
restart the periodic execution of this function, it will restart the
periodicClock
Clock object.
if (events & SP_PERIODIC_EVT)
{
// Perform periodic application task
SimplePeripheral_performPeriodicTask();
Util_startClock(&periodicClock);
}