SimpleLink MCU SDK Driver API Reference

Drivers

Shown below is a matrix of available drivers.

NOTE: Please view the Device Specific driver implementations as they may contain or exclude certain features that are defined in the top level interfaces.

Driver Interfaces CC13xx/CC26xx
Common Implementations
CC13x0/CC26x0
Implementations
CC13x2/CC26x2
Implementations
ADC.h ADCCC26XX.h
ADCBuf.h ADCBufCC26XX.h ADCBufCC26X2.h
AESCBC.h AESCBCCC26XX.h
AESCCM.h AESCCMCC26XX.h
AESECB.h AESECBCC26XX.h
Crypto CryptoCC26XX.h
ECDH.h ECDHCC26X2.h
ECDSA.h ECDSACC26X2.h
ECJPAKE.h ECJPAKECC26X2.h
GPIO.h GPIOCC26XX.h
GPTimer GPTimerCC26XX.h
I2C.h I2CCC26XX.h
NVS.h NVSCC26XX.h
NVSRAM.h
NVSSPI25X.h
PDM PDMCC26XX.h
PIN.h PINCC26XX.h
Power.h PowerCC26XX.h PowerCC26X2.h
PWM.h PWMTimerCC26XX.h
RF RF.h
SHA2.h SHA2CC26X2.h
SD.h SDSPI.h
SPI.h SPICC26XXDMA.h SPICC26X2DMA.h
TRNG.h TRNGCC26X0.h TRNGCC26X2.h
UART.h UARTCC26XX.h
UDMA UDMACC26XX.h
Watchdog.h WatchdogCC26XX.h

Display Driver

The Display driver is designed to abstract operations and considerations specific to a given output method.

Display Driver Interface Implementations
Display.h DisplayDogm1286.h
DisplayExt.h
DisplayHost.h
DisplaySharp.h
DisplayUart.h

Driver Utilities

These utilities are helper modules available to drivers. Shown below is a list of utility modules available to drivers:

Note: The SDFatFS interface is a wrapper to enable the use of the FatFS filesystem via the SD driver.

Note: The SPIFFSNVS is a wrapper to enable NVS as the physical layer to read/write memory for the SPIFFS file system. See spiffs.h.

NoRTOS Framework Module

The NoRTOS framework module is provided to enable use of drivers without an underlying operating system. The module provides interfaces used by drivers to perform delays, block execution, register interrupts and more. NoRTOS module documentation and usage can be found:

© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale