Setting up the BLE OAD Environment¶
This section will cover the steps required to setup a BLE OAD environment.
The BLE OAD topology is described below. Refer to Figure 129. for a review of the devices involved in an OAD.
- OAD Distributor: BTool connected to Host Test on CC13x2 or CC26x2 LaunchPad.
- OAD Target: BLE sample application (
simple_peripheral,project_zero) with OAD functionality enabled.Note
TI provides mobile applications that support OAD, these are outside of the scope of the OAD guide. Refer to the Quick Start Guide for more information. Project zero does not support secure OAD at this time
Prerequisites¶
This section requires the following hardware and software components
- 2x CC13x2 or CC26x2 LaunchPad
- SimpleLink CC13x2 / 26x2 SDK installed
- Uniflash
OAD Target Setup¶
In order to perform a BLE OAD, an OAD capable image must be loaded onto the OAD target device. This section will cover the steps required to load the CC13x2 or CC26x2 LaunchPad with an OAD enabled BLE image.
Navigate to the
simple_peripheral_oad_offchiporsimple_peripheral_oad_onchipfolder inside the BLE5-Stack.Import the projects into the workspace of your selected IDE.
- See the Quick Start Guide for instructions on how to work with your selected IDE.
- Select the proper build configuration based on security needs:
DebugorRelease: will use security and is the default configurationDebug_unsecureorRelease_unsecure: will not use security- Be sure that all projects configurations are in sync. If one
_unsecureproject is used, all other projects should use the unsecure flavor as well.- Based on the project configuration, the proper version of the OAD Image Tool will be used. If security is enabled the signature is automatically added to the image.
Build the stack project
(on-chip OAD only) Build and flash the persistent app project -The build steps must be done in order, or errors will occur
Build and flash the app project
- Uniflash must be used to flash the _oad.bin image that is produced by the oad_image_tool or the device will not boot after a reset.
- The _oad.bin file contains CRC and (if applicable) security information about the image. This is used by the BIM on boot to determine which image to run. If the image is flashed directly from the IDE, the device will not boot after subsequent resets as either CRC or security information is missing
- See Loading a Production Image for more information.
Build the flash the BIM project
- The BIM debug configuration does not do CRC checks on the image, making it possible to flash an image straight from the IDE.
- If your device does not boot, it is likely that the incorrect version of BIM was flashed, see Loading a Production Image for more info.
Verify the device has booted up and is advertising
- Verification: Open a terminal window with 115200 8N1 to the
XDS110 Class Application/User UARTport corresponding to your CC13x2 or CC26x2 LaunchPad.- The console should display the text below, use it to get the BLE address.
![]()
Alternatively, you can get the BLE address of the device using UNIFLASH.
- See the screenshot below for how to do this in UNIFLASH.
![]()
- Plug/unplug the device to prevent Halt In Boot (HIB)
- If the device does not advertise after reset, ensure the _oad.bin file was loaded.
OAD Distributor Setup¶
As per the Introduction section, the OAD Distributor is the device responsible for fragmenting an OAD enabled image in to chunks of OAD blocks and sending each block over the to the OAD Target device as they are requested.
In the case of BLE, the OAD Distributor is a combination of BTool running on
the PC connected to host_test running on a CC13x2 or CC26x2 LaunchPad. host_test is a BLE
enabled network processor application. BTool is a PC tool that is capable of
interfacing to host_test and performing various BLE functions in addition to
OAD. For more information, refer to the host_test README file or the BTool
User’s Guide.
Flashing the host_test Image¶
See below for the steps to setup the host_test image on a CC13x2 or CC26x2 LaunchPad.
- Navigate to
hexfilesfolder within the BLE5-Stack.- Select the
host_test_*.hexfile.- Flash the above hexfile using UNIFLASH. See image below
![]()
Connecting BTool to host_test¶
BTool and host_test communicate via USB through the XDS110 UART back channel. See below for a diagram
![]()
Find the port used by the UART backchannel of the CC13x2 or CC26x2 LaunchPad running host_test. This is the one with the name
XDS110 Class Application/User UARTOpen BTool (see the BTool executable in the tools folder of the BLE5-Stack)
Use the following serial port settings, hit OK
- Port: <PORT_FROM_ABOVE_STEP>
- Other settings: 115200 8N1
This should open and initialize the host_test device.
Pressing the scan button should populate a list of devices in the log
- A screen shot of a properly initialized BTool session is shown below
![]()