ECJPAKECC26X2.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2017-2018, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
88 #ifndef ti_drivers_ecjpake_ECJPAKECC26X2__include
89 #define ti_drivers_ecjpake_ECJPAKECC26X2__include
90 
91 #ifdef __cplusplus
92 extern "C" {
93 #endif
94 
95 #include <stdint.h>
96 #include <stdbool.h>
97 
98 #include <ti/drivers/Power.h>
99 #include <ti/drivers/ECJPAKE.h>
102 
103 #include <ti/drivers/dpl/HwiP.h>
104 #include <ti/drivers/dpl/SwiP.h>
105 #include <ti/drivers/dpl/SemaphoreP.h>
106 
107 /* Exit the SWI and wait until an HWI call posts the SWI again */
108 #define ECJPAKECC26X2_STATUS_FSM_RUN_PKA_OP ECJPAKE_STATUS_RESERVED - 0
109 /* Execute the next FSM state immediately without waiting for the next HWI */
110 #define ECJPAKECC26X2_STATUS_FSM_RUN_FSM ECJPAKE_STATUS_RESERVED - 1
111 
123 
137 
149 
160 
177 
187 
189 
196 typedef struct ECJPAKECC26X2_HWAttrs_ {
209  uint8_t intPriority;
211 
217 typedef struct ECJPAKECC26X2_Object_ {
218  bool isOpen;
221  int_fast16_t operationStatus;
224  ECJPAKECC26X2_FsmState fsmState;
228  uint32_t resultAddress;
230 
231 #ifdef __cplusplus
232 }
233 #endif
234 
235 #endif /* ti_drivers_ecjpake_ECJPAKECC26X2__include */
ECJPAKECC26X2 Hardware Attributes.
Definition: ECJPAKECC26X2.h:196
ECJPAKE_OperationType operationType
Definition: ECJPAKECC26X2.h:226
The CryptoKey type is an opaque representation of a cryptographic key.
bool operationCanceled
Definition: ECJPAKECC26X2.h:220
ECJPAKE_OperationType
Enum for the operation types supported by the driver.
Definition: ECJPAKE.h:1027
bool isOpen
Definition: ECJPAKECC26X2.h:218
Power Manager.
Definition: ECJPAKECC26X2.h:152
Definition: ECJPAKECC26X2.h:159
uint8_t intPriority
PKA Peripheral&#39;s interrupt priority.
Definition: ECJPAKECC26X2.h:209
ECJPAKE_CallbackFxn callbackFxn
Definition: ECJPAKECC26X2.h:222
Definition: ECJPAKECC26X2.h:148
struct ECJPAKECC26X2_HWAttrs_ ECJPAKECC26X2_HWAttrs
ECJPAKECC26X2 Hardware Attributes.
Definition: ECJPAKECC26X2.h:136
void(* ECJPAKE_CallbackFxn)(ECJPAKE_Handle handle, int_fast16_t returnStatus, ECJPAKE_Operation operation, ECJPAKE_OperationType operationType)
The definition of a callback function used by the ECJPAKE driver when used in ECJPAKE_RETURN_BEHAVIOR...
Definition: ECJPAKE.h:1053
Definition: ECJPAKECC26X2.h:169
ECJPAKECC26X2 Object.
Definition: ECJPAKECC26X2.h:217
uint32_t resultAddress
Definition: ECJPAKECC26X2.h:228
uint32_t semaphoreTimeout
Definition: ECJPAKECC26X2.h:227
int_fast16_t operationStatus
Definition: ECJPAKECC26X2.h:221
Definition: ECJPAKECC26X2.h:174
bool operationInProgress
Definition: ECJPAKECC26X2.h:219
ECJPAKECC26X2_FsmState fsmState
Definition: ECJPAKECC26X2.h:224
Definition: ECJPAKECC26X2.h:176
Definition: ECJPAKECC26X2.h:151
ECJPAKECC26X2_FsmState_
ECJPAKECC26X2 states.
Definition: ECJPAKECC26X2.h:121
enum ECJPAKECC26X2_FsmState_ ECJPAKECC26X2_FsmState
ECJPAKECC26X2 states.
struct ECJPAKECC26X2_Object_ ECJPAKECC26X2_Object
ECJPAKECC26X2 Object.
ECJPAKE_ReturnBehavior returnBehavior
Definition: ECJPAKECC26X2.h:223
TI Driver for Elliptic Curve Password Authenticated Key Exchange by Juggling.
Definition: ECJPAKECC26X2.h:122
Definition: ECJPAKECC26X2.h:142
ECJPAKE_Operation operation
Definition: ECJPAKECC26X2.h:225
ECJPAKE_ReturnBehavior
The way in which ECJPAKE function calls return after performing an encryption + authentication or dec...
Definition: ECJPAKE.h:766
Definition: ECJPAKECC26X2.h:157
Definition: ECJPAKECC26X2.h:153
Definition: ECJPAKECC26X2.h:155
Union containing pointers to all supported operation structs.
Definition: ECJPAKE.h:1016
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale