|
TI BLE Stack API Documentation
2.03.11
|
HCI layer interface. More...
#include "bcomdef.h"#include "osal.h"#include "ll.h"#include "hal_assert.h"Go to the source code of this file.
Classes | |
| struct | hciEvt_BLEConnComplete_t |
| LE Connection Complete Event. More... | |
| struct | hciEvt_BLEEnhConnComplete_t |
| LE Enhanced Connection Complete Event. More... | |
| union | _hciEvt_BLEConnComplete_u_ |
| LE Connection Complete Event. More... | |
| struct | hciEvt_DevInfo_t |
| LE Advertising Report Event. More... | |
| struct | hciEvt_BLEAdvPktReport_t |
| LE Advertising Packet Report Event. More... | |
| struct | hciEvt_BLEScanReqReport_t |
| VS LE Scan Request Report Event. More... | |
| struct | hciEvt_BLEConnUpdateComplete_t |
| LE Connection Update Complete Event. More... | |
| struct | hciEvt_BLEReadRemoteFeatureComplete_t |
| LE Read Remote Used Features Complete Event. More... | |
| struct | hciEvt_EncryptChange_t |
| LE Encryption Change Event. More... | |
| struct | hciEvt_BLELTKReq_t |
| LE Long Term Key Requested Event. More... | |
| struct | hciEvt_NumCompletedPkt_t |
| Number of Completed Packets Event. More... | |
| struct | hciEvt_CmdComplete_t |
| Command Complete Event. More... | |
| struct | hciEvt_VSCmdComplete_t |
| Vendor Specific Command Complete Event. More... | |
| struct | hciEvt_CommandStatus_t |
| Command Status Event. More... | |
| struct | hciEvt_HardwareError_t |
| Hardware Error Event. More... | |
| struct | hciEvt_DisconnComplete_t |
| Disconnection Complete Event. More... | |
| struct | hciEvt_BufferOverflow_t |
| Data Buffer Overflow Event. More... | |
| struct | hciEvt_AptoExpired_t |
| Authenticated Payload Timeout Expired Event. More... | |
| struct | hciEvt_BLERemoteConnParamReq_t |
| LE Remote Connection Parameter Request Event. More... | |
| struct | hciEvt_BLEPhyUpdateComplete_t |
| LE Phy Update Complete Event. More... | |
| struct | hciEvt_BLEDataLengthChange_t |
| LE Data Length Change Event. More... | |
| struct | hciEvt_BLEReadP256PublicKeyComplete_t |
| LE Read P256 Public Key Complete Event. More... | |
| struct | hciEvt_BLEGenDHKeyComplete_t |
| LE Generate DHKey Complete Event. More... | |
| struct | hciRetParam_LeReadBufSize_t |
| Data structure for HCI Command Complete Event Return Parameter. More... | |
| struct | hciPacket_t |
| HCI Packet event. More... | |
| struct | hciDataPacket_t |
| HCI Data Packet. More... | |
| struct | hciConnInfo_t |
| struct | hciPER_t |
Macros | |
| #define | HCI_SUCCESS 0x00 |
| Success. | |
| #define | HCI_ERROR_CODE_UNKNOWN_HCI_CMD 0x01 |
| Unknown HCI Command. | |
| #define | HCI_ERROR_CODE_UNKNOWN_CONN_ID 0x02 |
| Unknown Connection ID. | |
| #define | HCI_ERROR_CODE_HW_FAILURE 0x03 |
| Hardware Failure. | |
| #define | HCI_ERROR_CODE_PAGE_TIMEOUT 0x04 |
| Page Timeout. | |
| #define | HCI_ERROR_CODE_AUTH_FAILURE 0x05 |
| Authentication Fialure. | |
| #define | HCI_ERROR_CODE_PIN_KEY_MISSING 0x06 |
| Pin Key Missing. | |
| #define | HCI_ERROR_CODE_MEM_CAP_EXCEEDED 0x07 |
| Memory Capability Exceeded. | |
| #define | HCI_ERROR_CODE_CONN_TIMEOUT 0x08 |
| Connection Timeout. | |
| #define | HCI_ERROR_CODE_CONN_LIMIT_EXCEEDED 0x09 |
| Connection Limit Exceeded. | |
| #define | HCI_ERROR_CODE_SYNCH_CONN_LIMIT_EXCEEDED 0x0A |
| Synchonous Connection Limit Exceeded. | |
| #define | HCI_ERROR_CODE_ACL_CONN_ALREADY_EXISTS 0x0B |
| ACL Connection Already Exists. | |
| #define | HCI_ERROR_CODE_CMD_DISALLOWED 0x0C |
| Command Disallowed. | |
| #define | HCI_ERROR_CODE_CONN_REJ_LIMITED_RESOURCES 0x0D |
| Connection Rejected due to Limited Resources. | |
| #define | HCI_ERROR_CODE_CONN_REJECTED_SECURITY_REASONS 0x0E |
| Connection Rejected for Security Reasons. | |
| #define | HCI_ERROR_CODE_CONN_REJECTED_UNACCEPTABLE_BDADDR 0x0F |
| Connection Rejected due to Unacceptable BDADDR. | |
| #define | HCI_ERROR_CODE_CONN_ACCEPT_TIMEOUT_EXCEEDED 0x10 |
| Connection Acceptance Timeout Exceeded. | |
| #define | HCI_ERROR_CODE_UNSUPPORTED_FEATURE_PARAM_VALUE 0x11 |
| Unsupported Paramter. | |
| #define | HCI_ERROR_CODE_INVALID_HCI_CMD_PARAMS 0x12 |
| Invalid HCI Command Parameters. | |
| #define | HCI_ERROR_CODE_REMOTE_USER_TERM_CONN 0x13 |
| Remote User Terminated Connection. | |
| #define | HCI_ERROR_CODE_REMOTE_DEVICE_TERM_CONN_LOW_RESOURCES 0x14 |
| Remote Device Terminated Connection due to Low Resources. | |
| #define | HCI_ERROR_CODE_REMOTE_DEVICE_TERM_CONN_POWER_OFF 0x15 |
| Remote Device Terminated Connection due to Power Off. | |
| #define | HCI_ERROR_CODE_CONN_TERM_BY_LOCAL_HOST 0x16 |
| Connection Terminated by Local Host. | |
| #define | HCI_ERROR_CODE_REPEATED_ATTEMPTS 0x17 |
| Repeated Attempts. | |
| #define | HCI_ERROR_CODE_PAIRING_NOT_ALLOWED 0x18 |
| Pairing Not Allowed. | |
| #define | HCI_ERROR_CODE_UNKNOWN_LMP_PDU 0x19 |
| Unknown LMP PDU. | |
| #define | HCI_ERROR_CODE_UNSUPPORTED_REMOTE_FEATURE 0x1A |
| Unsupported Remote Feature. | |
| #define | HCI_ERROR_CODE_SCO_OFFSET_REJ 0x1B |
| SCO Offset Rejected. | |
| #define | HCI_ERROR_CODE_SCO_INTERVAL_REJ 0x1C |
| SCO Interval Rejected. | |
| #define | HCI_ERROR_CODE_SCO_AIR_MODE_REJ 0x1D |
| SCO Air Mode Rejected. | |
| #define | HCI_ERROR_CODE_INVALID_LMP_PARAMS 0x1E |
| Invalid LMP Paramaters. | |
| #define | HCI_ERROR_CODE_UNSPECIFIED_ERROR 0x1F |
| Unspecified Error. | |
| #define | HCI_ERROR_CODE_UNSUPPORTED_LMP_PARAM_VAL 0x20 |
| Unsupported LMP Parameter Value. | |
| #define | HCI_ERROR_CODE_ROLE_CHANGE_NOT_ALLOWED 0x21 |
| Role Change Not Allowed. | |
| #define | HCI_ERROR_CODE_LMP_LL_RESP_TIMEOUT 0x22 |
| LMP LL Response Timeout. | |
| #define | HCI_ERROR_CODE_LMP_ERR_TRANSACTION_COLLISION 0x23 |
| LMP Error Transaction Collision. | |
| #define | HCI_ERROR_CODE_LMP_PDU_NOT_ALLOWED 0x24 |
| LMP DU Not Allowed. | |
| #define | HCI_ERROR_CODE_ENCRYPT_MODE_NOT_ACCEPTABLE 0x25 |
| Encrypt Mode not Acceptable. | |
| #define | HCI_ERROR_CODE_LINK_KEY_CAN_NOT_BE_CHANGED 0x26 |
| Link Key Can Not Be Changed. | |
| #define | HCI_ERROR_CODE_REQ_QOS_NOT_SUPPORTED 0x27 |
| Request QOS Not Supported. | |
| #define | HCI_ERROR_CODE_INSTANT_PASSED 0x28 |
| Instant Passed. | |
| #define | HCI_ERROR_CODE_PAIRING_WITH_UNIT_KEY_NOT_SUPPORTED 0x29 |
| Pairing with Unit Key Not Supported. | |
| #define | HCI_ERROR_CODE_DIFFERENT_TRANSACTION_COLLISION 0x2A |
| Different Transaction Collision. | |
| #define | HCI_ERROR_CODE_RESERVED1 0x2B |
| Reserved. | |
| #define | HCI_ERROR_CODE_QOS_UNACCEPTABLE_PARAM 0x2C |
| QOS Unacceptable Parameter. | |
| #define | HCI_ERROR_CODE_QOS_REJ 0x2D |
| QOS Reject. | |
| #define | HCI_ERROR_CODE_CHAN_ASSESSMENT_NOT_SUPPORTED 0x2E |
| Channel Assessment Not Supported. | |
| #define | HCI_ERROR_CODE_INSUFFICIENT_SECURITY 0x2F |
| Insufficient Security. | |
| #define | HCI_ERROR_CODE_PARAM_OUT_OF_MANDATORY_RANGE 0x30 |
| Paramater out of Mandatory Range. | |
| #define | HCI_ERROR_CODE_RESERVED2 0x31 |
| Reserved. | |
| #define | HCI_ERROR_CODE_ROLE_SWITCH_PENDING 0x32 |
| Role Switch Pending. | |
| #define | HCI_ERROR_CODE_RESERVED3 0x33 |
| Reserved. | |
| #define | HCI_ERROR_CODE_RESERVED_SLOT_VIOLATION 0x34 |
| Reserved Slot Violation. | |
| #define | HCI_ERROR_CODE_ROLE_SWITCH_FAILED 0x35 |
| Role Switch Failed. | |
| #define | HCI_ERROR_CODE_EXTENDED_INQUIRY_RESP_TOO_LARGE 0x36 |
| Extended Inquiry Response too Large. | |
| #define | HCI_ERROR_CODE_SIMPLE_PAIRING_NOT_SUPPORTED_BY_HOST 0x37 |
| Simple Pairing Not Supported by Host. | |
| #define | HCI_ERROR_CODE_HOST_BUSY_PAIRING 0x38 |
| Host Busy Pairing. | |
| #define | HCI_ERROR_CODE_CONN_REJ_NO_SUITABLE_CHAN_FOUND 0x39 |
| Connection Rejected No Suitable Channel Found. | |
| #define | HCI_ERROR_CODE_CONTROLLER_BUSY 0x3A |
| Controller Busy. | |
| #define | HCI_ERROR_CODE_UNACCEPTABLE_CONN_PARAMETERS 0x3B |
| Unacceptable Connection Parameters. | |
| #define | HCI_ERROR_CODE_DIRECTED_ADV_TIMEOUT 0x3C |
| Directed Advertising Timeout. | |
| #define | HCI_ERROR_CODE_CONN_TERM_MIC_FAILURE 0x3D |
| Connection Terminated due to MIC Failure. | |
| #define | HCI_ERROR_CODE_CONN_FAILED_TO_ESTABLISH 0x3E |
| Connection Failued to Establish. | |
| #define | HCI_ERROR_CODE_MAC_CONN_FAILED 0x3F |
| MAC Connection Failed. | |
| #define | HCI_ERROR_CODE_COARSE_CLOCK_ADJUST_REJECTED 0x40 |
| Coarse Clock Adjust Rejected. | |
| #define | HCI_MAX_NUM_CMD_BUFFERS LL_MAX_NUM_CMD_BUFFERS |
| Max Num Command Buffer. | |
| #define | FIRST_PKT_HOST_TO_CTRL LL_DATA_FIRST_PKT_HOST_TO_CTRL |
| First Host to Controller Packet. | |
| #define | CONTINUING_PKT LL_DATA_CONTINUATION_PKT |
| Continuing Packet. | |
| #define | FIRST_PKT_CTRL_TO_HOST LL_DATA_FIRST_PKT_CTRL_TO_HOST |
| First Packet Controller to Host. | |
| #define | HCI_RSSI_NOT_AVAILABLE LL_RSSI_NOT_AVAILABLE |
| Invalid RSSI. | |
| #define | HCI_DISCONNECT_AUTH_FAILURE HCI_ERROR_CODE_AUTH_FAILURE |
| Authentication Failure. | |
| #define | HCI_DISCONNECT_REMOTE_USER_TERM HCI_ERROR_CODE_REMOTE_USER_TERM_CONN |
| Remote User Terminated. | |
| #define | HCI_DISCONNECT_REMOTE_DEV_LOW_RESOURCES HCI_ERROR_CODE_REMOTE_DEVICE_TERM_CONN_LOW_RESOURCES |
| Remote Device Low Resources. | |
| #define | HCI_DISCONNECT_REMOTE_DEV_POWER_OFF HCI_ERROR_CODE_REMOTE_DEVICE_TERM_CONN_POWER_OFF |
| Remote Device Power Off. | |
| #define | HCI_DISCONNECT_UNSUPPORTED_REMOTE_FEATURE HCI_ERROR_CODE_UNSUPPORTED_REMOTE_FEATURE |
| Unsupported Remote Feature. | |
| #define | HCI_DISCONNECT_KEY_PAIRING_NOT_SUPPORTED HCI_ERROR_CODE_PAIRING_WITH_UNIT_KEY_NOT_SUPPORTED |
| Key Paring Not Supported. | |
| #define | HCI_DISCONNECT_UNACCEPTABLE_CONN_INTERVAL HCI_ERROR_CODE_UNACCEPTABLE_CONN_INTERVAL |
| Unnaceptable Connection Interval. | |
| #define | HCI_READ_CURRENT_TX_POWER_LEVEL LL_READ_CURRENT_TX_POWER_LEVEL |
| Read Current TX Power Level. | |
| #define | HCI_READ_MAX_TX_POWER_LEVEL LL_READ_MAX_TX_POWER_LEVEL |
| Read Max TX Power Level. | |
| #define | HCI_CTRL_TO_HOST_FLOW_CTRL_OFF 0 |
| Controller to Host Flow Controll Off. | |
| #define | HCI_CTRL_TO_HOST_FLOW_CTRL_ACL_ON_SYNCH_OFF 1 |
| ACL On, Synchronous Off. | |
| #define | HCI_CTRL_TO_HOST_FLOW_CTRL_ACL_OFF_SYNCH_ON 2 |
| ACL Off, Synchronous On. | |
| #define | HCI_CTRL_TO_HOST_FLOW_CTRL_ACL_ON_SYNCH_ON 3 |
| ACL On, Synchronous On. | |
| #define | HCI_PUBLIC_DEVICE_ADDRESS LL_DEV_ADDR_TYPE_PUBLIC |
| Public Device Address. | |
| #define | HCI_RANDOM_DEVICE_ADDRESS LL_DEV_ADDR_TYPE_RANDOM |
| Random Device Address. | |
| #define | HCI_CONNECTABLE_UNDIRECTED_ADV LL_ADV_CONNECTABLE_UNDIRECTED_EVT |
| Connectable Undirected Advertising. | |
| #define | HCI_CONNECTABLE_DIRECTED_HDC_ADV LL_ADV_CONNECTABLE_DIRECTED_HDC_EVT |
| Connectable Directed High Duty Cycle Advertising. | |
| #define | HCI_SCANNABLE_UNDIRECTED LL_ADV_SCANNABLE_UNDIRECTED_EVT |
| Scannable Undirected Advertising. | |
| #define | HCI_NONCONNECTABLE_UNDIRECTED_ADV LL_ADV_NONCONNECTABLE_UNDIRECTED_EVT |
| Nonconnectable Undirected Advertising. | |
| #define | HCI_CONNECTABLE_DIRECTED_LDC_ADV LL_ADV_CONNECTABLE_DIRECTED_LDC_EVT |
| Connectable Directed Low Duty Cycle Advertising. | |
| #define | HCI_ADV_CHAN_37 LL_ADV_CHAN_37 |
| Channel 37. | |
| #define | HCI_ADV_CHAN_38 LL_ADV_CHAN_38 |
| Channel 38. | |
| #define | HCI_ADV_CHAN_39 LL_ADV_CHAN_39 |
| Channel 39. | |
| #define | HCI_ADV_CHAN_ALL (LL_ADV_CHAN_37 | LL_ADV_CHAN_38 | LL_ADV_CHAN_39) |
| All Channels. | |
| #define | HCI_ADV_WL_POLICY_ANY_REQ LL_ADV_WL_POLICY_ANY_REQ |
| Any Request. | |
| #define | HCI_ADV_WL_POLICY_WL_SCAN_REQ LL_ADV_WL_POLICY_WL_SCAN_REQ |
| Scan Requests. | |
| #define | HCI_ADV_WL_POLICY_WL_CONNECT_REQ LL_ADV_WL_POLICY_WL_CONNECT_REQ |
| Connection Requests. | |
| #define | HCI_ADV_WL_POLICY_WL_ALL_REQ LL_ADV_WL_POLICY_WL_ALL_REQ |
| All Requests. | |
| #define | HCI_ENABLE_ADV LL_ADV_MODE_ON |
| Advertising Enable. | |
| #define | HCI_DISABLE_ADV LL_ADV_MODE_OFF |
| Advertising Disable. | |
| #define | HCI_SCAN_PASSIVE LL_SCAN_PASSIVE |
| Passive Scan. | |
| #define | HCI_SCAN_ACTIVE LL_SCAN_ACTIVE |
| Active Scan. | |
| #define | HCI_SCAN_WL_POLICY_ANY_ADV_PKTS LL_SCAN_WL_POLICY_ANY_ADV_PKTS |
| Any Advertising Packets. | |
| #define | HCI_SCAN_WL_POLICY_USE_WHITE_LIST LL_SCAN_WL_POLICY_USE_WHITE_LIST |
| Use Whitelist. | |
| #define | HCI_FILTER_REPORTS_DISABLE LL_FILTER_REPORTS_DISABLE |
| Disable. | |
| #define | HCI_FILTER_REPORTS_ENABLE LL_FILTER_REPORTS_ENABLE |
| Enable. | |
| #define | HCI_SCAN_STOP LL_SCAN_STOP |
| Scan Stop. | |
| #define | HCI_SCAN_START LL_SCAN_START |
| Scan Start. | |
| #define | HCI_INIT_WL_POLICY_USE_PEER_ADDR LL_INIT_WL_POLICY_USE_PEER_ADDR |
| Use Peer Address. | |
| #define | HCI_INIT_WL_POLICY_USE_WHITE_LIST LL_INIT_WL_POLICY_USE_WHITE_LIST |
| Use Whitelist. | |
| #define | HCI_ENCRYPTION_OFF LL_ENCRYPTION_OFF |
| Off. | |
| #define | HCI_ENCRYPTION_ON LL_ENCRYPTION_ON |
| On. | |
| #define | HCI_DIRECT_TEST_PAYLOAD_PRBS9 LL_DIRECT_TEST_PAYLOAD_PRBS9 |
| PRBS9. | |
| #define | HCI_DIRECT_TEST_PAYLOAD_0x0F LL_DIRECT_TEST_PAYLOAD_0x0F |
| 0x0F | |
| #define | HCI_DIRECT_TEST_PAYLOAD_0x55 LL_DIRECT_TEST_PAYLOAD_0x55 |
| 0x55 | |
| #define | HCI_DIRECT_TEST_PAYLOAD_PRBS15 LL_DIRECT_TEST_PAYLOAD_PRBS15 |
| PRBS15. | |
| #define | HCI_DIRECT_TEST_PAYLOAD_0xFF LL_DIRECT_TEST_PAYLOAD_0xFF |
| 0xFF | |
| #define | HCI_DIRECT_TEST_PAYLOAD_0x00 LL_DIRECT_TEST_PAYLOAD_0x00 |
| 0x00 | |
| #define | HCI_DIRECT_TEST_PAYLOAD_0xF0 LL_DIRECT_TEST_PAYLOAD_0xF0 |
| 0xF0 | |
| #define | HCI_DIRECT_TEST_PAYLOAD_0xAA LL_DIRECT_TEST_PAYLOAD_0xAA |
| 0xAA | |
| #define | HCI_DTM_STANDARD_MODULATION_INDEX LL_DTM_STANDARD_MODULATION_INDEX |
| Standard Modulation. | |
| #define | HCI_DTM_STABLE_MODULATION_INDEX LL_DTM_STABLE_MODULATION_INDEX |
| Stable Modulation. | |
| #define | HCI_DISABLE_ADDR_RESOLUTION LL_DISABLE_ADDR_RESOLUTION |
| Disable. | |
| #define | HCI_ENABLE_ADDR_RESOLUTION LL_ENABLE_ADDR_RESOLUTION |
| Enable. | |
| #define | HCI_PHY_USE_PHY_PARAM LL_PHY_USE_PHY_PARAM |
| Use PHY specified by Phy Types. | |
| #define | HCI_PHY_USE_ANY_PHY LL_PHY_USE_ANY_PHY |
| Use any PHY. | |
| #define | HCI_PHY_1_MBPS LL_PHY_1_MBPS |
| 1 Mbps | |
| #define | HCI_PHY_2_MBPS LL_PHY_2_MBPS |
| 2 Mbps | |
| #define | HCI_EXT_RX_GAIN_STD LL_EXT_RX_GAIN_STD |
| Standard Gain. | |
| #define | HCI_EXT_RX_GAIN_HIGH LL_EXT_RX_GAIN_HIGH |
| High Gain. | |
| #define | HCI_EXT_TX_POWER_MINUS_23_DBM LL_EXT_TX_POWER_MINUS_23_DBM |
| -23 dBm | |
| #define | HCI_EXT_TX_POWER_MINUS_6_DBM LL_EXT_TX_POWER_MINUS_6_DBM |
| -6 dBm | |
| #define | HCI_EXT_TX_POWER_0_DBM LL_EXT_TX_POWER_0_DBM |
| 0 dBm | |
| #define | HCI_EXT_TX_POWER_4_DBM LL_EXT_TX_POWER_4_DBM |
| 4 dBm | |
| #define | HCI_EXT_ENABLE_ONE_PKT_PER_EVT LL_EXT_ENABLE_ONE_PKT_PER_EVT |
| Enable. | |
| #define | HCI_EXT_DISABLE_ONE_PKT_PER_EVT LL_EXT_DISABLE_ONE_PKT_PER_EVT |
| Disable. | |
| #define | HCI_EXT_ENABLE_CLK_DIVIDE_ON_HALT LL_EXT_ENABLE_CLK_DIVIDE_ON_HALT |
| Enable. | |
| #define | HCI_EXT_DISABLE_CLK_DIVIDE_ON_HALT LL_EXT_DISABLE_CLK_DIVIDE_ON_HALT |
| Disable. | |
| #define | HCI_EXT_NV_IN_USE LL_EXT_NV_IN_USE |
| NV in Use. | |
| #define | HCI_EXT_NV_NOT_IN_USE LL_EXT_NV_NOT_IN_USE |
| NV Not in Use. | |
| #define | HCI_EXT_ENABLE_FAST_TX_RESP_TIME LL_EXT_ENABLE_FAST_TX_RESP_TIME |
| Enable. | |
| #define | HCI_EXT_DISABLE_FAST_TX_RESP_TIME LL_EXT_DISABLE_FAST_TX_RESP_TIME |
| Disable. | |
| #define | HCI_EXT_ENABLE_SL_OVERRIDE LL_EXT_ENABLE_SL_OVERRIDE |
| Enable. | |
| #define | HCI_EXT_DISABLE_SL_OVERRIDE LL_EXT_DISABLE_SL_OVERRIDE |
| Disable. | |
| #define | HCI_EXT_TX_MODULATED_CARRIER LL_EXT_TX_MODULATED_CARRIER |
| Modulated. | |
| #define | HCI_EXT_TX_UNMODULATED_CARRIER LL_EXT_TX_UNMODULATED_CARRIER |
| Unmodulated. | |
| #define | HCI_PTM_SET_FREQ_TUNE_DOWN LL_EXT_SET_FREQ_TUNE_DOWN |
| Tune Down. | |
| #define | HCI_PTM_SET_FREQ_TUNE_UP LL_EXT_SET_FREQ_TUNE_UP |
| Tune Up. | |
| #define | HCI_EXT_PM_IO_PORT_P0 LL_EXT_PM_IO_PORT_P0 |
| #define | HCI_EXT_PM_IO_PORT_P1 LL_EXT_PM_IO_PORT_P1 |
| #define | HCI_EXT_PM_IO_PORT_P2 LL_EXT_PM_IO_PORT_P2 |
| #define | HCI_EXT_PM_IO_PORT_NONE LL_EXT_PM_IO_PORT_NONE |
| #define | HCI_EXT_PM_IO_PORT_PIN0 LL_EXT_PM_IO_PORT_PIN0 |
| #define | HCI_EXT_PM_IO_PORT_PIN1 LL_EXT_PM_IO_PORT_PIN1 |
| #define | HCI_EXT_PM_IO_PORT_PIN2 LL_EXT_PM_IO_PORT_PIN2 |
| #define | HCI_EXT_PM_IO_PORT_PIN3 LL_EXT_PM_IO_PORT_PIN3 |
| #define | HCI_EXT_PM_IO_PORT_PIN4 LL_EXT_PM_IO_PORT_PIN4 |
| #define | HCI_EXT_PM_IO_PORT_PIN5 LL_EXT_PM_IO_PORT_PIN5 |
| #define | HCI_EXT_PM_IO_PORT_PIN6 LL_EXT_PM_IO_PORT_PIN6 |
| #define | HCI_EXT_PM_IO_PORT_PIN7 LL_EXT_PM_IO_PORT_PIN7 |
| #define | HCI_EXT_PER_RESET LL_EXT_PER_RESET |
| Reset. | |
| #define | HCI_EXT_PER_READ LL_EXT_PER_READ |
| Read. | |
| #define | HCI_EXT_HALT_DURING_RF_DISABLE LL_EXT_HALT_DURING_RF_DISABLE |
| Disable. | |
| #define | HCI_EXT_HALT_DURING_RF_ENABLE LL_EXT_HALT_DURING_RF_ENABLE |
| Enable. | |
| #define | HCI_EXT_SET_USER_REVISION LL_EXT_SET_USER_REVISION |
| Set. | |
| #define | HCI_EXT_READ_BUILD_REVISION LL_EXT_READ_BUILD_REVISION |
| Read. | |
| #define | HCI_EXT_RESET_SYSTEM_HARD LL_EXT_RESET_SYSTEM_HARD |
| Hard Reset. | |
| #define | HCI_EXT_RESET_SYSTEM_SOFT LL_EXT_RESET_SYSTEM_SOFT |
| Soft Reset. | |
| #define | HCI_EXT_DISABLE_OVERLAPPED_PROCESSING LL_EXT_DISABLE_OVERLAPPED_PROCESSING |
| Disable. | |
| #define | HCI_EXT_ENABLE_OVERLAPPED_PROCESSING LL_EXT_ENABLE_OVERLAPPED_PROCESSING |
| Enable. | |
| #define | HCI_EXT_DISABLE_NUM_COMPL_PKTS_ON_EVENT LL_EXT_DISABLE_NUM_COMPL_PKTS_ON_EVENT |
| Disable. | |
| #define | HCI_EXT_ENABLE_NUM_COMPL_PKTS_ON_EVENT LL_EXT_ENABLE_NUM_COMPL_PKTS_ON_EVENT |
| Enable. | |
| #define | HCI_EXT_DISABLE_SCAN_REQUEST_REPORT LL_EXT_DISABLE_SCAN_REQUEST_REPORT |
| Disable. | |
| #define | HCI_EXT_ENABLE_SCAN_REQUEST_REPORT LL_EXT_ENABLE_SCAN_REQUEST_REPORT |
| Enable. | |
| #define | HCI_LINK_TYPE_SCO_BUFFER_OVERFLOW 0 |
| SCO Buffer Overflow. | |
| #define | HCI_LINK_TYPE_ACL_BUFFER_OVERFLOW 1 |
| ACL Buffer Overflow. | |
Typedefs | |
| typedef union _hciEvt_BLEConnComplete_u_ | hciEvt_BLEConnComplete_u |
| LE Connection Complete Event. | |
Functions | |
| uint8 | HCI_ValidConnTimeParams (uint16 connIntervalMin, uint16 connIntervalMax, uint16 connLatency, uint16 connTimeout) |
| This API is used to check that the connection time parameter ranges are valid, and that the connection time parameter combination is valid. It also checks if the min/max CI range is valid. More... | |
| void | HCI_TestAppTaskRegister (uint8 taskID) |
| HCI vendor specific registration for HCI Test Application. More... | |
| void | HCI_GAPTaskRegister (uint8 taskID) |
| HCI vendor specific registration for Host GAP. More... | |
| void | HCI_L2CAPTaskRegister (uint8 taskID) |
| HCI vendor specific registration for Host L2CAP. More... | |
| void | HCI_SMPTaskRegister (uint8 taskID) |
| HCI vendor specific registration for Host SMP. More... | |
| void | HCI_ExtTaskRegister (uint8 taskID) |
| HCI vendor specific registration for Host extended commands. More... | |
| hciStatus_t | HCI_SendDataPkt (uint16 connHandle, uint8 pbFlag, uint16 pktLen, uint8 *pData) |
| This API is used to send a ACL data packet over a connection. More... | |
| hciStatus_t | HCI_DisconnectCmd (uint16 connHandle, uint8 reason) |
| This BT API is used to terminate a connection. More... | |
| hciStatus_t | HCI_ReadRemoteVersionInfoCmd (uint16 connHandle) |
| This BT API is used to request version information from the the remote device in a connection. More... | |
| hciStatus_t | HCI_SetEventMaskCmd (uint8 *pMask) |
| This BT API is used to set the HCI event mask, which is used to determine which events are supported. More... | |
| hciStatus_t | HCI_SetEventMaskPage2Cmd (uint8 *pMask) |
| This BT API is used to set the HCI event mask page 2, which is used to determine which events are supported. More... | |
| hciStatus_t | HCI_ResetCmd (void) |
| Reset the Link Layer. More... | |
| hciStatus_t | HCI_ReadTransmitPowerLevelCmd (uint16 connHandle, uint8 txPwrType) |
| Read the transmit power level. More... | |
| hciStatus_t | HCI_SetControllerToHostFlowCtrlCmd (uint8 flowControlEnable) |
| This BT API is used by the Host to turn flow control on or off for data sent from the Controller to Host. Related Events: HCI_CommandCompleteEvent. More... | |
| hciStatus_t | HCI_HostBufferSizeCmd (uint16 hostAclPktLen, uint8 hostSyncPktLen, uint16 hostTotalNumAclPkts, uint16 hostTotalNumSyncPkts) |
| This BT API is used by the Host to notify the Controller of the maximum size ACL buffer size the Controller can send to the Host. More... | |
| hciStatus_t | HCI_HostNumCompletedPktCmd (uint8 numHandles, uint16 *connHandles, uint16 *numCompletedPkts) |
| This BT API is used by the Host to notify the Controller of the number of HCI data packets that have been completed for each connection handle since this command was previously sent to the controller. More... | |
| hciStatus_t | HCI_ReadAuthPayloadTimeoutCmd (uint16 connHandle, uint16 *aptoValue) |
| Read the connection's Authenticated Payload Timeout value. More... | |
| hciStatus_t | HCI_WriteAuthPayloadTimeoutCmd (uint16 connHandle, uint16 aptoValue) |
| Used to write the connection's Authenticated Payload Timeout value. More... | |
| hciStatus_t | HCI_ReadLocalVersionInfoCmd (void) |
| Read the local version information. More... | |
| hciStatus_t | HCI_ReadLocalSupportedCommandsCmd (void) |
| Read the locally supported commands. More... | |
| hciStatus_t | HCI_ReadLocalSupportedFeaturesCmd (void) |
| Read the locally supported features. More... | |
| hciStatus_t | HCI_ReadBDADDRCmd (void) |
| Read this device's BLE address (BDADDR). More... | |
| hciStatus_t | HCI_ReadRssiCmd (uint16 connHandle) |
| Read RSSI of last packet. More... | |
| hciStatus_t | HCI_LE_SetEventMaskCmd (uint8 *pEventMask) |
| This LE API is used to set the HCI LE event mask, which is used to determine which LE events are supported. More... | |
| hciStatus_t | HCI_LE_ReadBufSizeCmd (void) |
| This LE API is used by the Host to determine the maximum ACL data packet size allowed by the Controller. More... | |
| hciStatus_t | HCI_LE_ReadLocalSupportedFeaturesCmd (void) |
| Read the LE locally supported features. More... | |
| hciStatus_t | HCI_LE_SetRandomAddressCmd (uint8 *pRandAddr) |
| Set this device's Random address. More... | |
| hciStatus_t | HCI_LE_SetAdvParamCmd (uint16 advIntervalMin, uint16 advIntervalMax, uint8 advType, uint8 ownAddrType, uint8 directAddrType, uint8 *directAddr, uint8 advChannelMap, uint8 advFilterPolicy) |
| Set the Advertising parameters. More... | |
| hciStatus_t | HCI_LE_SetAdvDataCmd (uint8 dataLen, uint8 *pData) |
| Set the Advertising data. More... | |
| hciStatus_t | HCI_LE_SetScanRspDataCmd (uint8 dataLen, uint8 *pData) |
| Set the Advertising Scan Response data. More... | |
| hciStatus_t | HCI_LE_SetAdvEnableCmd (uint8 advEnable) |
| Turn Advertising on or off. More... | |
| hciStatus_t | HCI_LE_ReadAdvChanTxPowerCmd (void) |
| Read transmit power when Advertising. More... | |
| hciStatus_t | HCI_LE_SetScanParamCmd (uint8 scanType, uint16 scanInterval, uint16 scanWindow, uint8 ownAddrType, uint8 filterPolicy) |
| Set the Scan parameters. More... | |
| hciStatus_t | HCI_LE_SetScanEnableCmd (uint8 scanEnable, uint8 filterDuplicates) |
| Turn Scanning on or off. More... | |
| hciStatus_t | HCI_LE_CreateConnCmd (uint16 scanInterval, uint16 scanWindow, uint8 initFilterPolicy, uint8 addrTypePeer, uint8 *peerAddr, uint8 ownAddrType, uint16 connIntervalMin, uint16 connIntervalMax, uint16 connLatency, uint16 connTimeout, uint16 minLen, uint16 maxLen) |
| Create a connection. More... | |
| hciStatus_t | HCI_LE_CreateConnCancelCmd (void) |
| Cancel connection. More... | |
| hciStatus_t | HCI_LE_ReadWhiteListSizeCmd (void) |
| Read the white list. More... | |
| hciStatus_t | HCI_LE_ClearWhiteListCmd (void) |
| Clear the white list. More... | |
| hciStatus_t | HCI_LE_AddWhiteListCmd (uint8 addrType, uint8 *devAddr) |
| Add a white list entry. More... | |
| hciStatus_t | HCI_LE_RemoveWhiteListCmd (uint8 addrType, uint8 *devAddr) |
| Remove a white list entry. More... | |
| hciStatus_t | HCI_LE_ConnUpdateCmd (uint16 connHandle, uint16 connIntervalMin, uint16 connIntervalMax, uint16 connLatency, uint16 connTimeout, uint16 minLen, uint16 maxLen) |
| Update the connection parameters. More... | |
| hciStatus_t | HCI_LE_SetHostChanClassificationCmd (uint8 *chanMap) |
| Update the current data channel map. More... | |
| hciStatus_t | HCI_LE_ReadChannelMapCmd (uint16 connHandle) |
| Read a connection's data channel map. More... | |
| hciStatus_t | HCI_LE_ReadRemoteUsedFeaturesCmd (uint16 connHandle) |
| Read the remote device's used features. More... | |
| hciStatus_t | HCI_LE_EncryptCmd (uint8 *key, uint8 *plainText) |
| Perform an encryption using AES128. More... | |
| hciStatus_t | HCI_LE_RandCmd (void) |
| Generate a random number. More... | |
| hciStatus_t | HCI_LE_StartEncyptCmd (uint16 connHandle, uint8 *random, uint8 *encDiv, uint8 *ltk) |
| Start encryption in a connection. More... | |
| hciStatus_t | HCI_LE_LtkReqReplyCmd (uint16 connHandle, uint8 *ltk) |
| This LE API is used by the Host to send to the Controller a positive LTK reply. More... | |
| hciStatus_t | HCI_LE_LtkReqNegReplyCmd (uint16 connHandle) |
| This LE API is used by the Host to send to the Controller a negative LTK reply. More... | |
| hciStatus_t | HCI_LE_ReadSupportedStatesCmd (void) |
| Read the Controller's supported states. More... | |
| hciStatus_t | HCI_LE_ReceiverTestCmd (uint8 rxChan) |
| Start the receiver Direct Test Mode test. More... | |
| hciStatus_t | HCI_LE_TransmitterTestCmd (uint8 txChan, uint8 dataLen, uint8 pktPayload) |
| This LE API is used to start the transmit Direct Test Mode test. More... | |
| hciStatus_t | HCI_LE_TestEndCmd (void) |
| End the Direct Test Mode test. More... | |
| hciStatus_t | HCI_LE_RemoteConnParamReqReplyCmd (uint16 connHandle, uint16 connIntervalMin, uint16 connIntervalMax, uint16 connLatency, uint16 connTimeout, uint16 minLen, uint16 maxLen) |
| This LE API is used to positively reply to the HCI LE Remote Connection Parameter Request event from the Controller. This command indicates that the Host has accepted the remote device's request to change connection parameters. More... | |
| hciStatus_t | HCI_LE_RemoteConnParamReqNegReplyCmd (uint16 connHandle, uint8 reason) |
| Negatively reply to the Conneciton Parameter Update Request. More... | |
| hciStatus_t | HCI_LE_SetDataLenCmd (uint16 connHandle, uint16 txOctets, uint16 txTime) |
| Set Data Length. More... | |
| hciStatus_t | HCI_LE_ReadSuggestedDefaultDataLenCmd (void) |
| Read Suggested Default Data Length. More... | |
| hciStatus_t | HCI_LE_WriteSuggestedDefaultDataLenCmd (uint16 txOctets, uint16 txTime) |
| Write Suggested Default Data Length. More... | |
| hciStatus_t | HCI_LE_ReadMaxDataLenCmd (void) |
| Read max data length. More... | |
| hciStatus_t | HCI_LE_AddDeviceToResolvingListCmd (uint8 peerIdAddrType, uint8 *peerIdAddr, uint8 *peerIRK, uint8 *localIRK) |
| Add a device to the resolving list. More... | |
| hciStatus_t | HCI_LE_RemoveDeviceFromResolvingListCmd (uint8 peerIdAddrType, uint8 *peerIdAddr) |
| Remove a device from the whitelist. More... | |
| hciStatus_t | HCI_LE_ClearResolvingListCmd (void) |
| Remove all devices from the whitelist. More... | |
| hciStatus_t | HCI_LE_ReadResolvingListSizeCmd (void) |
| Read Resolving List Size. More... | |
| hciStatus_t | HCI_LE_ReadPeerResolvableAddressCmd (uint8 peerIdAddrType, uint8 *peerIdAddr) |
| Read the Peer Resolvable Address. More... | |
| hciStatus_t | HCI_LE_ReadLocalResolvableAddressCmd (uint8 localIdAddrType, uint8 *localIdAddr) |
| Read Local Resolvable Private Address. More... | |
| hciStatus_t | HCI_LE_SetAddressResolutionEnableCmd (uint8 addrResolutionEnable) |
| Disable / Enable Address Resolution. More... | |
| hciStatus_t | HCI_LE_SetResolvablePrivateAddressTimeoutCmd (uint16 rpaTimeout) |
| Set Resolvable Private Address Timeout. More... | |
| hciStatus_t | HCI_LE_ReadLocalP256PublicKeyCmd (void) |
| Read local P-256 Public Key. More... | |
| hciStatus_t | HCI_LE_GenerateDHKeyCmd (uint8 *publicKey) |
| Generate Diffie-Hellman Key. More... | |
| hciStatus_t | HCI_LE_ReadPhyCmd (uint16 connHandle) |
| Read the current transmitter and receiver PHY. More... | |
| hciStatus_t | HCI_LE_SetDefaultPhyCmd (uint8 allPhys, uint8 txPhy, uint8 rxPhy) |
| Set Default PHY. More... | |
| hciStatus_t | HCI_LE_SetPhyCmd (uint16 connHandle, uint8 allPhys, uint8 txPhy, uint8 rxPhy) |
| This LE API is used to request a change to the transmitter and receiver PHY for a connection. More... | |
| hciStatus_t | HCI_LE_EnhancedRxTestCmd (uint8 rxChan, uint8 rxPhy, uint8 modIndex) |
| Start Enhanced RX Test. More... | |
| hciStatus_t | HCI_LE_EnhancedTxTestCmd (uint8 txChan, uint8 payloadLen, uint8 payloadType, uint8 txPhy) |
| Start Enhanced TX Test. More... | |
| hciStatus_t | HCI_EXT_SetRxGainCmd (uint8 rxGain) |
| Set the receiver gain. More... | |
| hciStatus_t | HCI_EXT_SetTxPowerCmd (uint8 txPower) |
| Set the transmit power. More... | |
| hciStatus_t | HCI_EXT_OnePktPerEvtCmd (uint8 control) |
| This HCI Extension API is used to set whether a connection will be limited to one packet per event. More... | |
| hciStatus_t | HCI_EXT_ClkDivOnHaltCmd (uint8 control) |
| Set whether the system clock will be divided when the MCU is halted. More... | |
| hciStatus_t | HCI_EXT_DeclareNvUsageCmd (uint8 mode) |
| This HCI Extension API is used to indicate to the Controller whether or not the Host will be using the NV memory during BLE operations. More... | |
| hciStatus_t | HCI_EXT_DecryptCmd (uint8 *key, uint8 *encText) |
| This HCI Extension API is used to decrypt encrypted data using AES128. More... | |
| hciStatus_t | HCI_EXT_SetLocalSupportedFeaturesCmd (uint8 *localFeatures) |
| This HCI Extension API is used to write this device's supported features. More... | |
| hciStatus_t | HCI_EXT_SetFastTxResponseTimeCmd (uint8 control) |
| This HCI Extension API is used to set whether transmit data is sent as soon as possible even when slave latency is used. More... | |
| hciStatus_t | HCI_EXT_SetSlaveLatencyOverrideCmd (uint8 control) |
| This HCI Extension API is used to to enable or disable suspending slave latency. More... | |
| hciStatus_t | HCI_EXT_ModemTestTxCmd (uint8 cwMode, uint8 txChan) |
| This API is used start a continuous transmitter modem test, using either a modulated or unmodulated carrier wave tone, at the frequency that corresponds to the specified RF channel. Use HCI_EXT_EndModemTest command to end the test. More... | |
| hciStatus_t | HCI_EXT_ModemHopTestTxCmd (void) |
| Start Modem Hop Tx Test. More... | |
| hciStatus_t | HCI_EXT_ModemTestRxCmd (uint8 rxChan) |
| Start Modem Hop RX Test. More... | |
| hciStatus_t | HCI_EXT_EndModemTestCmd (void) |
| This API is used to shutdown a modem test. A complete Controller reset will take place. More... | |
| hciStatus_t | HCI_EXT_SetBDADDRCmd (uint8 *bdAddr) |
| This API is used to set this device's BLE address (BDADDR). More... | |
| hciStatus_t | HCI_EXT_SetSCACmd (uint16 scaInPPM) |
| This API is used to set this device's Sleep Clock Accuracy. More... | |
| hciStatus_t | HCI_EXT_EnablePTMCmd (void) |
| This HCI Extension API is used to enable Production Test Mode. More... | |
| hciStatus_t | HCI_EXT_SetFreqTuneCmd (uint8 step) |
| This HCI Extension API is used to set the frequency tuning up or down. Setting the mode up/down decreases/increases the amount of capacitance on the external crystal oscillator. More... | |
| hciStatus_t | HCI_EXT_SaveFreqTuneCmd (void) |
| This HCI Extension API is used to save the frequency tuning value to flash. More... | |
| hciStatus_t | HCI_EXT_SetMaxDtmTxPowerCmd (uint8 txPower) |
| This HCI Extension API is used to set the maximum transmit output power for Direct Test Mode. More... | |
| hciStatus_t | HCI_EXT_MapPmIoPortCmd (uint8 ioPort, uint8 ioPin) |
| This HCI Extension API is used to configure and map a CC254x I/O Port as a General Purpose I/O (GPIO) output signal that reflects the Power Management (PM) state of the CC254x device. The GPIO output will be High on Wake, and Low upon entering Sleep. This feature can be disabled by specifying HCI_EXT_PM_IO_PORT_NONE for the ioPort (ioPin is then ignored). The system default value upon hardware reset is disabled. This command can be used to control an external DC-DC Converter (its actual intent) such has the TI TPS62730 (or any similar converter that works the same way). This command should be used with extreme care as it will override how the Port/Pin was previously configured! This includes the mapping of Port 0 pins to 32kHz clock output, Analog I/O, UART, Timers; Port 1 pins to Observables, Digital Regulator status, UART, Timers; Port 2 pins to an external 32kHz XOSC. The selected Port/Pin will be configured as an output GPIO with interrupts masked. Careless use can result in a reconfiguration that could disrupt the system. It is therefore the user's responsibility to ensure the selected Port/Pin does not cause any conflicts in the system. More... | |
| hciStatus_t | HCI_EXT_DisconnectImmedCmd (uint16 connHandle) |
| This HCI Extension API is used to disconnect the connection immediately. More... | |
| hciStatus_t | HCI_EXT_PacketErrorRateCmd (uint16 connHandle, uint8 command) |
| This function is used to Reset or Read the Packet Error Rate counters for a connection. More... | |
| hciStatus_t | HCI_EXT_PERbyChanCmd (uint16 connHandle, perByChan_t *perByChan) |
| This HCI Extension API is used to start or end Packet Error Rate by Channel counter accumulation for a connection. If the pointer is not NULL, it is assumed there is sufficient memory for the PER data, per the type perByChan_t. If NULL, then the operation is considered disabled. More... | |
| hciStatus_t | HCI_EXT_ExtendRfRangeCmd (void) |
| This HCI Extension API is used to Extend Rf Range using the TI CC2590 2.4 GHz RF Front End device. More... | |
| hciStatus_t | HCI_EXT_HaltDuringRfCmd (uint8 mode) |
| Halt During RF Command. More... | |
| hciStatus_t | HCI_EXT_AdvEventNoticeCmd (uint8 taskID, uint16 taskEvent) |
| This HCI Extension API is used to enable or disable a notification to the specified task using the specified task event whenever a Adv event ends. A non-zero taskEvent value is taken to be "enable", while a zero valued taskEvent is taken to be "disable". More... | |
| hciStatus_t | HCI_EXT_ScanEventNoticeCmd (uint8 taskID, uint16 taskEvent) |
| Scan Event Notice Command. More... | |
| hciStatus_t | HCI_EXT_ConnEventNoticeCmd (uint16 connHandle, uint8 taskID, uint16 taskEvent) |
| This HCI Extension API is used to enable or disable a notification to the specified task using the specified task event whenever a Connection event ends. A non-zero taskEvent value is taken to be "enable", while a zero valued taskEvent taken to be "disable". More... | |
| hciStatus_t | HCI_EXT_BuildRevisionCmd (uint8 mode, uint16 userRevNum) |
| This HCI Extension API is used set a user revision number or read the build revision number. More... | |
| hciStatus_t | HCI_EXT_DelaySleepCmd (uint16 delay) |
| This HCI Extension API is used set the sleep delay. More... | |
| hciStatus_t | HCI_EXT_ResetSystemCmd (uint8 mode) |
| This HCI Extension API is used to issue a soft or hard system reset. More... | |
| hciStatus_t | HCI_EXT_LLTestModeCmd (uint8 testCase) |
| This HCI Extension API is used to send a LL Test Mode test case. More... | |
| hciStatus_t | HCI_EXT_OverlappedProcessingCmd (uint8 mode) |
| This HCI Extension API is used to enable or disable overlapped processing. More... | |
| hciStatus_t | HCI_EXT_NumComplPktsLimitCmd (uint8 limit, uint8 flushOnEvt) |
| This HCI Extension API is used to set the minimum number of completed packets which must be met before a Number of Completed Packets event is returned. If the limit is not reach by the end of the connection event, then a Number of Completed Packets event will be returned (if non-zero) based on the flushOnEvt flag. More... | |
| hciStatus_t | HCI_EXT_GetConnInfoCmd (uint8 *numAllocConns, uint8 *numActiveConns, hciConnInfo_t *activeConnInfo) |
| Get Connection Info. More... | |
| hciStatus_t | HCI_EXT_SetMaxDataLenCmd (uint16 txOctets, uint16 txTime, uint16 rxOctets, uint16 rxTime) |
| This LE API is used to set the maximum supported Rx and Tx Octets (in bytes) and Time (in us). More... | |
| hciStatus_t | HCI_EXT_ScanReqRptCmd (uint8 mode) |
| This LE API is used to enable/disable Scan Request Reports. More... | |
HCI layer interface.
End HCI_Function_Maps
1.8.12