SimpleLink™ CC13X0 SDK 4.20.01.03 Release Notes
Table of Contents
Introduction
The SimpleLink™ CC13x0 Software Development Kit (SDK) is part of the Texas Instruments SimpleLink family of wireless microcontrollers (MCUs), offering a single development environment that delivers flexible hardware, software and tool options for customers developing wired and wireless applications. For more information about the SimpleLink MCU platform, visit www.ti.com/simplelink.
SimpleLink™ CC13x0 Software Development Kit is a set of software development tools that enables engineers to develop software applications on the SimpleLink™ CC13x0 ULP devices. This powerful software toolkit provides a cohesive and consistent software experience for all SimpleLink™ CC13x0 users by packaging essential software components such as TI RTOS, peripheral drivers, TI 15.4-Stack, Bluetooth Low Energy, and RF-Proprietary examples in one easy-to-use software package along with exhaustive documentation.
This is version 4.20.01.03 of the SimpleLink CC13x0 SDK.
Documentation
What’s New
- Bugfix in the BLE-Stack and TI 15.4-Stack.
- Please refer to the Document Overview for the individual release notes and details for starting development with each SDK component
- SimpleLink platform level changes are available in SimpleLink Core SDK Release Notes
- SDK Change Log provides a list of all SDK component changes
Upgrade and Compatibility Information
If you are migrating from existing TI 15.4-Stack or Proprietary-RF examples, please review the SimpleLink™ CC13x0 SDK Migration Guide
Please ensure that you are using version 3.30.01.xx of the Linux Gateway SDK which is the latest compatible version for the CC13x0 SDK.
Operating System Support
- Windows 10
- Ubuntu 14.04 64-bit
- macOS Sierra
Dependencies
SimpleLink™ CC13x0 SDK 4.20.01.03 was built & tested on a Windows 7 host platform using the following Integrated Development Environment (IDE) and components. Using an IDE version or TI-RTOS version not listed below may result in compatibility issues with this SDK release.
- TI Code Composer Studio™:: 9.1.0
- IAR Embedded Workbench for Arm:: 8.32.2
- C Compiler for Arm: 18.12.2.LTS
- XDCTools: 3.51.03.28
- TI-RTOS for CC13XX: 4.20.05.01
Device Support
Development Board Support
Known Issues
- For all SDK components, the importing of IAR projects through dev.ti.com is currently unsupported.
Refer to the SDK Change Log for known issues of each of the SDK components.
- Please refer to the Document Overview for the individual release notes for details for each SDK component.
Versioning
This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.
M - Is incremented for the first release every year. 1 -> 2017, 2 -> 2018, and so on..
mm - indicates the specific quarter of the year the SDK was released. 10 -> Q1; 20 -> Q2; 30 -> Q3; 40 -> Q4