package ti.sysbios.hal

Contains Hardware Abstraction Layer (HAL) modules for the SYS/BIOS kernel

SYS/BIOS provides services for configuration and management of interrupts, cache, and timers. Unlike other SYS/BIOS services such as threading, these modules directly program aspects of a device's hardware and are grouped together in the Hardware Abstraction Layer (HAL) package. These modules provide services such as enabling and disabling interrupts, plugging of interrupt vectors, multiplexing of multiple interrupts to a single vector, and cache invalidation or writeback. [ more ... ]
XDCspec declarations sourced in ti/sysbios/hal/package.xdc
requires ti.sysbios.family;
 
package ti.sysbios.hal [2, 0, 0, 0] {
 
    module Cache;
    // Cache Manager Proxy
    module CacheNull;
    // Null Cache module
    module Core;
    // "Global Proxy" for target specific Core implementations
    module CoreNull;
    // Null ICore implementation for default BIOS CoreDelegate
    module Hwi;
    // Hardware Interrupt Manager Proxy
    module Power;
    // Power Manager Proxy
    module PowerNull;
    module Seconds;
    // Seconds Manager
    module SecondsCallback;
    // A Seconds module that calls user-supplied callbacks
    module SecondsClock;
    // Seconds module that uses Clock as its' time base
    module Timer;
    // Timer Manager Proxy
    module TimerNull;
    // Null Timer module
}
DETAILS
SYS/BIOS provides services for configuration and management of interrupts, cache, and timers. Unlike other SYS/BIOS services such as threading, these modules directly program aspects of a device's hardware and are grouped together in the Hardware Abstraction Layer (HAL) package. These modules provide services such as enabling and disabling interrupts, plugging of interrupt vectors, multiplexing of multiple interrupts to a single vector, and cache invalidation or writeback.
The HAL APIs fall into two categories:
  • Generic APIs that are available across all targets and devices.
  • Target/device-specific APIs that are available only for a specific device or ISA family
The generic APIs are designed to cover the great majority of use cases. If you are concerned with easy portability between different TI devices, you should use the generic APIs as much as possible. However, if the generic APIs cannot enable use of a device-specific hardware feature that is advantageous to the software application, you may choose to use the target/device-specific APIs.
The ti.sysbios.hal.Hwi, ti.sysbios.hal.Timer, and ti.sysbios.hal.Cache modules require target/device-specific API implementations to achieve their functionality. To provide a common set of APIs for these modules across all supported families/devices, SYS/BIOS uses the RTSC proxy-delegate module mechanism. That is, each of these modules serves as a proxy for a corresponding target/device-specific module implementation.
During the configuration step of the application build, the modules in the ti.sysbios.hal package locate and bind themselves to appropriate delegate module implementations based on the current target and platform specified in your config.bld file. The delegate binding process is done internally.
For example, if your config.bld file specifies that one of your build targets is the C64P family, the ti.sysbios.hal.Hwi knows to bind itself to the ti.sysbios.family.c64p.Hwi implementation.
generated on Fri, 22 Jan 2021 10:16:22 GMT