Terms and acronyms

General Terms and Acronyms

BIM
Boot Image Manager, the software bootloader
CCA
CCFG
Customer Configuration Area, contains lock-bits on flash page 31 and the Customer Configuration Table (.ccfg)
CCS
Code Composer Studio
IAR
IAR Systems
MCU
Microcontroller Unit
OAD
Over the Air Download
RCFG
TI-RTOS in ROM Configuration Table
ROM
Read-only Memory
SNV
Simple Non-Volatile storage
SNP
Simple Network Processor, a BLE network processor implementation that supports the peripheral and broadcaster GAP Roles.
AP
Application Processor, the host MCU that implements the user application. Connected to a network processor via a serial interface such as NPI
UNPI
Unified Network Processor Interface, a standardized serial transport format that is implemented by TI for the purposes of interfacing to network processor devices like the SNP. UNPI also manages the handshaking required for the serial interface.
cJTAG
Class 4 IEEE 1149.7: Standard for Reduced-pin and Enhanced-functionality Test Access Port and Boundary-scan Architecture. This is known by acronym cJTAG (compact JTAG).
JTAG
IEEE standard 1149.1: Standard Test Access Port and Boundary Scan Architecture Test Access Port (TAP). This standard is known by the acronym JTAG (Joint Test Action Group).

Bluetooth Low Energy Terms and Acronyms

BLE
Bluetooth Low Energy
CCCD
Client Characteristic Configuration Descriptor
L2CAP
Link Logical Control and Adaption Protocol
HCI
Host Control Interface
BR
Basic Rate
BR/EDR
Basic Rate/Enhanced Data Rate
LE
Low Energy
PHY
Physical Layer
GFSK
Gaussian Frequency-Shift Keying
ISM
Industrial, Scientific, and Medical
LL
Link Layer
GAP
Generic Access Protocol

TI-RTOS Terms and Acronyms

HWI
Hardware Interrupts
A TI-RTOS hardware interrupt.
Idle Task
A TI-RTOS default task that is executes when no other higher priority thread needs to run.
RCFG
TI-RTOS in ROM configuration table.
ROV
Runtime Object View
A TI-RTOS kernel plugin for CCS and IAR to view a target’s instrumentation data.
RTC
Real-Time Clock
An accurate computer clock which keeps track of the current time.
RTOS
Real Time Operating System
An operating system intended to serve applications with real-time requirements.
SWI
Software Interrupts
A TI-RTOS software interrupt.
TI-RTOS
Texas Instruments Real Time Operating System
An RTOS developed by TI for TI microcontrollers.
Zero-Latency Interrupts
An interrupt that will not be routed through the TI-RTOS kernel’s Hwi dispatcher. For more information, see the Hwi module documentation in the TI-RTOS Kernel (SYS/BIOS) User’s Guide.

Over the Air Download (OAD) Terms and Acronyms

BIM
Boot Image Manager
OAD
Over the Air Download
CCCD
Client Characteristic Configuration Descriptor
OAD Target

The device whose firmware is being upgraded over the air. This is assumed to be a CC26xx device running the TI OAD service.

OAD Target App also refers to the Image A project for on-chip OAD applications

OAD Downloader
The device responsible for accepting an OAD enabled image from the compiler and transferring it over the air to the OAD target.
SNV
Simple Non Volatile. An abstraction layer used by the BLE stack for reading and writing to non volatile memory. The GAPBondMgr layer of stack uses SNV to store keys. This region can also be used by the user.

Sensor Controller Terms and Acronyms

SC
Sensor Controller
A dedicated 16-bit CPU core on CC13xx and CC26xx devices, located in the auxiliary (AUX) power/clock domain. It can perform simple background tasks autonomously and independently of the System CPU and the MCU domain power states.
SCS
Sensor Controller Studio
A stand-alone IDE used to write, test and debug code for the Sensor Controller.