1    /* 
     2     *  Copyright (c) 2008 Texas Instruments. All rights reserved.
     3     *  This program and the accompanying materials are made available under the
     4     *  terms of the Eclipse Public License v1.0 and Eclipse Distribution License
     5     *  v. 1.0 which accompanies this distribution. The Eclipse Public License is
     6     *  available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
     7     *  Distribution License is available at
     8     *  http://www.eclipse.org/org/documents/edl-v10.php.
     9     *
    10     *  Contributors:
    11     *      Texas Instruments - initial implementation
    12     * */
    13    /*
    14     *  ======== IGateProvider.xdc ========
    15     */
    16    package xdc.runtime
    17    
    18    /*!
    19     *  ======== IGateProvider ========
    20     *  Interface implemented by all gate providers
    21     *
    22     *  Gates are used within the `xdc.runtime` package to serialize access
    23     *  to data structures that are used by more than one thread.
    24     *
    25     *  Gates are responsible for ensuring that only one out of multiple threads
    26     *  can access a data structure at a time.  There are important scheduling
    27     *  latency and performance considerations that affect the "type" of gate used
    28     *  to protect each data structure.  For example, the best way to protect a
    29     *  shared counter is to simply disable all interrupts before the update and
    30     *  restore the interrupt state after the update; disabling all interrupts
    31     *  prevents all thread switching, so the update is guaranteed to be "atomic".
    32     *  Although highly efficient, this  method of creating atomic sections causes
    33     *  serious system latencies when the time required to update the data structure
    34     *  can't be bounded.
    35     *
    36     *  For example, a memory manager's list of free blocks can grow indefinitely
    37     *  long during periods of high fragmentation.  Searching such a list with
    38     *  interrupts disabled would cause system latencies to also become unbounded.
    39     *  In this case, the best solution is to provide a gate that suspends the
    40     *  execution of  threads that try to enter a gate that has already been
    41     *  entered; i.e., the gate "blocks" the thread until the thread already in the
    42     *  gate leaves.  The time required to enter and leave the gate is greater than
    43     *  simply enabling and restoring interrupts, but since the time spent within
    44     *  the gate is relatively large, the overhead caused by entering and leaving
    45     *  gates will not become a significant percentage of overall system time.  More
    46     *  importantly, threads that do not need to access the shared data structure
    47     *  are completely unaffected by threads that do access it.
    48     *
    49     *  @a(Notes)
    50     *  Modules inheriting this interface should treat all names beginning with
    51     *  `Q_` as reserved words, i.e. the names from that namespace should not
    52     *  be used.  This will allow future version of this interface to define new
    53     *  constants ("qualities" ) similar to `{@link #Q_BLOCKING}` and
    54     *  `{@link #Q_PREEMPTING}` without breaking any existing modules.
    55     */
    56    @DirectCall
    57    interface IGateProvider {
    58    
    59        /*!
    60         *  ======== Q_BLOCKING ========
    61         *  Blocking quality
    62         *
    63         *  Gates with this "quality" may cause the calling thread to block; 
    64         *  i.e., suspend execution until another thread leaves the gate.
    65         */
    66        const Int Q_BLOCKING = 1;
    67    
    68        /*!
    69         *  ======== Q_PREEMPTING ========
    70         *  Preempting quality
    71         *
    72         *  Gates with this "quality" allow other threads to preempt the thread
    73         *  that has already entered the gate.
    74         */
    75        const Int Q_PREEMPTING = 2;
    76    
    77        /*!
    78         *  ======== query ========
    79         *  Configuration time test for a particular gate quality
    80         *
    81         *  @param(qual)    constant describing a quality
    82         *  @a(returns)     Returns `TRUE` if the gate has the given quality,
    83         *  and `FALSE` otherwise, which includes the case when the gate does not
    84         *  recognize the constant describing the quality.
    85         */
    86        metaonly Bool queryMeta(Int qual);
    87    
    88        /*!
    89         *  ======== query ========
    90         *  Runtime test for a particular gate quality
    91         *
    92         *  @param(qual)    constant describing a quality
    93         *  @a(returns)     Returns `TRUE` if the gate has the given quality,
    94         *  and `FALSE` otherwise, which includes the case when the gate does not
    95         *  recognize the constant describing the quality.
    96         */
    97        Bool query(Int qual);
    98    
    99    instance:
   100    
   101        /*!
   102         *  ======== create ========
   103         *  Create a gate instance
   104         */
   105        create();
   106    
   107        /*!
   108         *  ======== enter ========
   109         *  Enter this gate
   110         *
   111         *  Each gate provider can implement mutual exclusion using different
   112         *  algorithms; e.g., disabling all scheduling, disabling the scheduling
   113         *  of all threads below a specified "priority level", suspending the
   114         *  caller when the gate has been entered by another thread and
   115         *  re-enabling it when the the other thread leaves the gate.  However,
   116         *  in all cases, after this method returns that caller has exclusive
   117         *  access to the data protected by this gate.
   118         *
   119         *  A thread may reenter a gate without blocking or failing.
   120         *
   121         *  @a(returns)
   122         *  Returns a "key" that is used to `{@link #leave}` this gate; this 
   123         *  value is used to restore thread preemption to the state that
   124         *  existed just prior to entering this gate.
   125         */
   126        IArg enter();
   127    
   128        /*!
   129         *  ======== leave ========
   130         *  Leave this gate
   131         *
   132         *  This method is only called by threads that have previously entered 
   133         *  this gate via `{@link #enter}`.  After this method returns, the
   134         *  caller must not access the data structure protected by this gate
   135         *  (unless the caller has entered the gate more than once and other
   136         *  calls to `leave` remain to balance the number of previous
   137         *  calls to `enter`).
   138         *
   139         *  @param(key) the value returned by a matching call to
   140         *              `{@link #enter}`
   141         */
   142        Void leave(IArg key);
   143    }
   144    /*
   145     *  @(#) xdc.runtime; 2, 1, 0,0; 11-8-2017 17:11:26; /db/ztree/library/trees/xdc/xdc-D20.1/src/packages/
   146     */
   147