rfCarrierWave Example
Example Summary
The carrier wave (CW) example sends a continuous carrier wave or pseudo-random modulated signal on a fixed frequency. The frequency and other RF settings can be modified using SmartRF Studio.
Peripherals Exercised
N/A
System Confirguration Tool (SysConfig) Setup
Driver Configuration
RF- RF Driver Configuration- Hardware Used -
RF Antenna Switch
- Hardware Used -
Power- Power Manager Configuration- Default options used
Resources & Jumper Settings
If you’re using an IDE (such as CCS or IAR), please refer to Board.html in your project directory for resources used and board-specific jumper settings. Otherwise, you can find Board.html in the directory <SDK_INSTALL_DIR>/source/ti/boards/<BOARD>.
Board Specific Settings
- The default frequency is:
- 433.92 MHz for the CC1350-LAUNCHXL-433
- 433.92/490 MHz for the CC1352P-4-LAUNCHXL
- 2440 MHz on the CC2640R2-LAUNXHL
- 868.0 MHz for other launchpads In order to change frequency, modify the smartrf_settings.c file. This can be done using the code export feature in Smart RF Studio, or directly in the file
- On the CC1352P1 the high PA is enabled (high output power) for all Sub-1 GHz modes by default.
- On the CC1352P-2 the high PA operation for Sub-1 GHz modes is not supported
- On the CC1352P-4 the high PA is enabled (high output power) for all Sub-1 GHz modes by default.
- The center frequency for 2-GFSK is set to 490 MHz
- CAUTION: The center frequency for SimpleLink long range (SLR) is set to 433.92 MHz, but the high output power violates the maximum power output requirement for this band
- The CC2640R2 is setup to run all proprietary physical modes at a center frequency of 2440 MHz, at a data rate of 250 Kbps
Example Usage
Run the example.
Application Design Details
This examples consists of a single task and the exported SmartRF Studio radio settings.
To switch between carrier wave (1) and modulated signal (0) set the following in the code (CW is set as default):
RF_cmdTxTest.config.bUseCw = 1; // CW
RF_cmdTxTest.config.bUseCw = 0; // modulated signal
In order to achieve +14 dBm output power, make sure that the define CCFG_FORCE_VDDR_HH = 0x1 in ccfg.c. This requirement holds for CC13x2P boards when using the default PA.
When the task is executed it:
- Configures the radio for Proprietary mode
- Explicitly configures CW (1) or Modulated (0). Default modulated mode is PRBS-15
- Gets access to the radio via the RF drivers RF_open
- Sets up the radio using CMD_PROP_RADIO_DIV_SETUP command
- Sets the frequency using CMD_FS command
- Sends the CMD_TX_TEST command to start sending the CW or Pseudo-random signal forever
Note for IAR users: When using the CC1310DK, the TI XDS110v3 USB Emulator must be selected. For the CC1310_LAUNCHXL, select TI XDS110 Emulator. In both cases, select the cJTAG interface.