174 #ifndef ti_drivers_watchdog_WatchdogCC26XX__include 175 #define ti_drivers_watchdog_WatchdogCC26XX__include 213 #include <ti/drivers/dpl/HwiP.h> enum Watchdog_ResetMode_ Watchdog_ResetMode
Watchdog reset mode settings.
void(* Watchdog_Callback)(uintptr_t handle)
Watchdog callback pointer.
Definition: Watchdog.h:274
unsigned int baseAddr
Definition: WatchdogCC26XX.h:222
Watchdog driver interface.
Watchdog hardware attributes for CC26XX.
Definition: WatchdogCC26XX.h:221
Watchdog_Callback callbackFxn
Definition: WatchdogCC26XX.h:233
bool isOpen
Definition: WatchdogCC26XX.h:232
Watchdog Object for CC26XX.
Definition: WatchdogCC26XX.h:231
unsigned long reloadValue
Definition: WatchdogCC26XX.h:223
The definition of a Watchdog function table that contains the required set of functions to control a ...
Definition: Watchdog.h:347
Watchdog_ResetMode resetMode
Definition: WatchdogCC26XX.h:235
const Watchdog_FxnTable WatchdogCC26XX_fxnTable
Watchdog function table for CC26XX.
Watchdog_DebugMode debugStallMode
Definition: WatchdogCC26XX.h:237
struct WatchdogCC26XX_Object WatchdogCC26XX_Object
Watchdog Object for CC26XX.
enum Watchdog_DebugMode_ Watchdog_DebugMode
Watchdog debug stall settings.
struct WatchdogCC26XX_HWAttrs WatchdogCC26XX_HWAttrs
Watchdog hardware attributes for CC26XX.
HwiP_Struct hwi
Definition: WatchdogCC26XX.h:240