55 #ifndef ti_drivers_TRNG_TRNGCC26X0__include 56 #define ti_drivers_TRNG_TRNGCC26X0__include 69 #include <ti/drivers/dpl/HwiP.h> 70 #include <ti/drivers/dpl/SwiP.h> 71 #include <ti/drivers/dpl/SemaphoreP.h> enum TRNG_ReturnBehavior_ TRNG_ReturnBehavior
The way in which TRNG function calls return after generating the requested entropy.
The CryptoKey type is an opaque representation of a cryptographic key.
int_fast16_t returnStatus
Definition: TRNGCC26X0.h:108
uint8_t * entropyBuffer
Definition: TRNGCC26X0.h:113
CryptoKey datastructure.
Definition: CryptoKey.h:210
CryptoKey * entropyKey
Definition: TRNGCC26X0.h:114
uint32_t swiPriority
TRNG SWI priority. The higher the number, the higher the priority. The minimum is 0 and the maximum i...
Definition: TRNGCC26X0.h:98
TRNG_ReturnBehavior returnBehavior
Definition: TRNGCC26X0.h:109
TRNGCC26XX Object.
Definition: TRNGCC26X0.h:106
uint8_t intPriority
Crypto Peripheral's interrupt priority.
Definition: TRNGCC26X0.h:92
uint32_t semaphoreTimeout
Definition: TRNGCC26X0.h:112
size_t entropyGenerated
Definition: TRNGCC26X0.h:110
bool isOpen
Definition: TRNGCC26X0.h:107
SwiP_Struct callbackSwi
Definition: TRNGCC26X0.h:116
TRNGCC26X0 Hardware Attributes.
Definition: TRNGCC26X0.h:79
struct TRNGCC26X0_HWAttrs TRNGCC26X0_HWAttrs
TRNGCC26X0 Hardware Attributes.
void(* TRNG_CallbackFxn)(TRNG_Handle handle, int_fast16_t returnValue, CryptoKey *entropy)
The definition of a callback function used by the TRNG driver when used in TRNG_RETURN_BEHAVIOR_CALLB...
Definition: TRNG.h:467
TRNG_CallbackFxn callbackFxn
Definition: TRNGCC26X0.h:115
struct TRNGCC26X0_Object TRNGCC26X0_Object
TRNGCC26XX Object.
size_t entropyRequested
Definition: TRNGCC26X0.h:111