595 #ifndef ti_drivers_spi_SPICC26XXDMA__include 596 #define ti_drivers_spi_SPICC26XXDMA__include 609 #include <ti/drivers/dpl/HwiP.h> 610 #include <ti/drivers/dpl/SemaphoreP.h> 611 #include <ti/drivers/dpl/SwiP.h> 644 #define SPICC26XXDMA_CMD_RETURN_PARTIAL_ENABLE (SPI_CMD_RESERVED + 0) 653 #define SPICC26XXDMA_CMD_RETURN_PARTIAL_DISABLE (SPI_CMD_RESERVED + 1) 661 #define SPICC26XXDMA_CMD_SET_CSN_PIN (SPI_CMD_RESERVED + 2) 665 #define SPICC26XXDMA_RETURN_PARTIAL_ENABLE SPICC26XXDMA_CMD_RETURN_PARTIAL_ENABLE 666 #define SPICC26XXDMA_RETURN_PARTIAL_DISABLE SPICC26XXDMA_CMD_RETURN_PARTIAL_DISABLE 667 #define SPICC26XXDMA_SET_CSN_PIN SPICC26XXDMA_CMD_SET_CSN_PIN Definition: SPICC26XXDMA.h:687
uint8_t PIN_Id
Pin identifier data type.
Definition: PIN.h:577
PIN_Id csnPin
Definition: SPICC26XXDMA.h:824
const SPI_FxnTable SPICC26XXDMA_fxnTable
uint16_t defaultTxBufValue
Definition: SPICC26XXDMA.h:773
uint32_t baseAddr
Definition: SPICC26XXDMA.h:747
void(* SPI_CallbackFxn)(SPI_Handle handle, SPI_Transaction *transaction)
The definition of a callback function used by the SPI driver when used in SPI_MODE_CALLBACK.
Definition: SPI.h:569
enum SPI_Mode_ SPI_Mode
Definitions for various SPI modes of operation.
Power_NotifyObj spiPostObj
Definition: SPICC26XXDMA.h:843
unsigned int bitRate
SPI bit rate in Hz.
Definition: SPICC26XXDMA.h:808
A SPI_Transaction data structure is used with SPI_transfer(). It indicates how many SPI_FrameFormat f...
Definition: SPI.h:548
SPI_CallbackFxn transferCallbackFxn
Definition: SPICC26XXDMA.h:800
struct SPICC26XXDMA_Object * SPICC26XXDMA_Handle
uint32_t minDmaTransferSize
Definition: SPICC26XXDMA.h:788
uint8_t intPriority
SPI CC26XXDMA Peripheral's interrupt priority.
Definition: SPICC26XXDMA.h:763
uint32_t rxChannelBitMask
Definition: SPICC26XXDMA.h:775
void * spiPreFxn
Definition: SPICC26XXDMA.h:840
UDMACC26XX Global configuration.
Definition: UDMACC26XX.h:231
uint32_t txChannelBitMask
Definition: SPICC26XXDMA.h:777
uint16_t scratchBuf
Definition: SPICC26XXDMA.h:837
Power manager interface for CC26XX/CC13XX.
Power notify object structure.
Definition: Power.h:121
PIN_Id clkPin
Definition: SPICC26XXDMA.h:783
SPICC26XXDMA Hardware attributes.
Definition: SPICC26XXDMA.h:745
volatile bool spiPowerConstraint
Definition: SPICC26XXDMA.h:845
PIN_Id misoPin
Definition: SPICC26XXDMA.h:781
SPI_TransferMode transferMode
Definition: SPICC26XXDMA.h:798
SPICC26XXDMA Object.
Definition: SPICC26XXDMA.h:796
enum SPI_TransferMode_ SPI_TransferMode
SPI transfer mode determines the whether the SPI controller operates synchronously or asynchronously...
Device-specific pin & GPIO driver for CC26xx family [def].
The definition of a SPI function table that contains the required set of functions to control a speci...
Definition: SPI.h:683
void * spiPostFxn
Definition: SPICC26XXDMA.h:841
PIN_State pinState
Definition: SPICC26XXDMA.h:827
SPI_Mode mode
Definition: SPICC26XXDMA.h:801
SPICC26XXDMA_FrameSize
Definition: SPICC26XXDMA.h:686
SPICC26XXDMA_FrameSize frameSize
Definition: SPICC26XXDMA.h:821
UDMACC26XX driver implementation.
bool returnPartial
Definition: SPICC26XXDMA.h:834
struct SPICC26XXDMA_Object SPICC26XXDMA_Object
SPICC26XXDMA Object.
struct SPICC26XXDMA_HWAttrsV1 SPICC26XXDMA_HWAttrsV1
SPICC26XXDMA Hardware attributes.
PIN_Id csnPin
Definition: SPICC26XXDMA.h:785
UDMACC26XX_Handle udmaHandle
Definition: SPICC26XXDMA.h:831
uint8_t intNum
Definition: SPICC26XXDMA.h:749
PIN_Id mosiPin
Definition: SPICC26XXDMA.h:779
unsigned int transferTimeout
Definition: SPICC26XXDMA.h:799
underlying data structure for type PIN_State
Definition: PIN.h:707
enum SPI_FrameFormat_ SPI_FrameFormat
Definitions for various SPI data frame formats.
HwiP_Struct hwi
Definition: SPICC26XXDMA.h:813
SPI_FrameFormat frameFormat
Definition: SPICC26XXDMA.h:810
Power_NotifyObj spiPreObj
Definition: SPICC26XXDMA.h:842
SemaphoreP_Struct transferComplete
Definition: SPICC26XXDMA.h:815
SwiP_Struct swi
Definition: SPICC26XXDMA.h:814
size_t amtDataXferred
Definition: SPICC26XXDMA.h:819
bool isOpen
Definition: SPICC26XXDMA.h:847
uint32_t swiPriority
SPI SWI priority. The higher the number, the higher the priority. The minimum is 0 and the maximum is...
Definition: SPICC26XXDMA.h:769
Definition: SPICC26XXDMA.h:688
PowerCC26XX_Resource powerMngrId
Definition: SPICC26XXDMA.h:771
size_t currentXferAmt
Definition: SPICC26XXDMA.h:820
PIN_Handle pinHandle
Definition: SPICC26XXDMA.h:828
unsigned int dataSize
Definition: SPICC26XXDMA.h:809
SPI_Transaction * currentTransaction
Definition: SPICC26XXDMA.h:818