106 #ifndef ti_drivers_ecdh_ECDHCC26X2__include 107 #define ti_drivers_ecdh_ECDHCC26X2__include 121 #include <ti/devices/DeviceFamily.h> 122 #include DeviceFamily_constructPath(driverlib/pka.h) 124 #include <ti/drivers/dpl/HwiP.h> 125 #include <ti/drivers/dpl/SwiP.h> 126 #include <ti/drivers/dpl/SemaphoreP.h> 129 #define ECDHCC26X2_STATUS_FSM_RUN_PKA_OP ECDH_STATUS_RESERVED - 0 131 #define ECDHCC26X2_STATUS_FSM_RUN_FSM ECDH_STATUS_RESERVED - 1 Definition: ECDHCC26X2.h:145
Definition: ECDHCC26X2.h:160
The CryptoKey type is an opaque representation of a cryptographic key.
Definition: ECDHCC26X2.h:143
uint32_t swiPriority
ECC SWI priority. The higher the number, the higher the priority. The minimum is 0 and the maximum is...
Definition: ECDHCC26X2.h:190
uint32_t resultAddress
Definition: ECDHCC26X2.h:207
Definition: ECDHCC26X2.h:162
Definition: ECDHCC26X2.h:147
Definition: ECDHCC26X2.h:152
ECDHCC26X2_FsmState fsmState
Definition: ECDHCC26X2.h:205
Definition: ECDHCC26X2.h:151
ECDH_ReturnBehavior returnBehavior
Definition: ECDHCC26X2.h:202
struct ECDHCC26X2_Object_ ECDHCC26X2_Object
ECDHCC26X2 Object.
SwiP_Struct callbackSwi
Definition: ECDHCC26X2.h:208
ECDH_CallbackFxn callbackFxn
Definition: ECDHCC26X2.h:201
void(* ECDH_CallbackFxn)(ECDH_Handle handle, int_fast16_t returnStatus, ECDH_Operation operation, ECDH_OperationType operationType)
The definition of a callback function used by the ECDH driver when used in ECDH_RETURN_BEHAVIOR_CALLB...
Definition: ECDH.h:572
Definition: ECDHCC26X2.h:156
ECDH_Operation operation
Definition: ECDHCC26X2.h:203
ECDHCC26X2 Hardware Attributes.
Definition: ECDHCC26X2.h:171
TI Driver for Elliptic Curve Diffie-Hellman key agreement scheme.
Union containing pointers to all supported operation structs.
Definition: ECDH.h:541
Definition: ECDHCC26X2.h:155
enum ECDH_OperationType_ ECDH_OperationType
Enum for the operation types supported by the driver.
bool isOpen
Definition: ECDHCC26X2.h:199
Definition: ECDHCC26X2.h:146
Definition: ECDHCC26X2.h:157
ECDHCC26X2_FsmState_
ECDHCC26X2 states.
Definition: ECDHCC26X2.h:142
Definition: ECDHCC26X2.h:150
uint8_t intPriority
Crypto Peripheral's interrupt priority.
Definition: ECDHCC26X2.h:184
Definition: ECDHCC26X2.h:153
Definition: ECDHCC26X2.h:161
uint32_t semaphoreTimeout
Definition: ECDHCC26X2.h:206
ECDH_OperationType operationType
Definition: ECDHCC26X2.h:204
Definition: ECDHCC26X2.h:148
ECDHCC26X2 Object.
Definition: ECDHCC26X2.h:198
struct ECDHCC26X2_HWAttrs_ ECDHCC26X2_HWAttrs
ECDHCC26X2 Hardware Attributes.
int_fast16_t returnValue
Definition: ECDHCC26X2.h:200
enum ECDHCC26X2_FsmState_ ECDHCC26X2_FsmState
ECDHCC26X2 states.
Definition: ECDHCC26X2.h:158
enum ECDH_ReturnBehavior_ ECDH_ReturnBehavior
The way in which ECC function calls return after performing an encryption + authentication or decrypt...