371 #ifndef ti_drivers_uart_UARTCC26XX__include 372 #define ti_drivers_uart_UARTCC26XX__include 386 #include <ti/devices/DeviceFamily.h> 387 #include DeviceFamily_constructPath(driverlib/uart.h) 389 #include <ti/drivers/dpl/HwiP.h> 390 #include <ti/drivers/dpl/SwiP.h> 391 #include <ti/drivers/dpl/ClockP.h> 392 #include <ti/drivers/dpl/SemaphoreP.h> 425 #define UARTCC26XX_CMD_RETURN_PARTIAL_ENABLE (UART_CMD_RESERVED + 0) 434 #define UARTCC26XX_CMD_RETURN_PARTIAL_DISABLE (UART_CMD_RESERVED + 1) 442 #define UARTCC26XX_CMD_RX_FIFO_FLUSH (UART_CMD_RESERVED + 2) 446 #define UARTCC26XX_FIFO_SIZE 32 467 #define UARTCC26XX_RETURN_PARTIAL_ENABLE UARTCC26XX_CMD_RETURN_PARTIAL_ENABLE 468 #define UARTCC26XX_RETURN_PARTIAL_DISABLE UARTCC26XX_CMD_RETURN_PARTIAL_DISABLE uint8_t rtsPin
Definition: UARTCC26XX.h:555
UARTCC26XX Hardware attributes.
Definition: UARTCC26XX.h:529
UART_Mode readMode
Definition: UARTCC26XX.h:586
UARTCC26XX_FifoThreshold
UART TX/RX interrupt FIFO threshold select.
Definition: UARTCC26XX.h:454
Definition: UARTCC26XX.h:570
Power_NotifyObj uartPostObj
Definition: UARTCC26XX.h:628
uint32_t baudRate
Baud rate for CC26xx UART.
Definition: UARTCC26XX.h:602
const void * writeBuf
Definition: UARTCC26XX.h:609
size_t writeSize
Definition: UARTCC26XX.h:611
enum UART_PAR_ UART_PAR
UART parity type settings.
enum UART_LEN_ UART_LEN
UART data length settings.
const UART_FxnTable UARTCC26XX_fxnTable
RingBuf_Object ringBuffer
Definition: UARTCC26XX.h:619
enum UART_Mode_ UART_Mode
UART mode settings.
Power notify object structure.
Definition: Power.h:121
SemaphoreP_Struct readSem
Definition: UARTCC26XX.h:634
size_t readSize
Definition: UARTCC26XX.h:618
Definition: UARTCC26XX.h:572
unsigned int readTimeout
Definition: UARTCC26XX.h:588
Definition: UARTCC26XX.h:455
bool readRetPartial
Definition: UARTCC26XX.h:615
void * uartPostFxn
Definition: UARTCC26XX.h:626
UART_ReturnMode readReturnMode
Definition: UARTCC26XX.h:592
UART_Status
UART status.
Definition: UARTCC26XX.h:569
Definition: UARTCC26XX.h:574
UARTCC26XX Object.
Definition: UARTCC26XX.h:583
UART_Callback readCallback
Definition: UARTCC26XX.h:590
UART Global configuration.
Definition: UART.h:695
UART_PAR parityType
Definition: UARTCC26XX.h:605
Definition: UARTCC26XX.h:573
size_t readCount
Definition: UARTCC26XX.h:617
UART_LEN dataLength
Definition: UARTCC26XX.h:603
Device-specific pin & GPIO driver for CC26xx family [def].
struct UARTCC26XX_HWAttrsV2 UARTCC26XX_HWAttrsV2
UARTCC26XX Hardware attributes.
HwiP_Struct hwi
Definition: UARTCC26XX.h:631
SemaphoreP_Struct writeSem
Definition: UARTCC26XX.h:633
ClockP_Struct txFifoEmptyClk
Definition: UARTCC26XX.h:635
uint32_t baseAddr
Definition: UARTCC26XX.h:530
Definition: UARTCC26XX.h:460
int intNum
Definition: UARTCC26XX.h:532
UART_Status status
Definition: UARTCC26XX.h:606
Definition: UARTCC26XX.h:575
The definition of a UART function table that contains the required set of functions to control a spec...
Definition: UART.h:652
UARTCC26XX_FifoThreshold txIntFifoThr
Definition: UARTCC26XX.h:558
size_t writeCount
Definition: UARTCC26XX.h:610
unsigned int writeTimeout
Definition: UARTCC26XX.h:589
bool opened
Definition: UARTCC26XX.h:585
uint8_t intPriority
UART Peripheral's interrupt priority.
Definition: UARTCC26XX.h:545
size_t ringBufSize
Definition: UARTCC26XX.h:557
uint8_t rxPin
Definition: UARTCC26XX.h:553
unsigned char * ringBufPtr
Definition: UARTCC26XX.h:556
void(* UARTCC26XX_ErrorCallback)(UART_Handle handle, uint32_t error)
The definition of an optional callback function used by the UART driver to notify the application whe...
Definition: UARTCC26XX.h:481
UART_STOP stopBits
Definition: UARTCC26XX.h:604
bool writeCR
Definition: UARTCC26XX.h:612
Definition: UARTCC26XX.h:571
underlying data structure for type PIN_State
Definition: PIN.h:707
UART_Mode writeMode
Definition: UARTCC26XX.h:587
enum UART_STOP_ UART_STOP
UART stop bit settings.
Definition: UARTCC26XX.h:463
enum UART_ReturnMode_ UART_ReturnMode
UART return mode settings.
SwiP_Struct swi
Definition: UARTCC26XX.h:632
Definition: UARTCC26XX.h:462
Definition: UARTCC26XX.h:461
void * readBuf
Definition: UARTCC26XX.h:616
UART_DataMode readDataMode
Definition: UARTCC26XX.h:593
UARTCC26XX_ErrorCallback errorFxn
Definition: UARTCC26XX.h:561
struct UARTCC26XX_Object * UARTCC26XX_Handle
Definition: UARTCC26XX.h:459
UART_DataMode writeDataMode
Definition: UARTCC26XX.h:594
PIN_State pinState
Definition: UARTCC26XX.h:622
uint8_t ctsPin
Definition: UARTCC26XX.h:554
UARTCC26XX_FifoThreshold rxIntFifoThr
Definition: UARTCC26XX.h:559
struct UARTCC26XX_Object UARTCC26XX_Object
UARTCC26XX Object.
uint32_t swiPriority
SPI SWI priority. The higher the number, the higher the priority. The minimum is 0 and the maximum is...
Definition: UARTCC26XX.h:551
UART_Callback writeCallback
Definition: UARTCC26XX.h:591
uint32_t powerMngrId
Definition: UARTCC26XX.h:531
PIN_Handle hPin
Definition: UARTCC26XX.h:623
void(* UART_Callback)(UART_Handle handle, void *buf, size_t count)
The definition of a callback function used by the UART driver when used in UART_MODE_CALLBACK The cal...
Definition: UART.h:438
uint8_t txPin
Definition: UARTCC26XX.h:552
enum UART_DataMode_ UART_DataMode
UART data mode settings.