SimpleLink™ CC13x0 Proprietary RF User's Guide
1.03.01.00
  • Proprietary RF Quick Start Guide
  • Examples User’s Guide
  • RF Driver Examples
  • EasyLink Examples
  • RF Settings; What are they and how to use them
  • Running Examples in Code Composer Studio (CCS)
  • Running Examples in IAR
  • Building Examples From the Command Line
  • RF Core
  • Proprietary physical layer
  • EasyLink layer
    • Overview
    • General Behavior
    • Error Handling
    • Supported Functions
    • Frame Structure
  • Over the Air Download (OAD)
  • API References
SimpleLink™ CC13x0 Proprietary RF User's Guide
  • Docs »
  • EasyLink layer

EasyLink layer¶

Overview¶

The EasyLink API should be used in application code. The EasyLink API is intended to abstract the RF Driver in order to give a simple API for customers to use as is or extend to suit their application[Use Cases]

General Behavior¶

Before using the EasyLink API the EasyLink Layer is initialized by calling EasyLink_init(). This initialises and opens the RF driver and configures the modulation scheme passed to EasyLink_init.

The RX and TX can operate independently of each other.

RX is enabled by calling EasyLink_receive() or EasyLink_receiveAsync(). Entering RX can be immediate or scheduled by using the EasyLink_RxPacket::absTime field. EasyLink_receive() is blocking and EasyLink_receiveAsync() is nonblocking. The EasyLink API does not queue messages so calling another API function while in EasyLink_receiveAsync() will return EasyLink_Status_Busy_Error. An Asynchronous Rx operation can be cancelled with EasyLink_abort().

TX is enabled by calling EasyLink_transmit() or EasyLink_transmitAsync(). TX can be immediate or scheduled by using the EasyLink_TxPacket::absTime field. EasyLink_transmit() is blocking and EasyLink_transmitAsync() is nonblocking. The EasyLink API does not queue messages so calling another API function while in EasyLink_transmitAsync() will return EasyLink_Status_Busy_Error An Asynchronous operation can be cancelled with EasyLink_abort().

Error Handling¶

The EasyLink API will return EasyLink_Status containing success or error code.

The EasyLink_Status code are:

EasyLink_Status_Success
EasyLink_Status_Config_Error
EasyLink_Status_Param_Error
EasyLink_Status_Mem_Error
EasyLink_Status_Cmd_Error
EasyLink_Status_Tx_Error
EasyLink_Status_Rx_Error
EasyLink_Status_Rx_Timeout
EasyLink_Status_Busy_Error
EasyLink_Status_Aborted

Supported Functions¶

Generic API function Description
EasyLink_init() Init’s and opens the RF driver and configures the specified modulation
EasyLink_transmit() Blocking Transmit
EasyLink_transmitAsync() Nonblocking Transmit
EasyLink_receive() Blocking Receive
EasyLink_receiveAsync() Nonblocking Receive
EasyLink_abort() Aborts a non blocking call
EasyLink_EnableRxAddrFilter() Enables/Disables RX filtering on the Addr
EasyLink_GetIeeeAddr() Gets the IEEE Address
EasyLink_SetFreq() Sets the frequency
EasyLink_GetFreq() Gets the frequency
EasyLink_SetRfPwr() Sets the Tx Power
EasyLink_GetRfPwr() Gets the Tx Power

Frame Structure¶

The EasyLink implements a basic header for transmitting and receiving data. This header supports addressing for a star or point-to-point network with acknowledgements.

Packet structure:

1B Length 1-64b Dst Address Payload
Next Previous

© Copyright 2016-2018, Texas Instruments.