SimpleLink™ CC13x0 SDK 1.60.00.21 Change log
Table of Contents
New Features
TI 15.4 Stack
None
TI Proprietary-RF
ID | Summary |
---|---|
EZLINKPROP-101 | Add Tx/Rx echo RF driver example |
EZLINKPROP-97 | Converge EasyLink_init() and EasyLink_init_multimode() APIs |
EZLINKPROP-89 | Add Tx/Rx echo EasyLink example |
EZLINKPROP-57 | RF driver example for dual-mode for 1350/1352 |
EZLINKPROP-54 | New API that supports EasyLink TX with CCA and Random Timeout |
EZLINKPROP-45 | Add a RX test mode for NP project |
TI-RTOS and Drivers
ID | Summary |
---|---|
TIRTOS-1355 | Sync CC1352 smartrf settings with SmartRF Studio 2.8.0 |
TIRTOS-1348 | Update RF examples to share common code for TIRTOS and NORTOS |
TIRTOS-1312 | Update POSIX pthread support to show ‘fxn’ in UIA execution graph |
TIRTOS-1285 | Enable FreeRTOS re-entrancy support for GNU targets (use newlib-nano) |
TIRTOS-1212 | Add examples for CC1312R1 launchpad |
TIDRIVERS-1279 | Revise Crypto APIs |
TIDRIVERS-1278 | Remove internal key generation from Agama crypto driver implementations |
TIDRIVERS-1257 | Add board and linker files for CC1312R LaunchPad |
TIDRIVERS-1214 | LaunchPad Board files should disable external flash memory during initialization |
TIDRIVERS-1183 | Improve RAM footprint of No-RTOS HwiP dispatch table |
TIDRIVERS-1174 | Provide IOCTL command for FIFO interrupt depth in CC26xx UART driver |
TIDRIVERS-1159 | Enable UART1 in CC26XX driver |
TIDRIVERS-1132 | Implement generic ECDSA driver for CC13X2/CC26X2 devices |
TIDRIVERS-1105 | Implement generic EC J-PAKE driver for CC13X2/CC26X2 devices |
TIDRIVERS-956 | Implement generic SHA2 driver for CC13X2/CC26X2 devices |
TIDRIVERS-952 | Implement generic AES_ECB driver for CC13X2/CC26X2 devices |
TIDRIVERS-736 | Remove CSN wakeup functionality from SPICC26XXDMA |
TIDRIVERS-476 | Provide convenience macros to convert time into RAT ticks in the RF driver |
Fixed Issues
TI 15.4 Stack
ID | Summary |
---|---|
TIMAC-1661 | Fixed issue of no data cnf received after call ApiMac_mcpsDataReq with success return |
TIMAC-1656 | Fixed issue where 15.4 collector stops sending Beacon in Beacon mode with BO=5 |
TIMAC-1654 | Fixed a case where orphan device stopped sending Orphan Notification after 10 hours |
TIMAC-1653 | Fixed issue where 15.4 sensor device cannot sleep before start event |
TIMAC-1600 | NVOCOP_deleteItem can now delete specific items in NV instead of whole page |
SDKSYSAPPS-284 | Fixed CC13xx-SBL 15.4 Linux Gateway project does not work with a bare UART interface |
TI Proprietary-RF
ID | Summary |
---|---|
EZLINKPROP-104 | EasyLink_getRfPwr has function type int_8, but may return a status (EasyLink_Status_Config_Error) |
TI-RTOS and Drivers
ID | Summary |
---|---|
TIRTOS-1282 | FreeRTOS POSIX clock should support CLOCK_REALTIME |
TIRTOS-1214 | GPIO callbacks cannot be disabled in GPIO Interrupt example |
TIRTOS-1199 | Example gcc makefiles are missing rts include path |
TIRTOS-906 | Add support for POSIX errno |
TIDRIVERS-1286 | RF driver scheduling issue for high priority client scheduling in the future |
TIDRIVERS-1284 | NoRTOS SemaphoreP_post can permanently disable power policy |
TIDRIVERS-1270 | Provide more SPI CS management options for NVSSPI25X |
TIDRIVERS-1269 | ADC driver does not clear IRQ flags |
TIDRIVERS-1265 | CC26xx ADC driver configures IO incorrectly |
TIDRIVERS-1260 | NVS post verify always fails |
TIDRIVERS-1256 | Correct the RAT sync criterion in single-mode |
TIDRIVERS-1249 | NoRTOS HwiPCC26XX dispatch table does not cover all possible CC13X2/CC26X2 interrupts |
TIDRIVERS-1243 | RAT Compare prevents BLE5-posted command from starting |
TIDRIVERS-1225 | NVS drivers pre-erase 2 sectors when write is equal to sector size |
TIDRIVERS-1217 | RF Driver: fsmSetupState is changing the rate word in the setup command in proprietary mode |
TIDRIVERS-1208 | NoRTOS HwiPCC26XX_construct not setting the correct priority when called from UARTCC26XX_Open |
TIDRIVERS-1178 | Introduce automatic power management for the RAT APIs |
TIDRIVERS-1172 | SPICC26XXDMA should require transfer buffers to be aligned to data size |
TIDRIVERS-1022 | Remove AUX power down code from Power_init() for CC13X2/CC26X2 devices |
TIDRIVERS-724 | SPI drivers should set transaction status |
Known Issues
TI 15.4 Stack
ID | Summary |
---|---|
SDKSYSAPPS-129 | MT Fragmentation issue on the Linux collector application limits the MT message max length to be 128 bytes. |
TI Proprietary-RF
ID | Summary |
---|---|
None | None |
TI-RTOS and Drivers
ID | Summary |
---|---|
TIRTOS-476 | POSIX threads render as single task in execution graph |
TIDRIVERS-858 | Stack Underflow in SHA256 finish |
TIDRIVERS-723 | UARTCC26XX.c accepts invalid open parameters |
TIDRIVERS-439 | RF_ratCompare works intermittently in single mode code when future commands are posted |
TIDRIVERS-406 | Warning in sensorI2C.c when building BLE CCS projects using I2C |
TIDRIVERS-386 | Timing difference from SYSRESET as compared to a hard reset |
TIDRIVERS-206 | Display driver does not support float |
TIDRIVERS-204 | LCDDogm128 writes outside buffer |
TIDRIVERS-188 | SPICC26XXDMA / UDMACC26XX - Bus faults not handled |
TIDRIVERS-146 | Possible bug in LCD driver (DOGM 128-6) for drawing/clearing vertical lines |
TIDRIVERS-92 | Incorrect thread safety in LCD_open |