rfEasyLinkEchoRx Example
Example Summary
This example demonstrates the use of the EasyLink API in doing bi-directional communication. It will require the use of two boards, one running the rfEasyLinkEchoTx project that will originate the packets, while another board running the rfEasyLinkEchoRx project will re-transmit (echo) them back to the originator.
For more information on the EasyLink API and usage refer to https://processors.wiki.ti.com/index.php/SimpleLink-EasyLink
Peripherals Exercised
For the rfEasyLinkEchoTx (Board_1) project,
Board_PIN_LED1- Blinking indicates a successful transmission and reception of a packet (echo)Board_PIN_LED2- Indicates an abort occurred in packet reception (waiting for the echo)Board_PIN_LED1&Board_PIN_LED2indicate an error condition
For the rfEasyLinkEchoRx (Board_2) project,
Board_PIN_LED2- Blinking indicates a successful reception and re-transmission of a packet (echo)Board_PIN_LED1- Indicates an error in either reception of a packet or in its re-transmission
Resources & Jumper Settings
If you’re using an IDE (such as CCS or IAR), please refer to Board.html in your project directory for resources used and board-specific jumper settings. Otherwise, you can find Board.html in the directory <SDK_INSTALL_DIR>/source/ti/boards/<BOARD>.
Example Usage
The user will require two launchpads, one running rfEasyLinkEchoTx (Board_1), another running rfEasyLinkEchoRx (Board_2). Run Board_2 first, followed by Board_1. Board_1 is set to transmit a packet every second while Board_2 is set to receive the packet and then turnaround and transmit it after a delay of 100ms. Board_PIN_LED1 on Board_1 will toggle when it’s able to successfully transmits a packet, and when it receives its echo. Board_PIN_LED2 on Board_2 will toggle when it receives a packet, and then when its able to re-transmit it (see figure 1).
If the receiver (Board_2) is turned off and the rfEchoTx (Board_1) begins transmitting, Board_1 switches over to the receiver mode waiting for an echo that will never come; in this situation a timeout timer is started and if no packet is received within 300ms the receiver operation is aborted. This condition is indicated by Board_PIN_LED1 being cleared and Board_PIN_LED2 being set (see figure 2).
If the receiver continues to stay turned off then the rfEchoTx example will alternate between transmitting and aborted receiver operations. Board_PIN_LED1 and Board_PIN_LED2 will start alternating, as seen in figure 3.
An error in transmission of a packet, or the reception of its echo, is indicated by both LEDs going high on Board_1, while an error on Board_2 will cause it to set Board_PIN_LED1 high and Board_PIN_LED2 low (see figure 4).
.
Application Design Details
This example shows how to use the EasyLink API to access the RF driver, set the frequency and transmit packets. The RFEASYLINKTX_ASYNC define is used to select between the Blocking or Async TX/RX API.
The rfEasyLinkEchoTx example will transmit a packet every second while the rfEasyLinkEchoRx will echo all received packets after a delay of 100ms. If Board_1 aborts a packet reception Board_PIN_LED2 is set while Board_PIN_LED1 is cleared. An error condition on Board_1 is indicated by both LEDs going high. An error condition on Board_2 is indicated by Board_LED_1 going high while Board_LED_2 is cleared.
A single task, “rfEasyLinkEchoFnx”, configures the RF driver through the EasyLink API and transmits and receives messages.
EasyLink API
Overview
The EasyLink API should be used in application code. The EasyLink API is intended to abstract the RF Driver in order to give a simple API for customers to use as is or extend to suit their application[Use Cases] (@ref USE_CASES).
General Behavior
Before using the EasyLink API:
- The EasyLink Layer is initialized by calling EasyLink_init(). This initializes and opens the RF driver and configures a modulation scheme passed to EasyLink_init.
- The RX and TX can operate independently of each other.
The following is true for receive operation:
- RX is enabled by calling EasyLink_receive() or EasyLink_receiveAsync()
- Entering RX can be immediate or scheduled
- EasyLink_receive() is blocking and EasyLink_receiveAsync() is non-blocking
- The EasyLink API does not queue messages so calling another API function while in EasyLink_receiveAsync() will return EasyLink_Status_Busy_Error
- An Async operation can be cancelled with EasyLink_abort()
The following apply for transmit operation:
- TX is enabled by calling EasyLink_transmit(), EasyLink_transmitAsync() or EasyLink_transmitCcaAsync()
- TX can be immediate or scheduled
- EasyLink_transmit() is blocking and EasyLink_transmitAsync(), EasyLink_transmitCcaAsync() are non-blocking
- EasyLink_transmit() for a scheduled command, or if TX cannot start
- The EasyLink API does not queue messages so calling another API function while in either EasyLink_transmitAsync() or EasyLink_transmitCcaAsync() will return EasyLink_Status_Busy_Error
- An Async operation can be cancelled with EasyLink_abort()
Error Handling
The EasyLink API will return EasyLink_Status containing success or error code. The EasyLink_Status codes are:
- EasyLink_Status_Success
- EasyLink_Status_Config_Error
- EasyLink_Status_Param_Error
- EasyLink_Status_Mem_Error
- EasyLink_Status_Cmd_Error
- EasyLink_Status_Tx_Error
- EasyLink_Status_Rx_Error
- EasyLink_Status_Rx_Timeout
- EasyLink_Status_Busy_Error
- EasyLink_Status_Aborted
Power Management
The power management framework will try to put the device into the most power efficient mode whenever possible. Please see the technical reference manual for further details on each power mode.
The EasyLink Layer uses the power management offered by the RF driver Refer to the RF Driver documentation for more details.
Supported Functions
| Generic API function | Description |
|-------------------------------|----------------------------------------------------|
| EasyLink_init() | Init's and opens the RF driver and configures the |
| | specified modulation |
| EasyLink_transmit() | Blocking Transmit |
| EasyLink_transmitAsync() | Non-blocking Transmit |
| EasyLink_transmitCcaAsync() | Non-blocking Transmit with Clear Channel Assessment|
| EasyLink_receive() | Blocking Receive |
| EasyLink_receiveAsync() | Non-blocking Receive |
| EasyLink_abort() | Aborts a non-blocking call |
| EasyLink_EnableRxAddrFilter() | Enables/Disables RX filtering on the Addr |
| EasyLink_GetIeeeAddr() | Gets the IEEE Address |
| EasyLink_SetFreq() | Sets the frequency |
| EasyLink_GetFreq() | Gets the frequency |
| EasyLink_SetRfPwr() | Sets the TX Power |
| EasyLink_GetRfPwr() | Gets the TX Power |
Frame Structure
The EasyLink implements a basic header for transmitting and receiving data. This header supports addressing for a star or point-to-point network with acknowledgements.
Packet structure:
_________________________________________________________
| | | |
| 1B Length | 1-64b Dst Address | Payload |
|___________|___________________|_________________________|
Note for IAR users: When using the CC1310DK, the TI XDS110v3 USB Emulator must be selected. For the CC1310_LAUNCHXL, select TI XDS110 Emulator. In both cases, select the cJTAG interface.