TI 15.4-Stack 2.02.00.00 Release Notes
Table of Contents
Introduction
TI 15.4-Stack is an IEEE 802.15.4e/g based software stack part of the SimpleLink CC13x0 SDK that supports a Star network topology for Sub-1GHz applications. TI 15.4-Stack software runs on TI’s SimpleLink™ Sub-1GHz wireless microcontrollers, including the CC1310 and CC1350. Devices running TI 15.4-Stack offer key benefits, such as longer range in the FCC band and better protection against in-band interference through use of WiSun based frequency hopping, ability to send BLE beacons while operating on Sub1GHz TI 15.4-Stack network when using dual-band CC1350. TI 15.4-Stack provides a complete end-to-end wireless application development solution to reduce time and cost of getting your product to market quickly.
Documentation
- TI 15.4-Stack Quick Start Guide
- TI 15.4-Stack User's Guide
- TI 15.4-Stack CoP Interface Guide
- TI 15.4 Stack APIs
- Software License
- Software Manifest
What’s New
ID | Summary |
---|---|
TIMAC-1192 | Added support for latest wireshark release v2.2.1 |
SDKSYSAPPS-22 | Added support for Over the Air Download using TI-15.4 Stack |
Fixed Issues
ID | Summary |
---|---|
TIMAC-1535 | Updated to use the latest coreSDK version 3-20-00-17 |
TIMAC-1518 | Sensor example application start time is randomized for all modes to handle the case where large number of sensors are starting at the same time and attempting to join the network at the same time. Reduced OTA traffic and load on PAN coordinator. |
TIMAC-1508 | Fixed an issue where function macCmdIncludeFHIE() was is in the project even when FH is disabled. |
TIMAC-1488 | Fixed the issue where Board_Palna_initialize gets called when CONFIG_RANGE_EXT_MODE=APIMAC_NO_EXTENDER |
TIMAC-1486 | Fixed a rare issue in Frequency Hopping mode where an error could cause the radio operations to halt until reset. |
TIMAC-1485 | Fixed an issue which prevented dynamic power change using the API ApiMac_mcpsDataReq() |
TIMAC-1484 | Removed “MODULE_CC13XX_7X7” from mac_user_confic.c. The implementation in file mac_user_config.c is not package type dependent |
TIMAC-1479 | Fixed the issue that the device disassociation on the sensor example application does not work when button 1 is pressed. |
TIMAC-1478 | Fixed the issue that the function removeTheFirstDevice() on collector example application does not work |
TIMAC-1477 | In collector example application optimized function Cllc_removeDevice() to stop the loop after desired device has been found |
TIMAC-1476 | Fixed the issue where wrong function identifier addBlackListItem() was getting called instead of Csf_addBlackListItem() in function removeTheFirstDevice() csf.c |
TIMAC-1471 | Enabling compile flag POWER_MEAS now removes UART, LCD and other functionality to allow measuring power without peripheral power being added into measurements |
TIMAC-1466 | Fixed an issue in Frequency Hopping mode where adding a non-sleepy device will make the network unstable |
TIMAC-1448 | Added DEFAULT_ADVERTISING_INTERVAL define in config.h |
TIMAC-1429 | Added variable I2C_count to the board file |
TIMAC-1428 | Example applications allow to configure the BOOST_MODE for 14dBm output power |
TIMAC-1398 | Optimized operation in beacon mode, where after sync loss RFD would still wake up every Beacon Interval |
TIMAC-1330 | Resolved the issue where removing USE_UART_PRINTF compile flag results in errors |
TIMAC-1328 | Fixed an issue for MAC CoProcessor where bad FCS in NPI transaction could cause memory leak. |
TIMAC-1327 | Fixed an issue where in rare cases stack may need to be reset after power up due to a lock up condition. |
TIMAC-1138 | Optimized power consumption for 15.4 MAC by allowing Radio to power down during CSMA backoff |
Known Issues
ID | Summary |
---|---|
SDKSYSAPPS-130 | OAD UI in some cases do not show message failure |
Upgrade and Compatibility Information
Operating System Support
The TI 15.4-Stack SDK is supported on the Microsoft Windows® platform.
Dependencies
TI 15.4-Stack 2.02.00.00 was built & tested on a Windows 7 host platform using the following Integrated Development Environment (IDE) and components. Using an IDE version or TI-RTOS version not listed below may result in compatibility issues with this SDK release.
- Code Composer Studio: 7.2.0
- TI-RTOS for CC13XX: 3.20.00.17
- C Compiler for ARM: 16.09.3.LTS
- XDCTools: 3.50.02.20
Device Support
Development Board Support
Validation
TI 15.4-Stack 2.02.00.00 was tested using the following components:
- TI-RTOS for CC13XX: 3.20.00.17
- C Compiler for ARM: 16.09.3.LTS
- XDCTools: 3.50.02.20
- CC1310 LaunchPad
- CC1350 LaunchPad
Versioning
This product follows a version format, M.mm.pp.bb, where:
- M is a 1 digit major number,
- mm is a 2 digit minor number,
- pp is a 2 digit patch number,
- bb is a 2 digit incrementing build counter.