Zigbee Router Door Lock Example App
Introduction
This document discusses how to use the Zigbee Door Lock Example App and the different parts that compose it. Zigbee Door Lock Application is an example which exercises different features of TI Z-Stack.
Some of the features exercised include:
- Base Device Behavior attribute configuration.
- This Door Lock device that acts as Target and Initiator of Finding and Binding.
Hardware Prerequisites
Software Prerequisites
Code Composer Studio™ (CCS) v7.3 or newer
Functional Description
Software Overview
This section describes software components and the corresponding source file.
Application Files
- zcl_sampledoorlock.c/.h: Contains the application’s event loop, device initialization function calls (for timers, peripherals, Nvm, LEDs, Switches, Serial interface), Zigbee stack notifications and all Door Lock specific logic.
- zcl_sampledoorlock_data.c/.h: Contains the endpoint, cluster and attribute definitions for this sample application.
- main.c Defines the application task, the application stack size.
- bdb_interface.h Defines commissioning parameters to be used and configured in the application upon calling commissioning methods (see zclSampleDoorLock_initParameters()).
Example Usage
This section describes how to use this sample application.
Buttons
BTN-1
: Starts the commissioning process.
LEDs
DIO6
: Is set to On when the Door is Locked, Off otherwise.
Serial interface
- Open a serial session (e.g.
PuTTY
, etc.) to the appropriate COM port.- The COM port can be determined via Device Manager in Windows or via
ls /dev/tty*
in Linux.
- The COM port can be determined via Device Manager in Windows or via
The connection will have the following settings:
Baud-rate: 115200
Data bits: 8
Stop bits: 1
Parity: None
Flow Control: None
Note: The serial output is known to be formatted incorrectly in Tera Term and in the CCS Terminal.
The serial interface allows you to control the commissioning configuration as well as application behavior. The commissioning interface is common for all applications and is implemented in the module zcl_sampleapps_ui.c/.h. Any application specific behavior of the serial interface is implemented in the example application files.
The serial interface implements a common set of menus described in Application Overview. This common menu has to be used to commission the device into a network.
Commissioning the Device Into the Network
Zigbee router devices can create a network with limited security capabilities (Distributed network) or join a network. The commissioning process to be done can be configured in the Commissioning screen, note that if both Formation Mode and Steering Mode are enabled when Commissioning is executed, the stack will first try to join a network, after which if it fails, the device will create its own network. This sample applications uses the stack notifications (zstackmsg_CmdIDs_BDB_NOTIFICATION) on a successful network formation process to open the network and allow new devices join, even if the Steering Mode is not enabled from the common user interface. In the same way, if the device joins a network, it will open the network for 180 seconds. If the network is closed, it can be open again by enabling the Steering Mode and execute the commmissioning process in the Commissioning Screen.
Interfacing with the Door Lock Controller Example App
Once the Door Lock and Door Lock Controller device are in the same network, enable the Finding and Binding Mode and excecute it from the Commissioning Screen on both devices. Both devices will be set in Identify mode for 180 seconds and will search for each other to create a bind (Door Lock will create a bind to Door Lock Controller and the otherway around as well).
Finding and binding status screen
IdXXX shows the remaining XXX seconds in Identify mode, SrchYYY/ZZ shows the remaining YYY seconds searching for devices in Identify mode and ZZ the number of binds created during this process. Once the Door Lock Controller device has the bind, it will be able to lock or unlock the door in the Door Lock screen. When the Door Lock creates the bind to the Door Lock Controller it will be able to report the state of the door automatically through reporting mechanism.
Both devices will set IdXXX and SrcYYY to 180 seconds and will count down as ZZ will count the binds to the other devices found. Multiple devices can perform this procedure at the same time, by default one device can have up to 4 binds (one Door Lock can report up to 4 Door Lock Controllers or one Door Lock Controller can control 4 Door Locks), this is defined by NWK_MAX_BINDING_ENTRIES. There is no limit on the number of Door Lock Controllers that can control a single Door Lock.
Finding and Binding for Door Lock cluster is meant to be use to create the bind in Door Lock only, but this sample application has been modify to create the bind in the Door Lock Controller to allow sending the controller commands easily.
Enter into App Menu to access to application specific application controls.
Application menu entrance screen
In the Change PIN screen the PIN can be changed, both devices Door Lock and Door Lock Controller must have the same PIN in order to lock or unlock the door.
Change PIN screen
The status of the door is display in the Door Lock status screen in which it can also be changed. The Door Lock Controller can keep track of the status of the Door Lock due to the reports the Door Lock sends whenever the status of the door changes.
Control door screen