Zigbee OTA Server Example App
Introduction
This document only discusses how to commission OTA server application into a network, as details on how OTA upgrade process is done is fully described in Z-Stack OTA Upgrade User’s Guide.
Hardware Prerequisites
Software Prerequisites
Code Composer Studio™ (CCS) v7.3 or newer
Example Usage
This sample application is meant to be used along with OTAServer desktop application provided in Z-Stack SDK in tools folder. The serial interface must be configured with the following serial parameters:
Baud-rate: 115200
Data bits: 8
Stop bits: 1
Parity: None
Flow Control: CTS/RST
To commission the device into the network press the button 1 (BTN-1
) or use the interface provided in the desktop application. To fully run a OTA upgrade process, a Client Device is also required. Further details on how to setup the devices, generate the binaries, use the desktop application and complete a full OTA upgrade are described in Z-Stack OTA Upgrade User’s Guide.