Main Page | Alphabetical List | Data Structures | Directories | File List | Data Fields | Globals

RingIO_Config_Tag Struct Reference

#include <RingIO.h>

Collaboration diagram for RingIO_Config_Tag:

Collaboration graph
[legend]

Detailed Description

Structure defining config parameters for the RingIO module.

Definition at line 391 of file RingIO.h.

Data Fields

UInt32 maxNameLen
UInt32 maxInstances


Field Documentation

UInt32 RingIO_Config_Tag::maxInstances
 

Maximum number of RingIO's that can be made

Definition at line 395 of file RingIO.h.

UInt32 RingIO_Config_Tag::maxNameLen
 

Maximum length of the name of RingIO instance

Definition at line 393 of file RingIO.h.


The documentation for this struct was generated from the following file:
Generated on Mon Mar 14 11:59:54 2011 for Syslink by  doxygen 1.4.4