Main Page | Alphabetical List | Data Structures | Directories | File List | Data Fields | Globals

RingIOShm_Config_Tag Struct Reference

#include <RingIOShm.h>

Collaboration diagram for RingIOShm_Config_Tag:

Collaboration graph
[legend]

Detailed Description

Structure defining config parameters for the RingIOShm module.

Definition at line 310 of file RingIOShm.h.

Data Fields

UInt32 notifyEventNo


Field Documentation

UInt32 RingIOShm_Config_Tag::notifyEventNo
 

Notify event number to be used by the Client Notify Manager

Definition at line 312 of file RingIOShm.h.


The documentation for this struct was generated from the following file:
Generated on Mon Mar 14 11:59:54 2011 for Syslink by  doxygen 1.4.4