Main Page | Alphabetical List | Data Structures | Directories | File List | Data Fields | Globals

ProcMgr_StartParams_tag Struct Reference

#include <ProcMgr.h>

Collaboration diagram for ProcMgr_StartParams_tag:

Collaboration graph
[legend]

Detailed Description

Configuration parameters to be provided while starting the slave processor.

Definition at line 330 of file ProcMgr.h.

Data Fields

UInt32 reserved


Field Documentation

UInt32 ProcMgr_StartParams_tag::reserved
 

Reserved for future params.

Definition at line 332 of file ProcMgr.h.


The documentation for this struct was generated from the following file:
Generated on Mon Mar 14 11:59:53 2011 for Syslink by  doxygen 1.4.4