Main Page | Alphabetical List | Data Structures | Directories | File List | Data Fields | Globals

List_Params_tag Struct Reference

#include <List.h>

Collaboration diagram for List_Params_tag:

Collaboration graph
[legend]

Detailed Description

Structure defining params for the list.

Definition at line 96 of file List.h.

Data Fields

UInt32 temp


Field Documentation

UInt32 List_Params_tag::temp
 

Definition at line 97 of file List.h.


The documentation for this struct was generated from the following file:
Generated on Mon Mar 14 11:59:52 2011 for Syslink by  doxygen 1.4.4