Main Page | Alphabetical List | Data Structures | Directories | File List | Data Fields | Globals

FrameQBufMgr_CommonOpenParams_Tag Struct Reference

#include <FrameQBufMgr.h>

Collaboration diagram for FrameQBufMgr_CommonOpenParams_Tag:

Collaboration graph
[legend]

Detailed Description

Common parameters required to open a FrameQBufMgr instance of any implementation.

Definition at line 426 of file FrameQBufMgr.h.

Data Fields

String name
UInt32 cpuAccessFlags
Ptr sharedAddr


Field Documentation

UInt32 FrameQBufMgr_CommonOpenParams_Tag::cpuAccessFlags
 

cpuAccessFlags flags to know if Frame buffers are accessed through CPU

Definition at line 431 of file FrameQBufMgr.h.

String FrameQBufMgr_CommonOpenParams_Tag::name
 

Name of the instance to open

Definition at line 428 of file FrameQBufMgr.h.

Ptr FrameQBufMgr_CommonOpenParams_Tag::sharedAddr
 

Virtual shared Region addr in case open by address is required.

Definition at line 434 of file FrameQBufMgr.h.


The documentation for this struct was generated from the following file:
Generated on Mon Mar 14 11:59:50 2011 for Syslink by  doxygen 1.4.4