| Cache.h [code] | Defines Cache API interface |
| FrameQ.h [code] | Defines for interfaces for FrameQ module |
| FrameQ_ShMem.h [code] | Header file for FrameQ on SharedMemory interface |
| FrameQBufMgr.h [code] | Defines for interfaces for FrameQBufMgr module |
| FrameQBufMgr_ShMem.h [code] | Header file for FrameQBufMgr ShMem |
| FrameQBufMgrDefs.h [code] | Defines configurable elements for FrameQBufMgr module |
| FrameQDefs.h [code] | Defines configurable elements for FrameQ module |
| Gate.h [code] | Critical section support |
| GateMonitor.h [code] | Header file for Gate based on Monitor |
| GateMutex.h [code] | Gate based on Mutex |
| GateSem.h [code] | Header file for Gate based on Semaphore |
| GateSpinlock.h [code] | Gate based on Spinlock |
| IGateProvider.h [code] | Interface implemented by all gate providers |
| IHeap.h [code] | Defines Heap based memory allocator |
| IpcHost.h [code] | This file contains APIs and defines that are used by applications only on the host-side of the device |
| List.h [code] | Creates a doubly linked list |
| Memory.h [code] | Memory manager interface definitions |
| MemoryDefs.h [code] | Definitions for Memory module |
| MemoryOS.h [code] | Memory abstraction APIs for local memory allocation |
| OsalPrint.h [code] | Kernel utils Print interface definitions |
| OsalSemaphore.h [code] | Kernel utils Semaphore interface definitions |
| ProcMgr.h [code] | The Processor Manager on a master processor provides control functionality for a slave device |
| RingIO.h [code] | This will have definitions for interfaces and structures for RingIO module |
| RingIOShm.h [code] | RingIOShm shared memory based physical transport for communication with the remote processor |
| Std.h [code] | This will have definitions of standard data types for platform abstraction |
| String.h [code] | Defines for String manipulation library |
| SysLink.h [code] | This module contains common definitions, types, structures and functions used by SysLink |
| SyslinkMemMgr.h [code] | Header file implementing Memory manager |
| Trace.h [code] | Kernel Trace enabling/disabling/application interface |
1.4.4