Main Page | Alphabetical List | Data Structures | Directories | File List | Data Fields | Globals

Memory.h File Reference


Detailed Description

Memory manager interface definitions.

This abstracts the Memory management interface to be used with SysLink code. Allocation, Freeing-up, copy and address translate are supported for the memory management.

02.00.00.68_beta1

============================================================================

Copyright (c) 2008-2009, Texas Instruments Incorporated

Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:

* Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer.

* Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution.

* Neither the name of Texas Instruments Incorporated nor the names of its contributors may be used to endorse or promote products derived from this software without specific prior written permission.

THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. Contact information for paper mail: Texas Instruments Post Office Box 655303 Dallas, Texas 75265 Contact information: http://www-k.ext.ti.com/sc/technical-support/product-information-centers.htm? DCMP=TIHomeTracking&HQS=Other+OT+home_d_contact ============================================================================

Definition in file Memory.h.

#include <ti/syslink/utils/MemoryDefs.h>
#include <ti/syslink/utils/MemoryOS.h>
#include <ti/syslink/utils/IHeap.h>

Include dependency graph for Memory.h:

Go to the source code of this file.

Defines

#define Memory_Q_BLOCKING   1
 Blocking quality Heaps with this "quality" may cause the calling thread to block; i.e., suspend execution until another thread leaves the gate.
#define Memory_map   MemoryOS_map
 Maps a memory area into virtual space.
#define Memory_unmap   MemoryOS_unmap
 Unmaps a memory area into virtual space.
#define Memory_copy   MemoryOS_copy
 Copies the data between memory areas.
#define Memory_set   MemoryOS_set
 Set the specific value in the said memory area.

Functions

Ptr Memory_alloc (IHeap_Handle heap, SizeT size, SizeT align, Ptr eb)
 Allocates the specified number of bytes.
Ptr Memory_calloc (IHeap_Handle heap, SizeT size, SizeT align, Ptr eb)
 Allocates the specified number of bytes and memory is set to zero.
Void Memory_free (IHeap_Handle heap, Ptr block, SizeT size)
 Frees up the specified chunk of memory.
Void Memory_getStats (IHeap_Handle heap, Memory_Stats *stats)
 Function to obtain statistics from a heap.
Bool Memory_query (IHeap_Handle heap, Int qual)
 Function to test for a particular IHeap quality.
SizeT Memory_getMaxDefaultTypeAlign (Void)
 Function to get memory alignment.
Ptr Memory_valloc (IHeap_Handle heap, SizeT size, SizeT align, Char value, Ptr eb)
 Allocates the specified number of bytes and memory is set to the specified value.
Ptr Memory_translate (Ptr srcAddr, Memory_XltFlags flags)
 Function to translate an address.


Define Documentation

#define Memory_copy   MemoryOS_copy
 

Copies the data between memory areas.

Definition at line 216 of file Memory.h.

#define Memory_map   MemoryOS_map
 

Maps a memory area into virtual space.

See also:
Memory_unmap

Definition at line 205 of file Memory.h.

#define Memory_Q_BLOCKING   1
 

Blocking quality Heaps with this "quality" may cause the calling thread to block; i.e., suspend execution until another thread leaves the gate.

Definition at line 81 of file Memory.h.

#define Memory_set   MemoryOS_set
 

Set the specific value in the said memory area.

Definition at line 221 of file Memory.h.

#define Memory_unmap   MemoryOS_unmap
 

Unmaps a memory area into virtual space.

See also:
Memory_unmap

Definition at line 211 of file Memory.h.


Function Documentation

Ptr Memory_alloc IHeap_Handle  heap,
SizeT  size,
SizeT  align,
Ptr  eb
 

Allocates the specified number of bytes.

Parameters:
heap Handle to the heap from which the memory is to be allocated. Specify NULL to allocate from local memory.
size Amount of memory to be allocated.
align Alignment constraints (power of 2)
eb Not used. Pass as NULL.
Return values:
Pointer Success: Pointer to allocated buffer
NULL Failed to allocate memory
See also:
Memory_calloc

Ptr Memory_calloc IHeap_Handle  heap,
SizeT  size,
SizeT  align,
Ptr  eb
 

Allocates the specified number of bytes and memory is set to zero.

Parameters:
heap Handle to the heap from which the memory is to be allocated. Specify NULL to allocate from local memory.
size Amount of memory to be allocated.
align Alignment constraints (power of 2)
eb Not used. Pass as NULL.
Return values:
Pointer Success: Pointer to allocated buffer
NULL Failed to allocate memory
See also:
Memory_alloc, MemoryOS_calloc

Void Memory_free IHeap_Handle  heap,
Ptr  block,
SizeT  size
 

Frees up the specified chunk of memory.

Parameters:
heap Handle to the heap
block Block of memory to be freed
size Amount of memory to be freed
See also:
IHeap_free, MemoryOS_free

SizeT Memory_getMaxDefaultTypeAlign Void   ) 
 

Function to get memory alignment.

Return values:
Alignment Maximum default alignment

Void Memory_getStats IHeap_Handle  heap,
Memory_Stats stats
 

Function to obtain statistics from a heap.

Parameters:
heap Handle to the heap
stats Pointer to the Memory stats structure to be filled.
See also:

Bool Memory_query IHeap_Handle  heap,
Int  qual
 

Function to test for a particular IHeap quality.

Parameters:
heap Handle to the heap
qual Quality to be queried.
See also:
Memory_Q_BLOCKING

Ptr Memory_translate Ptr  srcAddr,
Memory_XltFlags  flags
 

Function to translate an address.

Parameters:
srcAddr source address.
flags Tranlation flags.
Return values:
Pointer Success: Pointer to translated buffer
NULL Failed to translate

Ptr Memory_valloc IHeap_Handle  heap,
SizeT  size,
SizeT  align,
Char  value,
Ptr  eb
 

Allocates the specified number of bytes and memory is set to the specified value.

Parameters:
heap Handle to the heap from which the memory is to be allocated. Specify NULL to allocate from local memory.
size Amount of memory to be allocated.
align Alignment constraints (power of 2)
value Value to be set for all bytes in the buffer
eb Not used. Pass as NULL.
Return values:
Pointer Success: Pointer to allocated buffer
NULL Failed to allocate memory
See also:
Memory_alloc, MemoryOS_calloc


Generated on Mon Mar 14 11:59:47 2011 for Syslink by  doxygen 1.4.4