Main Page | Alphabetical List | Data Structures | Directories | File List | Data Fields | Globals

IpcHost.h File Reference


Detailed Description

This file contains APIs and defines that are used by applications only on the host-side of the device.

02.00.00.68_beta1

============================================================================

Copyright (c) 2008-2009, Texas Instruments Incorporated

Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:

* Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer.

* Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution.

* Neither the name of Texas Instruments Incorporated nor the names of its contributors may be used to endorse or promote products derived from this software without specific prior written permission.

THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. Contact information for paper mail: Texas Instruments Post Office Box 655303 Dallas, Texas 75265 Contact information: http://www-k.ext.ti.com/sc/technical-support/product-information-centers.htm? DCMP=TIHomeTracking&HQS=Other+OT+home_d_contact ============================================================================

Definition in file IpcHost.h.

Go to the source code of this file.

Defines

#define Ipc_CONTROLCMD_LOADCALLBACK   (0xBABE0000)
 Control command ID for load callback. This command should be used with Ipc_control function before using IPC with the slave, and after loading the slave with the slave executable. When ProcMgr is used, this command should be used after loading the slave execution.
#define Ipc_CONTROLCMD_STARTCALLBACK   (0xBABE0001)
 Control command ID for start callback. This command should be used with Ipc_control function before using IPC with the slave, and when the slave is in running state. When ProcMgr is used, this command should be used after starting the slave execution.
#define Ipc_CONTROLCMD_STOPCALLBACK   (0xBABE0002)
 Control command ID for stop callback. This command should be used with Ipc_control function when IPC no longer needs to be performed with the specific slave. When ProcMgr is used, this command should be used just before stopping the slave execution.

Functions

Int Ipc_control (UInt16 procId, Int32 cmdId, Ptr arg)
 Function to perform control operations for IPC with a specific slave.


Define Documentation

#define Ipc_CONTROLCMD_LOADCALLBACK   (0xBABE0000)
 

Control command ID for load callback. This command should be used with Ipc_control function before using IPC with the slave, and after loading the slave with the slave executable. When ProcMgr is used, this command should be used after loading the slave execution.

See also:
Ipc_control

Definition at line 73 of file IpcHost.h.

#define Ipc_CONTROLCMD_STARTCALLBACK   (0xBABE0001)
 

Control command ID for start callback. This command should be used with Ipc_control function before using IPC with the slave, and when the slave is in running state. When ProcMgr is used, this command should be used after starting the slave execution.

See also:
Ipc_control

Definition at line 83 of file IpcHost.h.

#define Ipc_CONTROLCMD_STOPCALLBACK   (0xBABE0002)
 

Control command ID for stop callback. This command should be used with Ipc_control function when IPC no longer needs to be performed with the specific slave. When ProcMgr is used, this command should be used just before stopping the slave execution.

See also:
Ipc_control

Definition at line 93 of file IpcHost.h.


Function Documentation

Int Ipc_control UInt16  procId,
Int32  cmdId,
Ptr  arg
 

Function to perform control operations for IPC with a specific slave.

Parameters:
procId Remote processor ID
cmdId Command ID
arg Argument


Generated on Mon Mar 14 11:59:47 2011 for Syslink by  doxygen 1.4.4