Main Page | Alphabetical List | Data Structures | Directories | File List | Data Fields | Globals

FrameQDefs.h File Reference


Detailed Description

Defines configurable elements for FrameQ module.

02.00.00.68_beta1

============================================================================

Copyright (c) 2008-2009, Texas Instruments Incorporated

Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:

* Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer.

* Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution.

* Neither the name of Texas Instruments Incorporated nor the names of its contributors may be used to endorse or promote products derived from this software without specific prior written permission.

THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. Contact information for paper mail: Texas Instruments Post Office Box 655303 Dallas, Texas 75265 Contact information: http://www-k.ext.ti.com/sc/technical-support/product-information-centers.htm? DCMP=TIHomeTracking&HQS=Other+OT+home_d_contact ============================================================================

Definition in file FrameQDefs.h.

Go to the source code of this file.

Data Structures

struct  Frame_FrameBufInfo_tag
 Structure to frame buffer informantion in frame header. More...
struct  Frame_FrameHeader_Tag
 Structure of the base frame header. FrameQ maintains list of frames to be retrieved by FrameQ reader client. Application is expected to use Helper API to extract fileds and exteneded header pointer. More...

Defines

#define FrameQ_MAX_FRAMESINVAPI   (64u)
 Macro used in FrameQ for sorting of passed parameters in V API. In FrameQ_allocv case this denotes the number of frames that can be allocated in one call. In FrameQ_putv case this denotes the number of frames that can be put in one call. In FrameQ_getv case this denotes the number of frames that can be retrieved in one call.

Typedefs

typedef Frame_FrameBufInfo_tag Frame_FrameBufInfo
 Structure to frame buffer informantion in frame header.
typedef Frame_FrameHeader_Tag Frame_FrameHeader
 Structure of the base frame header. FrameQ maintains list of frames to be retrieved by FrameQ reader client. Application is expected to use Helper API to extract fileds and exteneded header pointer.
typedef Frame_FrameHeaderFrame
 Defines the type for a frame pointer.


Define Documentation

#define FrameQ_MAX_FRAMESINVAPI   (64u)
 

Macro used in FrameQ for sorting of passed parameters in V API. In FrameQ_allocv case this denotes the number of frames that can be allocated in one call. In FrameQ_putv case this denotes the number of frames that can be put in one call. In FrameQ_getv case this denotes the number of frames that can be retrieved in one call.

Definition at line 74 of file FrameQDefs.h.


Typedef Documentation

typedef Frame_FrameHeader* Frame
 

Defines the type for a frame pointer.

Definition at line 130 of file FrameQDefs.h.

typedef struct Frame_FrameBufInfo_tag Frame_FrameBufInfo
 

Structure to frame buffer informantion in frame header.

typedef struct Frame_FrameHeader_Tag Frame_FrameHeader
 

Structure of the base frame header. FrameQ maintains list of frames to be retrieved by FrameQ reader client. Application is expected to use Helper API to extract fileds and exteneded header pointer.


Generated on Mon Mar 14 11:59:46 2011 for Syslink by  doxygen 1.4.4