| const SharedMemoryMgr_MAX_NAME_LENGTH |
 |
#define SharedMemoryMgr_MAX_NAME_LENGTH (UInt8)32
| const SharedMemoryMgr_MAX_TILER_BLOCKS |
 |
#define SharedMemoryMgr_MAX_TILER_BLOCKS (UInt8)10
| enum SharedMemoryMgr_AddrType |
 |
typedef enum SharedMemoryMgr_AddrType {
SharedMemoryMgr_AddrType_Virtual,
SharedMemoryMgr_AddrType_Portable,
SharedMemoryMgr_AddrType_EndValue
} SharedMemoryMgr_AddrType;
| enum SharedMemoryMgr_Type |
 |
typedef enum SharedMemoryMgr_Type {
SharedMemoryMgr_TYPE_SHAREDMEM,
SharedMemoryMgr_TYPE_TILERMEM,
SharedMemoryMgr_TYPE_NONE
} SharedMemoryMgr_Type;
| struct SharedMemoryMgr_AllocBlock |
 |
typedef struct SharedMemoryMgr_AllocBlock {
UInt16 pixelFormat;
union {
struct {
UInt16 width;
UInt16 height;
} area;
UInt16 len;
} dim;
UInt32 stride;
} SharedMemoryMgr_AllocBlock;
| struct SharedMemoryMgr_allocParams |
 |
typedef struct SharedMemoryMgr_allocParams {
UInt32 size;
UInt32 align;
UInt32 tilerBlocks;
} SharedMemoryMgr_allocParams;
| struct SharedMemoryMgr_createParams |
 |
typedef struct SharedMemoryMgr_createParams {
UInt32 size;
} SharedMemoryMgr_createParams;
| struct SharedMemoryMgr_freeParams |
 |
typedef struct SharedMemoryMgr_freeParams {
Ptr ptr;
UInt32 size;
} SharedMemoryMgr_freeParams;
| Module-Wide Built-Ins |
 |
// Get this module's unique id
Bool SharedMemoryMgr_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool SharedMemoryMgr_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 SharedMemoryMgr_Module_getMask();
// Returns the diagnostics mask for this module
Void SharedMemoryMgr_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
| Instance Object Types |
 |
typedef struct SharedMemoryMgr_Object SharedMemoryMgr_Object;
// Opaque internal representation of an instance object
// Client reference to an instance object
typedef struct SharedMemoryMgr_Struct SharedMemoryMgr_Struct;
// Opaque client structure large enough to hold an instance object
// Convert this instance structure pointer into an instance handle
// Convert this instance handle into an instance structure pointer
| Instance Config Parameters |
 |
typedef struct SharedMemoryMgr_Params {
// Instance config-params structure
// Common per-instance configs
//
} SharedMemoryMgr_Params;
// Initialize this config-params structure with supplier-specified defaults before instance creation
| config SharedMemoryMgr_heapHandle // instance |
 |
| SharedMemoryMgr_alloc() // instance |
 |
ARGUMENTS
handle
handle of a previously-created SharedMemoryMgr instance object
| SharedMemoryMgr_free() // instance |
 |
ARGUMENTS
handle
handle of a previously-created SharedMemoryMgr instance object
| SharedMemoryMgr_translate() // instance |
 |
ARGUMENTS
handle
handle of a previously-created SharedMemoryMgr instance object
| Instance Convertors |
 |
// unconditionally move one level up the inheritance hierarchy
// conditionally move one level down the inheritance hierarchy; NULL upon failure
| Instance Built-Ins |
 |
Int SharedMemoryMgr_Object_count();
// The number of statically-created instance objects
// The handle of the i-th statically-created instance object (array == NULL)
// The handle of the first dynamically-created instance object, or NULL
// The handle of the next dynamically-created instance object, or NULL
// The heap used to allocate dynamically-created instance objects
// The label associated with this instance object
// The name of this instance object