| const MemMgrSupportNull_MAX_NAME_LENGTH |
 |
#define MemMgrSupportNull_MAX_NAME_LENGTH (UInt8)32
| const MemMgrSupportNull_MAX_TILER_BLOCKS |
 |
#define MemMgrSupportNull_MAX_TILER_BLOCKS (UInt8)10
| enum MemMgrSupportNull_AddrType |
 |
typedef enum MemMgrSupportNull_AddrType {
MemMgrSupportNull_AddrType_Virtual,
MemMgrSupportNull_AddrType_Portable,
MemMgrSupportNull_AddrType_EndValue
} MemMgrSupportNull_AddrType;
| enum MemMgrSupportNull_Type |
 |
typedef enum MemMgrSupportNull_Type {
MemMgrSupportNull_TYPE_SHAREDMEM,
MemMgrSupportNull_TYPE_TILERMEM,
MemMgrSupportNull_TYPE_NONE
} MemMgrSupportNull_Type;
| struct MemMgrSupportNull_AllocBlock |
 |
typedef struct MemMgrSupportNull_AllocBlock {
UInt16 pixelFormat;
union {
struct {
UInt16 width;
UInt16 height;
} area;
UInt16 len;
} dim;
UInt32 stride;
} MemMgrSupportNull_AllocBlock;
| struct MemMgrSupportNull_allocParams |
 |
typedef struct MemMgrSupportNull_allocParams {
UInt32 size;
UInt32 align;
UInt32 tilerBlocks;
} MemMgrSupportNull_allocParams;
| struct MemMgrSupportNull_createParams |
 |
typedef struct MemMgrSupportNull_createParams {
UInt32 size;
} MemMgrSupportNull_createParams;
| struct MemMgrSupportNull_freeParams |
 |
typedef struct MemMgrSupportNull_freeParams {
Ptr ptr;
UInt32 size;
} MemMgrSupportNull_freeParams;
| Module-Wide Built-Ins |
 |
// Get this module's unique id
Bool MemMgrSupportNull_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool MemMgrSupportNull_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 MemMgrSupportNull_Module_getMask();
// Returns the diagnostics mask for this module
Void MemMgrSupportNull_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
| Instance Object Types |
 |
typedef struct MemMgrSupportNull_Object MemMgrSupportNull_Object;
// Opaque internal representation of an instance object
// Client reference to an instance object
typedef struct MemMgrSupportNull_Struct MemMgrSupportNull_Struct;
// Opaque client structure large enough to hold an instance object
// Convert this instance structure pointer into an instance handle
// Convert this instance handle into an instance structure pointer
| Instance Config Parameters |
 |
typedef struct MemMgrSupportNull_Params {
// Instance config-params structure
// Common per-instance configs
//
} MemMgrSupportNull_Params;
// Initialize this config-params structure with supplier-specified defaults before instance creation
| config MemMgrSupportNull_heapHandle // instance |
 |
| MemMgrSupportNull_alloc() // instance |
 |
ARGUMENTS
handle
handle of a previously-created MemMgrSupportNull instance object
| MemMgrSupportNull_free() // instance |
 |
ARGUMENTS
handle
handle of a previously-created MemMgrSupportNull instance object
| MemMgrSupportNull_translate() // instance |
 |
ARGUMENTS
handle
handle of a previously-created MemMgrSupportNull instance object
| Instance Convertors |
 |
// unconditionally move one level up the inheritance hierarchy
// conditionally move one level down the inheritance hierarchy; NULL upon failure
| Instance Built-Ins |
 |
Int MemMgrSupportNull_Object_count();
// The number of statically-created instance objects
// The handle of the i-th statically-created instance object (array == NULL)
// The handle of the first dynamically-created instance object, or NULL
// The handle of the next dynamically-created instance object, or NULL
// The heap used to allocate dynamically-created instance objects
// The label associated with this instance object
// The name of this instance object