| proxy IFrameQBufMgr.GateProxy |
 |
IGateProvider Proxy
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
DETAILS
Module used to provide default critical region management when accessing
the shared memory. The default is
ti.sdo.ipc.gates.GatePeterson.
Requires Arm to be procId 0 or 1 and the DSP be 1 or 0.
| const IFrameQBufMgr.DYNAMIC_CREATE |
 |
Type of creation
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
const UInt32 DYNAMIC_CREATE = 0x4;
| const IFrameQBufMgr.DYNAMIC_CREATE_USEDREGION |
 |
Type of creation
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
const UInt32 DYNAMIC_CREATE_USEDREGION = 0x8;
| const IFrameQBufMgr.DYNAMIC_FRAME |
 |
Denotes Frame belongs to dynamic frame grougp that are added dynamically at runtime
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
const UInt8 DYNAMIC_FRAME = 2;
| const IFrameQBufMgr.DYNAMIC_OPEN |
 |
Type of open
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
const UInt32 DYNAMIC_OPEN = 0x20;
| const IFrameQBufMgr.FRAMEBUF_CPUACCESSFLAGS_BITOFFSET |
 |
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
const UInt32 FRAMEBUF_CPUACCESSFLAGS_BITOFFSET = 16;
| const IFrameQBufMgr.INVALID |
 |
Type of open
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
const UInt32 INVALID = 0xFF;
| const IFrameQBufMgr.MAX_FRAMEBUFS |
 |
Maximum number of frame buffers in a frame managed by in
FrameQBufMgr instance
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
const UInt32 MAX_FRAMEBUFS = 8;
| const IFrameQBufMgr.MAX_POOLS |
 |
Maximum number of Free Frame pools pools managed by FrameQBufMgr
instance
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
const UInt32 MAX_POOLS = 64;
| const IFrameQBufMgr.POOL_DYNAMIC_MAXFRAMES |
 |
Maximum number of dynbuffers managed by each buffer pool in
FrameQBufMgr instance
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
const UInt32 POOL_DYNAMIC_MAXFRAMES = 1;
| const IFrameQBufMgr.POOL_DYNAMIC_MAXHDRS |
 |
Maximum number of additional dynamic free headers managed by FrameQBufMgr
instance for each Free Frame pool
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
const UInt32 POOL_DYNAMIC_MAXHDRS = 1;
| const IFrameQBufMgr.POOL_MAXFRAMES |
 |
Maximum number of static free Frames managed by FrameQBufMgr
instance for a Free Frame pool
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
const UInt32 POOL_MAXFRAMES = 32;
| const IFrameQBufMgr.POOL_MAXHDRS |
 |
Maximum number of additional static free headers managed by FrameQBufMgr
instance for each Free Frame pool
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
const UInt32 POOL_MAXHDRS = 64;
| const IFrameQBufMgr.STATIC_CREATE |
 |
Type of creation
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
const UInt32 STATIC_CREATE = 0x1;
| const IFrameQBufMgr.STATIC_CREATE_USEDREGION |
 |
Type of creation
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
const UInt32 STATIC_CREATE_USEDREGION = 0x2;
| const IFrameQBufMgr.STATIC_FRAME |
 |
Denotes Frame belongs to static frames that are populated at create time of the instance
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
const UInt8 STATIC_FRAME = 1;
| const IFrameQBufMgr.STATIC_OPEN |
 |
Type of open
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
const UInt32 STATIC_OPEN = 0x10;
| const IFrameQBufMgr.VERSION |
 |
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
const UInt32 VERSION = 1;
| enum IFrameQBufMgr.AddrType |
 |
Enumerations to indicate address types used for translation
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
enum AddrType {
AddrType_Virtual,
AddrType_Portable,
AddrType_EndValue
};
VALUES
AddrType_Virtual
Virtual address on calling process on DSP where
MMU is not configured it could be the physical
address.
AddrType_Portable
This is the shared region address incase
sharedmemory manager plugged in to
frameQbufMgr. In case of tiler it could be the
tiler specific portable address
AddrType_EndValue
End delimiter indicating start of invalid
values for this enum
| enum IFrameQBufMgr.BufType |
 |
Enumerations to indicate address types used for translation
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
enum BufType {
BUF_FRAMEHEADER,
BUF_FRAMEBUF,
BUF_ENDVALUE
};
VALUES
BUF_FRAMEHEADER
Denotes buffer is of type used for frame headers.
BUF_FRAMEBUF
Denotes buffer is of type used for frame buffers
AddrType_EndValue
End delimiter indicating start of invalid
values for this enum
| enum IFrameQBufMgr.CpuAccessFlags |
 |
Enumeration of CPU access flags for frame buffers. For frame headers CPUACCESS is assumed to be TRUE
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
enum CpuAccessFlags {
FRAMEBUF0_CPUACCESS,
FRAMEBUF1_CPUACCESS,
FRAMEBUF2_CPUACCESS,
FRAMEBUF3_CPUACCESS,
FRAMEBUF4_CPUACCESS,
FRAMEBUF5_CPUACCESS,
FRAMEBUF6_CPUACCESS,
FRAMEBUF7_CPUACCESS
};
VALUES
FRAMEBUF0_CPUACCESS
If specified first frame buffer is accessed through CPU(direct memory access).
FRAMEBUF1_CPUACCESS
If specified second frame buffer is accessed through CPU(direct memory access).
FRAMEBUF2_CPUACCESS
If specified third frame buffer is accessed through CPU(direct memory access).
FRAMEBUF3_CPUACCESS
If specified fourth frame buffer is accessed through CPU(direct memory access).
FRAMEBUF4_CPUACCESS
If specified fifth frame buffer is accessed through CPU(direct memory access).
FRAMEBUF5_CPUACCESS
If specified sixth frame buffer is accessed through CPU(direct memory access).
FRAMEBUF6_CPUACCESS
If specified seventh frame buffer is accessed through CPU(direct memory access).
FRAMEBUF7_CPUACCESS
If specified eigth frame buffer is accessed through CPU(direct memory access).
| enum IFrameQBufMgr.Interface |
 |
Enumeration of FrameQBufMgr interface types.Denotes different implementation types
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
enum Interface {
INTERFACE_SHAREDMEM,
INTERFACE_TILERMEM,
INTERFACE_NONE
};
VALUES
INTERFACE_SHAREDMEM
FrameQNufMgr implementation (FrameQBufMgr_ShMem Implementation) on shared memory.
| typedef IFrameQBufMgr.Frame |
 |
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
| typedef IFrameQBufMgr.NotifyFunc |
 |
Prototype of the FrameQbufMgr call back function
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
| typedef IFrameQBufMgr.Status |
 |
type used for API return code
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
| struct IFrameQBufMgr.Attrs |
 |
Shared control strucrue for the instance attributes
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
struct Attrs {
UInt32 status;
UInt32 version;
UInt32 localProtect;
UInt32 remoteProtect;
Ptr gateMPAddr;
Ptr sharedDataBufAddr;
UInt32 sharedAddrSize;
UInt32 numFreeFramePools;
UInt32 numNotifyEntries;
UInt16 entryId;
};
FIELDS
status
Flag denoting whether instance is created or not.
version
Version of the instance.
gateMPAddr
GateMP address (shm safe)
name
Name of the instance.
sharedDataBufAddr
Holds Data buffer start address provided at instance crate time.
sharedAddrSize
The size of the data buffer.
FILED
Number of free frame pools maintained by this instance.
Unique id of the instance in the system. Combination of
creator procId and instance no on that processor.
| struct IFrameQBufMgr.CommonOpenParams |
 |
Common paramters requiredto open a FrameQBufMgr instance of any implementation
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
struct CommonOpenParams {
String name;
UInt32 cpuAccessFlags;
Ptr sharedAddr;
};
FIELDS
name
Name of the instance to open.
(cacheFlags) Cache flags to perform cache operations .
sharedAddr
Shared addr in case open by address is required.
gate
gate for protection.
| struct IFrameQBufMgr.Config |
 |
mouduleconfig structure
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
struct Config {
UInt32 eventNo;
Bool useNameServer;
Bool maxInstances;
};
FIELDS
sharedAddr
Shared region address for module initialization.
sharedAddrSize
Size of the shared region .
(cacheFlags) Cache flags to perform cache operations on module wide shared control structure.
eventNo
The event number used for notification.
name
Name for the module.
shCtrlOpenFlag
Boolean flag if set to FALSE, populate the shared control info
required between processors for this module. If it set to TRUE,
module initialize call opens the shared control info.Ideally master processor
set this flag to FALSE to crate the shared control info.
| struct IFrameQBufMgr.ControlStruct |
 |
Shared control structure for the FrameQBufMgr instance
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
struct ControlStruct {
};
FIELDS
attrs
Shared control info of type Attrs.
| struct IFrameQBufMgr.CreateParams |
 |
Structure defining common instance parameters for the FrameQ
module.Should be the first element in the create params strcture of
the actual implementation
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
struct CreateParams {
UInt32 size;
String name;
Bool openFlag;
};
FIELDS
size
Size of the Create params structure(Should be the size of the actual
implementation's Create params structure in which this FrameQ_CreateParams is the
first element.
interface
type of implementation. See Interface.
name
Name of the instance.
openFlag
Denotes whether create should actually create/open instance.
| struct IFrameQBufMgr.FrameBufInfo |
 |
Structure of the framebuffer info in frame
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
struct FrameBufInfo {
UInt32 bufPtr;
UInt32 bufSize;
UInt32 startOffset;
UInt32 validSize;
UInt32 pixelFormat;
UInt32 height;
UInt32 width;
UInt32 stride;
};
FIELDS
bufPtr
Pointer to the frame buffer.
bufSize
Size of the buffer.
startOffSet
Start offset in the buffer from where valid data starts.
validSize
Valid size in the buffer from the zeroth offset in the frame buffer.
height
Pointer to the frame buffer.
width
Size of the buffer.
stride
Multiple of page size and needs to be added to Tile
start address in order to get the address starting on
next row in same tile.
| struct IFrameQBufMgr.FrameBufParams |
 |
Structure defining common frame buf params for tiled as well as non tiled buffers
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
struct FrameBufParams {
UInt32 size;
UInt32 pixelFormat;
UInt32 height;
UInt32 width;
UInt32 align;
};
FIELDS
size
size for non tiled buffer.
Structure defining parameters for the Tiled data buffers
pixelFormat
pixel format for tiled buffer.
height
height .
width
width .
stride
stride of container, must be multiple of page size.
align
Alignment of the buffer .
| struct IFrameQBufMgr.FrameHeader |
 |
Structure of the base frame header. FrameQ maintains list of frames to be
retrieved by FrameQ reader client. Application is expected to use Helper
API to extract fileds and exteneded header pointer
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
struct FrameHeader {
UInt32 reserved0;
UInt32 reserved1;
UInt16 baseHeaderSize;
UInt16 headerSize;
UInt32 frmAllocaterId;
UInt32 frameBufType;
UInt8 freeFrmQueueNo;
UInt8 numFrameBuffers;
};
FIELDS
baseHeaderSize
Size of the base frame header.
headerSize
Size of the frame header(total size of base header
and extended header).
frmAllocaterId
Denotes the FrameQBufMgr Id from which frame is allocated.
freeFrmQueueNo
Free quque No from which frame is allocated in FrameQBufMgr.
numFrameBuffers
Number of framebuffers in a frame.
| struct IFrameQBufMgr.FreeFramePoolObj |
 |
Free Frame pool structure to keep track of the free frames in a frame pool
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
struct FreeFramePoolObj {
UInt32 numFrms;
UInt32 freeFrms;
UInt32 numFrmHdrBufs;
UInt32 freeFrmHdrBufs;
UInt32 frmHdrBufSize;
UInt32 numBufsInFrame;
UInt32 numDynamicHdrBufs;
UInt32 freeDynamicHdrBufs;
UInt32 numDynamicFrames;
UInt32 freeDynamicFrames;
UInt32 frmStartAddrp;
UInt32 frmEndAddrp;
UInt32 hdrBufStartAddrp;
UInt32 hdrBufEndAddrp;
UInt32 frmBufsStartAddrp;
UInt32 frmBufsEndAddrp;
};
| struct IFrameQBufMgr.NotifyParams |
 |
Structure defining notification parameter structure
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
struct NotifyParams {
UInt32 watermark;
Ptr cbContext;
Ptr cbClientHandle;
};
FIELDS
watermark
Minumum number of free frames required to generate
notification Same water mark for all the individual
freeFramePools in the set.
cbFxnPtr
Cacll back function.
cbContext
Context pointer that needs to be passed to call back
function.
cbClientHandle
Handle that needs to be passed as first arg to
call back.Ideally this should be callers client
handle.
| config IFrameQBufMgr.Attrs_STRUCT_PADDING // module-wide |
 |
Padding required for the Attrs structure
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
| config IFrameQBufMgr.CACHE_LINESIZE // module-wide |
 |
Cache line size
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
config UInt32 CACHE_LINESIZE = 128;
| config IFrameQBufMgr.MAXINSTANCES // module-wide |
 |
Maximum number of instances that can be created for this module
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
config UInt32 MAXINSTANCES = 64;
| config IFrameQBufMgr.MAX_NAMELEN // module-wide |
 |
Maximum length of the name strings
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
config UInt32 MAX_NAMELEN = 32;
| config IFrameQBufMgr.NOTIFY_RESERVED_EVENTNO // module-wide |
 |
Event Number to be used by FrameQBufMgr module
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
config UInt32 NOTIFY_RESERVED_EVENTNO = 3;
| config IFrameQBufMgr.nameServer // module-wide |
 |
Handle to the name server
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
| config IFrameQBufMgr.usedefaultgate // module-wide |
 |
If set to true FrameQBufMgr instances will use dafault gate set in
FrameQBufMgr.
If default gate is not set in FrameQBufMgr, it uses GateMP's default
gate. Set it to zero if FrameQBufMgr needs to create gate for a
instance (remoteProtect and localProtect flags should be valid in
params in this case)
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
config Bool usedefaultgate = false;
| metaonly config IFrameQBufMgr.common$ // module-wide |
 |
Common module configuration parameters
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
| metaonly config IFrameQBufMgr.nameSrvPrms // module-wide |
 |
This Params object is used for temporary storage of the
module wide parameters that are for setting the NameServer instance
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
| metaonly config IFrameQBufMgr.tableSection // module-wide |
 |
Section name is used to place the names table
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
metaonly config String tableSection = null;
| metaonly config IFrameQBufMgr.useNameServer // module-wide |
 |
Whether to have this module use the NameServer or not
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
metaonly config Bool useNameServer = true;
DETAILS
Currently defaulted to false because static creation of NameServer
instances is not supported.
| IFrameQBufMgr.getConfig() // module-wide |
 |
Initialize the passed pointer with the current parameters
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
ARGUMENTS
cfgParams
Pointer to parameter structure to be initialized.
| IFrameQBufMgr.getHandle() // module-wide |
 |
Function to create a nameServer
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
Ptr getHandle(UInt32 id);
ARGUMENTS
id
Id of the FrameQBufMgr instance.
RETURNS
Returns instance handle if it is created or opened on the caller processor.
| IFrameQBufMgr.add() // instance |
 |
Function to add free frames dynamically which are allocated out side of
FrmaeQbufMgr through the same memory manager
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
ARGUMENTS
freeQId
freeFrame Pool No to whcih the frame needs to be
added.
framePtr
frame to be added.
RETURNS
returns 0 if successfully added the frame.
| IFrameQBufMgr.alloc() // instance |
 |
Function to allocate a buffer from the FrameQBufMgr instance
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
ARGUMENTS
frame
Location to receive the allocated frame pointer.
RETURNS
returns 0 if successfully allocated the buffer.
| IFrameQBufMgr.allocv() // instance |
 |
Function to allocate multiple frames from the FrameQBufMgr instance from
the free Frame pool nos given
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
ARGUMENTS
framePtr
array of pointers to receive allocate frame pointers.
freeQId
array of freeFrame poolNos to allocate frames from.
if API retruns success, this represents ths actual size of the buffer allocated.
numFrames
Number of frames to allocate.
RETURNS
returns value greater than zero
if successfully allocated frames.
| IFrameQBufMgr.control() // instance |
 |
Provides a hook to perform implementation dependent operation
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
Int32 control(Int32 cmd, Ptr arg);
ARGUMENTS
cmd
command to exectue.
arg
argument of type void*.
| IFrameQBufMgr.dup() // instance |
 |
API to duplicate the given frame i.e it increments the corresponding
frames 's reference count.It internally allocates headers for the duped
frames.It fails if it is not able to dup all the frames
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
ARGUMENTS
buf
Pointer to the frame which needs to be duplicated.
size
Size of the buffer.
dupCount
Duplication count.
| IFrameQBufMgr.dupv() // instance |
 |
API to duplicate the given frames i.e it increments the corresponding
frames 's reference count.It internally allocates headers for the duped
frames.It fails if it is not able to dup all the frames
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
ARGUMENTS
buf
Pointer to the frames which needs to be duplicated.
size
Size of the buffer.
dupCount
Duplication count.
| IFrameQBufMgr.free() // instance |
 |
Function to free frame
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
ARGUMENTS
frame
frame to be freed.
RETURNS
returns 0 if successfully freed the allocated buffer.
| IFrameQBufMgr.freev() // instance |
 |
Function to free frames
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
ARGUMENTS
framePtr
array of frames to be freed.
RETURNS
returns 0 if successfully freed the allocated frames.
| IFrameQBufMgr.getId() // instance |
 |
Function to get the id of the instance
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
RETURNS
Returns FrameQBufMgr Id for the handle.
| IFrameQBufMgr.getNumFreeFrames() // instance |
 |
Function to get the number of free frames available in the in
FrameQbufMgr's FreeFramePool 0. The returned number free frame may not
exist in the frameQbufMgr after this call.This is because
if any allocs are done by the other FrameQ writers on the
same FrameQBufMgr.If frees are not other frameQ writers the free Frames
would be even more than the value that we have got
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
Int32 getNumFreeFrames(UInt32 *numFreeFrames);
ARGUMENTS
numFrames
Outputparameter indicates number of free frames
.
RETURNS
returns 0 if successfully returned the number of
free frames.
| IFrameQBufMgr.getvNumFreeFrames() // instance |
 |
Function to get the number of free frames available in the in the given
Free FramePool
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
Int32 getvNumFreeFrames(UInt32 numFreeFrames[], UInt8 freeFramePoolNo[], UInt8 numFreeFramePools);
ARGUMENTS
numFreeFrames
Outputparameter indicates number of free frames in
each given free quque at that instance.
filledQId
Array of free Queue ids(freeFramePool nos).
numFreeQids
Number of free queueids same as freeFrame PoolNo of
plugged in FrameQBufMgr .
RETURNS
returns 0 if successfully returned the frames.
| IFrameQBufMgr.invalidate() // instance |
 |
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
| IFrameQBufMgr.invalidateFrameBuf() // instance |
 |
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
Int32 invalidateFrameBuf(Ptr frameBuf, UInt32 size, UInt8 bufNumInFrame);
| IFrameQBufMgr.invalidateHeaderBuf() // instance |
 |
invalidates contents of buffer . buffer is treated as frame header
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
Int32 invalidateHeaderBuf(Ptr headerBuf);
| IFrameQBufMgr.isCacheEnabledForFrameBuf() // instance |
 |
Function to determine whether cache calls(writeback/invalidate) are
enabled for frame buffers
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
Bool isCacheEnabledForFrameBuf(UInt8 framebufIndex);
| IFrameQBufMgr.isCacheEnabledForHeaderBuf() // instance |
 |
Function to determine whether cache calls(writeback/invalidate) are
enabled for frame headers
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
Bool isCacheEnabledForHeaderBuf();
| IFrameQBufMgr.registerNotifier() // instance |
 |
Function to Register notification with the instance. It internally registers
notification with the individual free queues(free frame pools).
If alloc on free queue 0 failed,Notification will be generated if free frames
in that queue becomes more than watermark(all the free frames in that queue)
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
ARGUMENTS
RETURNS
returns >0 if successfully registered the call back function.
| IFrameQBufMgr.remove() // instance |
 |
Function to remove dynamically added frames which are allocated out side of
FrmaeQbufMgr through the same memory managers that are plugged in to
FrameQBufMgr instance
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
ARGUMENTS
freeQId
freeFrame Pool No to whcih the frame needs to be
added.
framePtr
frame to be added.
RETURNS
returns 0 if successfully added the frame.
| IFrameQBufMgr.translateAddr() // instance |
 |
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
| IFrameQBufMgr.unregisterNotifier() // instance |
 |
Function to unregister the registered call back function with the instance.
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
Int32 unregisterNotifier();
RETURNS
Returns positive value if successfully unregistered the call back function.
| IFrameQBufMgr.writeBack() // instance |
 |
Write back the contents of a frame including frame buffers
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
| IFrameQBufMgr.writeBackFrameBuf() // instance |
 |
Write back the contents of buffer . buffe is treated as frame buffer.
bufNumInFrame denotes buffer number in the frame.This is to identify
the cache flags and cpu access flags for the buffer
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
Int32 writeBackFrameBuf(Ptr frameBuf, UInt32 size, UInt8 bufNumInFrame);
| IFrameQBufMgr.writeBackHeaderBuf() // instance |
 |
Write back the contents of buffer.buffer is treated as frame header
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrameQBufMgr.xdc |
Int32 writeBackHeaderBuf(Ptr headerBuf);