| typedef IFrame.Frame |
 |
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrame.xdc |
| struct IFrame.FrameBufInfo |
 |
Structure of the framebuffer info in frame
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrame.xdc |
struct FrameBufInfo {
UInt32 bufPtr;
UInt32 bufSize;
UInt32 startOffset;
UInt32 validSize;
UInt32 pixelFormat;
UInt32 height;
UInt32 width;
UInt32 stride;
};
FIELDS
bufPtr
Pointer to the frame buffer.
bufSize
Size of the buffer.
startOffSet
Start offset in the buffer from where valid data starts.
validSize
Valid size in the buffer from the zeroth offset in the frame buffer.
height
Pointer to the frame buffer.
width
Size of the buffer.
stride
Multiple of page size and needs to be added to Tile
start address in order to get the address starting on
next row in same tile.
| struct IFrame.FrameHeader |
 |
Structure of the base frame header. FrameQ maintains list of frames to be
retrieved by FrameQ reader client. Application is expected to use Helper
API to extract fileds and exteneded header pointer
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrame.xdc |
struct FrameHeader {
UInt32 reserved0;
UInt32 reserved1;
UInt16 baseHeaderSize;
UInt16 headerSize;
UInt32 frmAllocaterId;
UInt32 frameBufType;
UInt8 freeFrmQueueNo;
UInt8 numFrameBuffers;
};
FIELDS
baseHeaderSize
Size of the base frame header.
headerSize
Size of the frame header(total size of base header
and extended header).
frmAllocaterId
Denotes the FrameQBufMgr Id from which frame is allocated.
freeFrmQueueNo
Free quque No from which frame is allocated in FrameQBufMgr.
numFrameBuffers
Number of framebuffers in a frame.
| metaonly config IFrame.common$ // module-wide |
 |
Common module configuration parameters
| XDCspec declarations |
sourced in ti/syslink/ipc/rtos/interfaces/IFrame.xdc |
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.