| const FrameQBufMgr_DYNAMIC_CREATE |
 |
Type of creation
#define FrameQBufMgr_DYNAMIC_CREATE (UInt32)0x4
| const FrameQBufMgr_DYNAMIC_CREATE_USEDREGION |
 |
Type of creation
#define FrameQBufMgr_DYNAMIC_CREATE_USEDREGION (UInt32)0x8
| const FrameQBufMgr_DYNAMIC_FRAME |
 |
Denotes Frame belongs to dynamic frame grougp that are added dynamically at runtime
#define FrameQBufMgr_DYNAMIC_FRAME (UInt8)2
| const FrameQBufMgr_DYNAMIC_OPEN |
 |
Type of open
#define FrameQBufMgr_DYNAMIC_OPEN (UInt32)0x20
| const FrameQBufMgr_FRAMEBUF_CPUACCESSFLAGS_BITOFFSET |
 |
#define FrameQBufMgr_FRAMEBUF_CPUACCESSFLAGS_BITOFFSET (UInt32)16
| const FrameQBufMgr_INVALID |
 |
Type of open
#define FrameQBufMgr_INVALID (UInt32)0xFF
| const FrameQBufMgr_MAX_FRAMEBUFS |
 |
Maximum number of frame buffers in a frame managed by in
FrameQBufMgr instance
#define FrameQBufMgr_MAX_FRAMEBUFS (UInt32)8
| const FrameQBufMgr_MAX_POOLS |
 |
Maximum number of Free Frame pools pools managed by FrameQBufMgr
instance
#define FrameQBufMgr_MAX_POOLS (UInt32)64
| const FrameQBufMgr_POOL_DYNAMIC_MAXFRAMES |
 |
Maximum number of dynbuffers managed by each buffer pool in
FrameQBufMgr instance
#define FrameQBufMgr_POOL_DYNAMIC_MAXFRAMES (UInt32)1
| const FrameQBufMgr_POOL_DYNAMIC_MAXHDRS |
 |
Maximum number of additional dynamic free headers managed by FrameQBufMgr
instance for each Free Frame pool
#define FrameQBufMgr_POOL_DYNAMIC_MAXHDRS (UInt32)1
| const FrameQBufMgr_POOL_MAXFRAMES |
 |
Maximum number of static free Frames managed by FrameQBufMgr
instance for a Free Frame pool
#define FrameQBufMgr_POOL_MAXFRAMES (UInt32)32
| const FrameQBufMgr_POOL_MAXHDRS |
 |
Maximum number of additional static free headers managed by FrameQBufMgr
instance for each Free Frame pool
#define FrameQBufMgr_POOL_MAXHDRS (UInt32)64
| const FrameQBufMgr_STATIC_CREATE |
 |
Type of creation
#define FrameQBufMgr_STATIC_CREATE (UInt32)0x1
| const FrameQBufMgr_STATIC_CREATE_USEDREGION |
 |
Type of creation
#define FrameQBufMgr_STATIC_CREATE_USEDREGION (UInt32)0x2
| const FrameQBufMgr_STATIC_FRAME |
 |
Denotes Frame belongs to static frames that are populated at create time of the instance
#define FrameQBufMgr_STATIC_FRAME (UInt8)1
| const FrameQBufMgr_STATIC_OPEN |
 |
Type of open
#define FrameQBufMgr_STATIC_OPEN (UInt32)0x10
| const FrameQBufMgr_VERSION |
 |
#define FrameQBufMgr_VERSION (UInt32)1
| enum FrameQBufMgr_AddrType |
 |
Enumerations to indicate address types used for translation
typedef enum FrameQBufMgr_AddrType {
FrameQBufMgr_AddrType_Virtual,
FrameQBufMgr_AddrType_Portable,
FrameQBufMgr_AddrType_EndValue
} FrameQBufMgr_AddrType;
VALUES
AddrType_Virtual
Virtual address on calling process on DSP where
MMU is not configured it could be the physical
address.
AddrType_Portable
This is the shared region address incase
sharedmemory manager plugged in to
frameQbufMgr. In case of tiler it could be the
tiler specific portable address
AddrType_EndValue
End delimiter indicating start of invalid
values for this enum
| enum FrameQBufMgr_BufType |
 |
Enumerations to indicate address types used for translation
typedef enum FrameQBufMgr_BufType {
FrameQBufMgr_BUF_FRAMEHEADER,
FrameQBufMgr_BUF_FRAMEBUF,
FrameQBufMgr_BUF_ENDVALUE
} FrameQBufMgr_BufType;
VALUES
BUF_FRAMEHEADER
Denotes buffer is of type used for frame headers.
BUF_FRAMEBUF
Denotes buffer is of type used for frame buffers
AddrType_EndValue
End delimiter indicating start of invalid
values for this enum
| enum FrameQBufMgr_CpuAccessFlags |
 |
Enumeration of CPU access flags for frame buffers. For frame headers CPUACCESS is assumed to be TRUE
typedef enum FrameQBufMgr_CpuAccessFlags {
FrameQBufMgr_FRAMEBUF0_CPUACCESS,
FrameQBufMgr_FRAMEBUF1_CPUACCESS,
FrameQBufMgr_FRAMEBUF2_CPUACCESS,
FrameQBufMgr_FRAMEBUF3_CPUACCESS,
FrameQBufMgr_FRAMEBUF4_CPUACCESS,
FrameQBufMgr_FRAMEBUF5_CPUACCESS,
FrameQBufMgr_FRAMEBUF6_CPUACCESS,
FrameQBufMgr_FRAMEBUF7_CPUACCESS
} FrameQBufMgr_CpuAccessFlags;
VALUES
FRAMEBUF0_CPUACCESS
If specified first frame buffer is accessed through CPU(direct memory access).
FRAMEBUF1_CPUACCESS
If specified second frame buffer is accessed through CPU(direct memory access).
FRAMEBUF2_CPUACCESS
If specified third frame buffer is accessed through CPU(direct memory access).
FRAMEBUF3_CPUACCESS
If specified fourth frame buffer is accessed through CPU(direct memory access).
FRAMEBUF4_CPUACCESS
If specified fifth frame buffer is accessed through CPU(direct memory access).
FRAMEBUF5_CPUACCESS
If specified sixth frame buffer is accessed through CPU(direct memory access).
FRAMEBUF6_CPUACCESS
If specified seventh frame buffer is accessed through CPU(direct memory access).
FRAMEBUF7_CPUACCESS
If specified eigth frame buffer is accessed through CPU(direct memory access).
| enum FrameQBufMgr_Interface |
 |
Enumeration of FrameQBufMgr interface types.Denotes different implementation types
typedef enum FrameQBufMgr_Interface {
FrameQBufMgr_INTERFACE_SHAREDMEM,
FrameQBufMgr_INTERFACE_TILERMEM,
FrameQBufMgr_INTERFACE_NONE
} FrameQBufMgr_Interface;
VALUES
INTERFACE_SHAREDMEM
FrameQNufMgr implementation (FrameQBufMgr_ShMem Implementation) on shared memory.
| typedef FrameQBufMgr_Frame |
 |
| typedef FrameQBufMgr_NotifyFunc |
 |
Prototype of the FrameQbufMgr call back function
| typedef FrameQBufMgr_Status |
 |
type used for API return code
typedef UInt32 FrameQBufMgr_Status;
| struct FrameQBufMgr_Attrs |
 |
Shared control strucrue for the instance attributes
typedef struct FrameQBufMgr_Attrs {
UInt32 status;
UInt32 version;
UInt32 localProtect;
UInt32 remoteProtect;
Ptr gateMPAddr;
Ptr sharedDataBufAddr;
UInt32 sharedAddrSize;
UInt32 numFreeFramePools;
UInt32 numNotifyEntries;
UInt16 entryId;
} FrameQBufMgr_Attrs;
FIELDS
status
Flag denoting whether instance is created or not.
version
Version of the instance.
gateMPAddr
GateMP address (shm safe)
name
Name of the instance.
sharedDataBufAddr
Holds Data buffer start address provided at instance crate time.
sharedAddrSize
The size of the data buffer.
FILED
Number of free frame pools maintained by this instance.
Unique id of the instance in the system. Combination of
creator procId and instance no on that processor.
| struct FrameQBufMgr_CommonOpenParams |
 |
Common paramters requiredto open a FrameQBufMgr instance of any implementation
typedef struct FrameQBufMgr_CommonOpenParams {
String name;
UInt32 cpuAccessFlags;
Ptr sharedAddr;
} FrameQBufMgr_CommonOpenParams;
FIELDS
name
Name of the instance to open.
(cacheFlags) Cache flags to perform cache operations .
sharedAddr
Shared addr in case open by address is required.
gate
gate for protection.
| struct FrameQBufMgr_Config |
 |
mouduleconfig structure
typedef struct FrameQBufMgr_Config {
UInt32 eventNo;
Bool useNameServer;
Bool maxInstances;
} FrameQBufMgr_Config;
FIELDS
sharedAddr
Shared region address for module initialization.
sharedAddrSize
Size of the shared region .
(cacheFlags) Cache flags to perform cache operations on module wide shared control structure.
eventNo
The event number used for notification.
name
Name for the module.
shCtrlOpenFlag
Boolean flag if set to FALSE, populate the shared control info
required between processors for this module. If it set to TRUE,
module initialize call opens the shared control info.Ideally master processor
set this flag to FALSE to crate the shared control info.
| struct FrameQBufMgr_ControlStruct |
 |
Shared control structure for the FrameQBufMgr instance
typedef struct FrameQBufMgr_ControlStruct {
} FrameQBufMgr_ControlStruct;
FIELDS
attrs
Shared control info of type Attrs.
| struct FrameQBufMgr_CreateParams |
 |
Structure defining common instance parameters for the FrameQ
module.Should be the first element in the create params strcture of
the actual implementation
typedef struct FrameQBufMgr_CreateParams {
UInt32 size;
String name;
Bool openFlag;
} FrameQBufMgr_CreateParams;
FIELDS
size
Size of the Create params structure(Should be the size of the actual
implementation's Create params structure in which this FrameQ_CreateParams is the
first element.
interface
type of implementation. See Interface.
name
Name of the instance.
openFlag
Denotes whether create should actually create/open instance.
| struct FrameQBufMgr_FrameBufInfo |
 |
Structure of the framebuffer info in frame
typedef struct FrameQBufMgr_FrameBufInfo {
UInt32 bufPtr;
UInt32 bufSize;
UInt32 startOffset;
UInt32 validSize;
UInt32 pixelFormat;
UInt32 height;
UInt32 width;
UInt32 stride;
} FrameQBufMgr_FrameBufInfo;
FIELDS
bufPtr
Pointer to the frame buffer.
bufSize
Size of the buffer.
startOffSet
Start offset in the buffer from where valid data starts.
validSize
Valid size in the buffer from the zeroth offset in the frame buffer.
height
Pointer to the frame buffer.
width
Size of the buffer.
stride
Multiple of page size and needs to be added to Tile
start address in order to get the address starting on
next row in same tile.
| struct FrameQBufMgr_FrameBufParams |
 |
Structure defining common frame buf params for tiled as well as non tiled buffers
typedef struct FrameQBufMgr_FrameBufParams {
UInt32 size;
UInt32 pixelFormat;
UInt32 height;
UInt32 width;
UInt32 align;
} FrameQBufMgr_FrameBufParams;
FIELDS
size
size for non tiled buffer.
Structure defining parameters for the Tiled data buffers
pixelFormat
pixel format for tiled buffer.
height
height .
width
width .
stride
stride of container, must be multiple of page size.
align
Alignment of the buffer .
| struct FrameQBufMgr_FrameHeader |
 |
Structure of the base frame header. FrameQ maintains list of frames to be
retrieved by FrameQ reader client. Application is expected to use Helper
API to extract fileds and exteneded header pointer
typedef struct FrameQBufMgr_FrameHeader {
UInt32 reserved0;
UInt32 reserved1;
UInt16 baseHeaderSize;
UInt16 headerSize;
UInt32 frmAllocaterId;
UInt32 frameBufType;
UInt8 freeFrmQueueNo;
UInt8 numFrameBuffers;
} FrameQBufMgr_FrameHeader;
FIELDS
baseHeaderSize
Size of the base frame header.
headerSize
Size of the frame header(total size of base header
and extended header).
frmAllocaterId
Denotes the FrameQBufMgr Id from which frame is allocated.
freeFrmQueueNo
Free quque No from which frame is allocated in FrameQBufMgr.
numFrameBuffers
Number of framebuffers in a frame.
| struct FrameQBufMgr_FreeFramePoolObj |
 |
Free Frame pool structure to keep track of the free frames in a frame pool
typedef struct FrameQBufMgr_FreeFramePoolObj {
UInt32 numFrms;
UInt32 freeFrms;
UInt32 numFrmHdrBufs;
UInt32 freeFrmHdrBufs;
UInt32 frmHdrBufSize;
UInt32 numBufsInFrame;
UInt32 numDynamicHdrBufs;
UInt32 freeDynamicHdrBufs;
UInt32 numDynamicFrames;
UInt32 freeDynamicFrames;
UInt32 frmStartAddrp;
UInt32 frmEndAddrp;
UInt32 hdrBufStartAddrp;
UInt32 hdrBufEndAddrp;
UInt32 frmBufsStartAddrp;
UInt32 frmBufsEndAddrp;
} FrameQBufMgr_FreeFramePoolObj;
| struct FrameQBufMgr_NotifyParams |
 |
Structure defining notification parameter structure
typedef struct FrameQBufMgr_NotifyParams {
UInt32 watermark;
Ptr cbContext;
Ptr cbClientHandle;
} FrameQBufMgr_NotifyParams;
FIELDS
watermark
Minumum number of free frames required to generate
notification Same water mark for all the individual
freeFramePools in the set.
cbFxnPtr
Cacll back function.
cbContext
Context pointer that needs to be passed to call back
function.
cbClientHandle
Handle that needs to be passed as first arg to
call back.Ideally this should be callers client
handle.
| struct FrameQBufMgr_ShMem_InstNameServerEntryParams |
 |
Structure defining Additional specific parameters that name server maintains
alonh with the interface type
typedef struct FrameQBufMgr_ShMem_InstNameServerEntryParams {
Ptr sharedAddr;
UInt32 sharedAddrSize;
Ptr instGateMPAddr;
UInt8 frmBuf_regionId;
UInt8 hdrBuf_regionId;
Ptr cliGateMPAddr;
} FrameQBufMgr_ShMem_InstNameServerEntryParams;
FIELDS
sharedAddr
Virtual shared Region Address for control structure.
sharedAddrSize
Size of the shared memory for control structure.
instGateMPAddr
Instance gateMP shared address in
SharedRegion_SRPtr format.Valid only if it
is created internally.
memMgrType_HdrBufs
MemMgr type configured for Header buffers.
memMgrType_FrmBufs
MemMgr type configured for Frame buffers.
allocaterName_HdrBufs
Name of the HeapMemMp instance to be used
Header buffer allocation.
TODO: need to check if it is valid for
Tiler
allocaterName_FrmBufs
Name of the HeapMemMp instance to be used
frame buffer allocation.
TODO: need to check if it is valid for
Tiler
| config FrameQBufMgr_A_InvalidCreatorProcId // module-wide |
 |
Assert raised when creator processor id of the instance is not valid
extern const Assert_Id FrameQBufMgr_A_InvalidCreatorProcId;
| config FrameQBufMgr_A_InvalidInstNo // module-wide |
 |
Assert raised when Inst No of the instance is not valid
extern const Assert_Id FrameQBufMgr_A_InvalidInstNo;
| config FrameQBufMgr_A_invalidParams // module-wide |
 |
Assert raised when an invalid parameter(s) is passed into a function
extern const Assert_Id FrameQBufMgr_A_invalidParams;
| config FrameQBufMgr_A_nullHandle // module-wide |
 |
Assert raised when null handle is returned from modules
extern const Assert_Id FrameQBufMgr_A_nullHandle;
| config FrameQBufMgr_A_nullPointer // module-wide |
 |
Assert raised when a null pointer needs to be dereferenced
extern const Assert_Id FrameQBufMgr_A_nullPointer;
| config FrameQBufMgr_Attrs_STRUCT_PADDING // module-wide |
 |
Padding required for the Attrs structure
extern const UInt32 FrameQBufMgr_Attrs_STRUCT_PADDING;
| config FrameQBufMgr_CACHE_LINESIZE // module-wide |
 |
Cache line size
extern const UInt32 FrameQBufMgr_CACHE_LINESIZE;
| config FrameQBufMgr_E_CacheAlign // module-wide |
 |
Error raised when buffersize is not aligned to Cache line size
extern const Error_Id FrameQBufMgr_E_CacheAlign;
| config FrameQBufMgr_E_ClientNotifyMgrCreate // module-wide |
 |
Error raised when ClientNotifyMgr Create failed
extern const Error_Id FrameQBufMgr_E_ClientNotifyMgrCreate;
| config FrameQBufMgr_E_ClientNotifyMgrOpen // module-wide |
 |
Error raised when ClientNotifyMgrOpen failed
extern const Error_Id FrameQBufMgr_E_ClientNotifyMgrOpen;
| config FrameQBufMgr_E_FrameQBufMgrCreateFail // module-wide |
 |
Error raised when internal FrameQBufMgr create failed
extern const Error_Id FrameQBufMgr_E_FrameQBufMgrCreateFail;
| config FrameQBufMgr_E_FrameQBufMgrNotCreated // module-wide |
 |
Error raised when FrameQBufMgr is not created
extern const Error_Id FrameQBufMgr_E_FrameQBufMgrNotCreated;
| config FrameQBufMgr_E_FrameQBufMgrNotFound // module-wide |
 |
Error raised when FrameQBufMgr is not Found in NameServer
extern const Error_Id FrameQBufMgr_E_FrameQBufMgrNotFound;
| config FrameQBufMgr_E_FrameQBufMgrOpenFail // module-wide |
 |
Error raised when FrameQBufMgr open failed
extern const Error_Id FrameQBufMgr_E_FrameQBufMgrOpenFail;
| config FrameQBufMgr_E_InstanceExists // module-wide |
 |
Error raised when an instance already exists
extern const Error_Id FrameQBufMgr_E_InstanceExists;
| config FrameQBufMgr_E_InvAddr // module-wide |
 |
Error raised when Insufficient shared addrprovided to create call
extern const Error_Id FrameQBufMgr_E_InvAddr;
| config FrameQBufMgr_E_InvSize // module-wide |
 |
Error raised when Insufficient shared memory provided to create call
extern const Error_Id FrameQBufMgr_E_InvSize;
| config FrameQBufMgr_E_InvalidInterfaceType // module-wide |
 |
Error raised when an invalid interface type mentioned in params
extern const Error_Id FrameQBufMgr_E_InvalidInterfaceType;
| config FrameQBufMgr_E_InvalidParams // module-wide |
 |
Error raised when an invalid parameter(s) is passed into a function
extern const Error_Id FrameQBufMgr_E_InvalidParams;
| config FrameQBufMgr_E_maxInstances // module-wide |
 |
Error raised when max instances limit is reached
extern const Error_Id FrameQBufMgr_E_maxInstances;
| config FrameQBufMgr_MAXINSTANCES // module-wide |
 |
Maximum number of instances that can be created for this module
extern const UInt32 FrameQBufMgr_MAXINSTANCES;
| config FrameQBufMgr_MAX_NAMELEN // module-wide |
 |
Maximum length of the name strings
extern const UInt32 FrameQBufMgr_MAX_NAMELEN;
| config FrameQBufMgr_NOTIFY_RESERVED_EVENTNO // module-wide |
 |
Event Number to be used by FrameQBufMgr module
extern const UInt32 FrameQBufMgr_NOTIFY_RESERVED_EVENTNO;
| config FrameQBufMgr_nameServer // module-wide |
 |
Handle to the name server
| config FrameQBufMgr_usedefaultgate // module-wide |
 |
If set to true FrameQBufMgr instances will use dafault gate set in
FrameQBufMgr.
If default gate is not set in FrameQBufMgr, it uses GateMP's default
gate. Set it to zero if FrameQBufMgr needs to create gate for a
instance (remoteProtect and localProtect flags should be valid in
params in this case)
extern const Bool FrameQBufMgr_usedefaultgate;
| FrameQBufMgr_getBaseHeaderSize() // module-wide |
 |
API to open the created instance and to get a handle to it
UInt32 FrameQBufMgr_getBaseHeaderSize(UInt8 numFrameBufs);
ARGUMENTS
handlePtr
Handle to the instance will be returned through this pointer.
openParams
open parameters specific implementation.
Function to close the dynamically opened instance using
open call.
numFrameBufs
Number of frame buffers in frame.
RETURNS
returns 0 if successfully registered the call back function.
Retruns the base header size of frame based on the number of frame buffers
that will be contained in frame.
Base frame header size in bytes.
DETAILS
The instance must be created usng create call before opening it.
| FrameQBufMgr_getConfig() // module-wide |
 |
Initialize the passed pointer with the current parameters
ARGUMENTS
cfgParams
Pointer to parameter structure to be initialized.
| FrameQBufMgr_getHandle() // module-wide |
 |
Function to create a nameServer
Ptr FrameQBufMgr_getHandle(UInt32 id);
ARGUMENTS
id
Id of the FrameQBufMgr instance.
RETURNS
Returns instance handle if it is created or opened on the caller processor.
| Module-Wide Built-Ins |
 |
// Get this module's unique id
Bool FrameQBufMgr_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool FrameQBufMgr_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 FrameQBufMgr_Module_getMask();
// Returns the diagnostics mask for this module
Void FrameQBufMgr_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
| Instance Object Types |
 |
typedef struct FrameQBufMgr_Object FrameQBufMgr_Object;
// Opaque internal representation of an instance object
// Client reference to an instance object
typedef struct FrameQBufMgr_Struct FrameQBufMgr_Struct;
// Opaque client structure large enough to hold an instance object
// Convert this instance structure pointer into an instance handle
// Convert this instance handle into an instance structure pointer
| Instance Config Parameters |
 |
typedef struct FrameQBufMgr_Params {
// Instance config-params structure
// Common per-instance configs
//
Ptr impParams;
// Pointer to implementation specific parameters
UInt32 impParamsSize;
// Pointer to implementation specific parameters
} FrameQBufMgr_Params;
// Initialize this config-params structure with supplier-specified defaults before instance creation
| config FrameQBufMgr_commonCreateParams // instance |
 |
| config FrameQBufMgr_impParams // instance |
 |
Pointer to implementation specific parameters
| config FrameQBufMgr_impParamsSize // instance |
 |
Pointer to implementation specific parameters
...
UInt32 impParamsSize;
| FrameQBufMgr_add() // instance |
 |
Function to add free frames dynamically which are allocated out side of
FrmaeQbufMgr through the same memory manager
ARGUMENTS
handle
handle of a previously-created FrameQBufMgr instance object
freeQId
freeFrame Pool No to whcih the frame needs to be
added.
framePtr
frame to be added.
RETURNS
returns 0 if successfully added the frame.
| FrameQBufMgr_alloc() // instance |
 |
Function to allocate a buffer from the FrameQBufMgr instance
ARGUMENTS
handle
handle of a previously-created FrameQBufMgr instance object
frame
Location to receive the allocated frame pointer.
RETURNS
returns 0 if successfully allocated the buffer.
| FrameQBufMgr_allocv() // instance |
 |
Function to allocate multiple frames from the FrameQBufMgr instance from
the free Frame pool nos given
ARGUMENTS
handle
handle of a previously-created FrameQBufMgr instance object
framePtr
array of pointers to receive allocate frame pointers.
freeQId
array of freeFrame poolNos to allocate frames from.
if API retruns success, this represents ths actual size of the buffer allocated.
numFrames
Number of frames to allocate.
RETURNS
returns value greater than zero
if successfully allocated frames.
| FrameQBufMgr_control() // instance |
 |
Provides a hook to perform implementation dependent operation
ARGUMENTS
handle
handle of a previously-created FrameQBufMgr instance object
cmd
command to exectue.
arg
argument of type void*.
| FrameQBufMgr_dup() // instance |
 |
API to duplicate the given frame i.e it increments the corresponding
frames 's reference count.It internally allocates headers for the duped
frames.It fails if it is not able to dup all the frames
ARGUMENTS
handle
handle of a previously-created FrameQBufMgr instance object
buf
Pointer to the frame which needs to be duplicated.
size
Size of the buffer.
dupCount
Duplication count.
| FrameQBufMgr_dupv() // instance |
 |
API to duplicate the given frames i.e it increments the corresponding
frames 's reference count.It internally allocates headers for the duped
frames.It fails if it is not able to dup all the frames
ARGUMENTS
handle
handle of a previously-created FrameQBufMgr instance object
buf
Pointer to the frames which needs to be duplicated.
size
Size of the buffer.
dupCount
Duplication count.
| FrameQBufMgr_free() // instance |
 |
Function to free frame
ARGUMENTS
handle
handle of a previously-created FrameQBufMgr instance object
frame
frame to be freed.
RETURNS
returns 0 if successfully freed the allocated buffer.
| FrameQBufMgr_freev() // instance |
 |
Function to free frames
ARGUMENTS
handle
handle of a previously-created FrameQBufMgr instance object
framePtr
array of frames to be freed.
RETURNS
returns 0 if successfully freed the allocated frames.
| FrameQBufMgr_getId() // instance |
 |
Function to get the id of the instance
ARGUMENTS
handle
handle of a previously-created FrameQBufMgr instance object
RETURNS
Returns FrameQBufMgr Id for the handle.
| FrameQBufMgr_getNumFreeFrames() // instance |
 |
Function to get the number of free frames available in the in
FrameQbufMgr's FreeFramePool 0. The returned number free frame may not
exist in the frameQbufMgr after this call.This is because
if any allocs are done by the other FrameQ writers on the
same FrameQBufMgr.If frees are not other frameQ writers the free Frames
would be even more than the value that we have got
ARGUMENTS
handle
handle of a previously-created FrameQBufMgr instance object
numFrames
Outputparameter indicates number of free frames
.
RETURNS
returns 0 if successfully returned the number of
free frames.
| FrameQBufMgr_getvNumFreeFrames() // instance |
 |
Function to get the number of free frames available in the in the given
Free FramePool
Int32 FrameQBufMgr_getvNumFreeFrames(
FrameQBufMgr_Handle handle,
UInt32 numFreeFrames[
],
UInt8 freeFramePoolNo[
],
UInt8 numFreeFramePools);
ARGUMENTS
handle
handle of a previously-created FrameQBufMgr instance object
numFreeFrames
Outputparameter indicates number of free frames in
each given free quque at that instance.
filledQId
Array of free Queue ids(freeFramePool nos).
numFreeQids
Number of free queueids same as freeFrame PoolNo of
plugged in FrameQBufMgr .
RETURNS
returns 0 if successfully returned the frames.
| FrameQBufMgr_invalidate() // instance |
 |
ARGUMENTS
handle
handle of a previously-created FrameQBufMgr instance object
| FrameQBufMgr_invalidateFrameBuf() // instance |
 |
Int32 FrameQBufMgr_invalidateFrameBuf(
FrameQBufMgr_Handle handle,
Ptr frameBuf,
UInt32 size,
UInt8 bufNumInFrame);
ARGUMENTS
handle
handle of a previously-created FrameQBufMgr instance object
| FrameQBufMgr_invalidateHeaderBuf() // instance |
 |
invalidates contents of buffer . buffer is treated as frame header
ARGUMENTS
handle
handle of a previously-created FrameQBufMgr instance object
| FrameQBufMgr_isCacheEnabledForFrameBuf() // instance |
 |
Function to determine whether cache calls(writeback/invalidate) are
enabled for frame buffers
ARGUMENTS
handle
handle of a previously-created FrameQBufMgr instance object
| FrameQBufMgr_isCacheEnabledForHeaderBuf() // instance |
 |
Function to determine whether cache calls(writeback/invalidate) are
enabled for frame headers
ARGUMENTS
handle
handle of a previously-created FrameQBufMgr instance object
| FrameQBufMgr_registerNotifier() // instance |
 |
Function to Register notification with the instance. It internally registers
notification with the individual free queues(free frame pools).
If alloc on free queue 0 failed,Notification will be generated if free frames
in that queue becomes more than watermark(all the free frames in that queue)
ARGUMENTS
handle
handle of a previously-created FrameQBufMgr instance object
RETURNS
returns >0 if successfully registered the call back function.
| FrameQBufMgr_remove() // instance |
 |
Function to remove dynamically added frames which are allocated out side of
FrmaeQbufMgr through the same memory managers that are plugged in to
FrameQBufMgr instance
ARGUMENTS
handle
handle of a previously-created FrameQBufMgr instance object
freeQId
freeFrame Pool No to whcih the frame needs to be
added.
framePtr
frame to be added.
RETURNS
returns 0 if successfully added the frame.
| FrameQBufMgr_translateAddr() // instance |
 |
ARGUMENTS
handle
handle of a previously-created FrameQBufMgr instance object
| FrameQBufMgr_unregisterNotifier() // instance |
 |
Function to unregister the registered call back function with the instance.
ARGUMENTS
handle
handle of a previously-created FrameQBufMgr instance object
RETURNS
Returns positive value if successfully unregistered the call back function.
| FrameQBufMgr_writeBack() // instance |
 |
Write back the contents of a frame including frame buffers
ARGUMENTS
handle
handle of a previously-created FrameQBufMgr instance object
| FrameQBufMgr_writeBackFrameBuf() // instance |
 |
Write back the contents of buffer . buffe is treated as frame buffer.
bufNumInFrame denotes buffer number in the frame.This is to identify
the cache flags and cpu access flags for the buffer
Int32 FrameQBufMgr_writeBackFrameBuf(
FrameQBufMgr_Handle handle,
Ptr frameBuf,
UInt32 size,
UInt8 bufNumInFrame);
ARGUMENTS
handle
handle of a previously-created FrameQBufMgr instance object
| FrameQBufMgr_writeBackHeaderBuf() // instance |
 |
Write back the contents of buffer.buffer is treated as frame header
ARGUMENTS
handle
handle of a previously-created FrameQBufMgr instance object
| Instance Convertors |
 |
// unconditionally move one level up the inheritance hierarchy
// conditionally move one level down the inheritance hierarchy; NULL upon failure
| Instance Built-Ins |
 |
Int FrameQBufMgr_Object_count();
// The number of statically-created instance objects
// The handle of the i-th statically-created instance object (array == NULL)
// The handle of the first dynamically-created instance object, or NULL
// The handle of the next dynamically-created instance object, or NULL
// The heap used to allocate dynamically-created instance objects
// The label associated with this instance object
// The name of this instance object
| proxy FrameQBufMgr.GateProxy |
 |
IGateProvider Proxy
| XDCscript usage |
meta-domain |
// explicit access to the currently bound delegate module
FrameQBufMgr.GateProxy.abstractInstances$ = false
// use indirect runtime function calls if true
DETAILS
Module used to provide default critical region management when accessing
the shared memory. The default is
ti.sdo.ipc.gates.GatePeterson.
Requires Arm to be procId 0 or 1 and the DSP be 1 or 0.
| const FrameQBufMgr.DYNAMIC_CREATE |
 |
Type of creation
| XDCscript usage |
meta-domain |
const FrameQBufMgr.DYNAMIC_CREATE = 0x4;
C SYNOPSIS
| const FrameQBufMgr.DYNAMIC_CREATE_USEDREGION |
 |
Type of creation
| XDCscript usage |
meta-domain |
const FrameQBufMgr.DYNAMIC_CREATE_USEDREGION = 0x8;
C SYNOPSIS
| const FrameQBufMgr.DYNAMIC_FRAME |
 |
Denotes Frame belongs to dynamic frame grougp that are added dynamically at runtime
| XDCscript usage |
meta-domain |
const FrameQBufMgr.DYNAMIC_FRAME = 2;
C SYNOPSIS
| const FrameQBufMgr.DYNAMIC_OPEN |
 |
Type of open
| XDCscript usage |
meta-domain |
const FrameQBufMgr.DYNAMIC_OPEN = 0x20;
C SYNOPSIS
| const FrameQBufMgr.FRAMEBUF_CPUACCESSFLAGS_BITOFFSET |
 |
| XDCscript usage |
meta-domain |
const FrameQBufMgr.FRAMEBUF_CPUACCESSFLAGS_BITOFFSET = 16;
C SYNOPSIS
| const FrameQBufMgr.INVALID |
 |
Type of open
| XDCscript usage |
meta-domain |
const FrameQBufMgr.INVALID = 0xFF;
C SYNOPSIS
| const FrameQBufMgr.MAX_FRAMEBUFS |
 |
Maximum number of frame buffers in a frame managed by in
FrameQBufMgr instance
| XDCscript usage |
meta-domain |
const FrameQBufMgr.MAX_FRAMEBUFS = 8;
C SYNOPSIS
| const FrameQBufMgr.MAX_POOLS |
 |
Maximum number of Free Frame pools pools managed by FrameQBufMgr
instance
| XDCscript usage |
meta-domain |
const FrameQBufMgr.MAX_POOLS = 64;
C SYNOPSIS
| const FrameQBufMgr.POOL_DYNAMIC_MAXFRAMES |
 |
Maximum number of dynbuffers managed by each buffer pool in
FrameQBufMgr instance
| XDCscript usage |
meta-domain |
const FrameQBufMgr.POOL_DYNAMIC_MAXFRAMES = 1;
C SYNOPSIS
| const FrameQBufMgr.POOL_DYNAMIC_MAXHDRS |
 |
Maximum number of additional dynamic free headers managed by FrameQBufMgr
instance for each Free Frame pool
| XDCscript usage |
meta-domain |
const FrameQBufMgr.POOL_DYNAMIC_MAXHDRS = 1;
C SYNOPSIS
| const FrameQBufMgr.POOL_MAXFRAMES |
 |
Maximum number of static free Frames managed by FrameQBufMgr
instance for a Free Frame pool
| XDCscript usage |
meta-domain |
const FrameQBufMgr.POOL_MAXFRAMES = 32;
C SYNOPSIS
| const FrameQBufMgr.POOL_MAXHDRS |
 |
Maximum number of additional static free headers managed by FrameQBufMgr
instance for each Free Frame pool
| XDCscript usage |
meta-domain |
const FrameQBufMgr.POOL_MAXHDRS = 64;
C SYNOPSIS
| const FrameQBufMgr.STATIC_CREATE |
 |
Type of creation
| XDCscript usage |
meta-domain |
const FrameQBufMgr.STATIC_CREATE = 0x1;
C SYNOPSIS
| const FrameQBufMgr.STATIC_CREATE_USEDREGION |
 |
Type of creation
| XDCscript usage |
meta-domain |
const FrameQBufMgr.STATIC_CREATE_USEDREGION = 0x2;
C SYNOPSIS
| const FrameQBufMgr.STATIC_FRAME |
 |
Denotes Frame belongs to static frames that are populated at create time of the instance
| XDCscript usage |
meta-domain |
const FrameQBufMgr.STATIC_FRAME = 1;
C SYNOPSIS
| const FrameQBufMgr.STATIC_OPEN |
 |
Type of open
| XDCscript usage |
meta-domain |
const FrameQBufMgr.STATIC_OPEN = 0x10;
C SYNOPSIS
| const FrameQBufMgr.VERSION |
 |
| XDCscript usage |
meta-domain |
const FrameQBufMgr.VERSION = 1;
C SYNOPSIS
| enum FrameQBufMgr.AddrType |
 |
Enumerations to indicate address types used for translation
| XDCscript usage |
meta-domain |
values of type FrameQBufMgr.AddrType
const FrameQBufMgr.AddrType_Virtual;
const FrameQBufMgr.AddrType_Portable;
const FrameQBufMgr.AddrType_EndValue;
VALUES
AddrType_Virtual
Virtual address on calling process on DSP where
MMU is not configured it could be the physical
address.
AddrType_Portable
This is the shared region address incase
sharedmemory manager plugged in to
frameQbufMgr. In case of tiler it could be the
tiler specific portable address
AddrType_EndValue
End delimiter indicating start of invalid
values for this enum
C SYNOPSIS
| enum FrameQBufMgr.BufType |
 |
Enumerations to indicate address types used for translation
| XDCscript usage |
meta-domain |
values of type FrameQBufMgr.BufType
const FrameQBufMgr.BUF_FRAMEHEADER;
const FrameQBufMgr.BUF_FRAMEBUF;
const FrameQBufMgr.BUF_ENDVALUE;
VALUES
BUF_FRAMEHEADER
Denotes buffer is of type used for frame headers.
BUF_FRAMEBUF
Denotes buffer is of type used for frame buffers
AddrType_EndValue
End delimiter indicating start of invalid
values for this enum
C SYNOPSIS
| enum FrameQBufMgr.CpuAccessFlags |
 |
Enumeration of CPU access flags for frame buffers. For frame headers CPUACCESS is assumed to be TRUE
| XDCscript usage |
meta-domain |
values of type FrameQBufMgr.CpuAccessFlags
const FrameQBufMgr.FRAMEBUF0_CPUACCESS;
const FrameQBufMgr.FRAMEBUF1_CPUACCESS;
const FrameQBufMgr.FRAMEBUF2_CPUACCESS;
const FrameQBufMgr.FRAMEBUF3_CPUACCESS;
const FrameQBufMgr.FRAMEBUF4_CPUACCESS;
const FrameQBufMgr.FRAMEBUF5_CPUACCESS;
const FrameQBufMgr.FRAMEBUF6_CPUACCESS;
const FrameQBufMgr.FRAMEBUF7_CPUACCESS;
VALUES
FRAMEBUF0_CPUACCESS
If specified first frame buffer is accessed through CPU(direct memory access).
FRAMEBUF1_CPUACCESS
If specified second frame buffer is accessed through CPU(direct memory access).
FRAMEBUF2_CPUACCESS
If specified third frame buffer is accessed through CPU(direct memory access).
FRAMEBUF3_CPUACCESS
If specified fourth frame buffer is accessed through CPU(direct memory access).
FRAMEBUF4_CPUACCESS
If specified fifth frame buffer is accessed through CPU(direct memory access).
FRAMEBUF5_CPUACCESS
If specified sixth frame buffer is accessed through CPU(direct memory access).
FRAMEBUF6_CPUACCESS
If specified seventh frame buffer is accessed through CPU(direct memory access).
FRAMEBUF7_CPUACCESS
If specified eigth frame buffer is accessed through CPU(direct memory access).
C SYNOPSIS
| enum FrameQBufMgr.Interface |
 |
Enumeration of FrameQBufMgr interface types.Denotes different implementation types
| XDCscript usage |
meta-domain |
values of type FrameQBufMgr.Interface
const FrameQBufMgr.INTERFACE_SHAREDMEM;
const FrameQBufMgr.INTERFACE_TILERMEM;
const FrameQBufMgr.INTERFACE_NONE;
VALUES
INTERFACE_SHAREDMEM
FrameQNufMgr implementation (FrameQBufMgr_ShMem Implementation) on shared memory.
C SYNOPSIS
| struct FrameQBufMgr.Attrs |
 |
Shared control strucrue for the instance attributes
| XDCscript usage |
meta-domain |
var obj = new FrameQBufMgr.Attrs;
obj.status = UInt32 ...
obj.version = UInt32 ...
obj.localProtect = UInt32 ...
obj.remoteProtect = UInt32 ...
obj.gateMPAddr = Ptr ...
obj.sharedDataBufAddr = Ptr ...
obj.sharedAddrSize = UInt32 ...
obj.numFreeFramePools = UInt32 ...
obj.numNotifyEntries = UInt32 ...
obj.entryId = UInt16 ...
FIELDS
status
Flag denoting whether instance is created or not.
version
Version of the instance.
gateMPAddr
GateMP address (shm safe)
name
Name of the instance.
sharedDataBufAddr
Holds Data buffer start address provided at instance crate time.
sharedAddrSize
The size of the data buffer.
FILED
Number of free frame pools maintained by this instance.
Unique id of the instance in the system. Combination of
creator procId and instance no on that processor.
C SYNOPSIS
| struct FrameQBufMgr.CommonOpenParams |
 |
Common paramters requiredto open a FrameQBufMgr instance of any implementation
| XDCscript usage |
meta-domain |
var obj = new FrameQBufMgr.CommonOpenParams;
obj.name = String ...
obj.cpuAccessFlags = UInt32 ...
obj.sharedAddr = Ptr ...
FIELDS
name
Name of the instance to open.
(cacheFlags) Cache flags to perform cache operations .
sharedAddr
Shared addr in case open by address is required.
gate
gate for protection.
C SYNOPSIS
| struct FrameQBufMgr.Config |
 |
mouduleconfig structure
| XDCscript usage |
meta-domain |
var obj = new FrameQBufMgr.Config;
obj.eventNo = UInt32 ...
obj.useNameServer = Bool ...
obj.maxInstances = Bool ...
FIELDS
sharedAddr
Shared region address for module initialization.
sharedAddrSize
Size of the shared region .
(cacheFlags) Cache flags to perform cache operations on module wide shared control structure.
eventNo
The event number used for notification.
name
Name for the module.
shCtrlOpenFlag
Boolean flag if set to FALSE, populate the shared control info
required between processors for this module. If it set to TRUE,
module initialize call opens the shared control info.Ideally master processor
set this flag to FALSE to crate the shared control info.
C SYNOPSIS
| struct FrameQBufMgr.ControlStruct |
 |
Shared control structure for the FrameQBufMgr instance
| XDCscript usage |
meta-domain |
var obj = new FrameQBufMgr.ControlStruct;
FIELDS
attrs
Shared control info of type Attrs.
C SYNOPSIS
| struct FrameQBufMgr.CreateParams |
 |
Structure defining common instance parameters for the FrameQ
module.Should be the first element in the create params strcture of
the actual implementation
| XDCscript usage |
meta-domain |
var obj = new FrameQBufMgr.CreateParams;
obj.size = UInt32 ...
obj.name = String ...
obj.openFlag = Bool ...
FIELDS
size
Size of the Create params structure(Should be the size of the actual
implementation's Create params structure in which this FrameQ_CreateParams is the
first element.
interface
type of implementation. See Interface.
name
Name of the instance.
openFlag
Denotes whether create should actually create/open instance.
C SYNOPSIS
| struct FrameQBufMgr.FrameBufInfo |
 |
Structure of the framebuffer info in frame
| XDCscript usage |
meta-domain |
var obj = new FrameQBufMgr.FrameBufInfo;
obj.bufPtr = UInt32 ...
obj.bufSize = UInt32 ...
obj.startOffset = UInt32 ...
obj.validSize = UInt32 ...
obj.pixelFormat = UInt32 ...
obj.height = UInt32 ...
obj.width = UInt32 ...
obj.stride = UInt32 ...
FIELDS
bufPtr
Pointer to the frame buffer.
bufSize
Size of the buffer.
startOffSet
Start offset in the buffer from where valid data starts.
validSize
Valid size in the buffer from the zeroth offset in the frame buffer.
height
Pointer to the frame buffer.
width
Size of the buffer.
stride
Multiple of page size and needs to be added to Tile
start address in order to get the address starting on
next row in same tile.
C SYNOPSIS
| struct FrameQBufMgr.FrameBufParams |
 |
Structure defining common frame buf params for tiled as well as non tiled buffers
| XDCscript usage |
meta-domain |
var obj = new FrameQBufMgr.FrameBufParams;
obj.size = UInt32 ...
obj.pixelFormat = UInt32 ...
obj.height = UInt32 ...
obj.width = UInt32 ...
obj.align = UInt32 ...
FIELDS
size
size for non tiled buffer.
Structure defining parameters for the Tiled data buffers
pixelFormat
pixel format for tiled buffer.
height
height .
width
width .
stride
stride of container, must be multiple of page size.
align
Alignment of the buffer .
C SYNOPSIS
| struct FrameQBufMgr.FrameHeader |
 |
Structure of the base frame header. FrameQ maintains list of frames to be
retrieved by FrameQ reader client. Application is expected to use Helper
API to extract fileds and exteneded header pointer
| XDCscript usage |
meta-domain |
var obj = new FrameQBufMgr.FrameHeader;
obj.reserved0 = UInt32 ...
obj.reserved1 = UInt32 ...
obj.baseHeaderSize = UInt16 ...
obj.headerSize = UInt16 ...
obj.frmAllocaterId = UInt32 ...
obj.frameBufType = UInt32 ...
obj.freeFrmQueueNo = UInt8 ...
obj.numFrameBuffers = UInt8 ...
FIELDS
baseHeaderSize
Size of the base frame header.
headerSize
Size of the frame header(total size of base header
and extended header).
frmAllocaterId
Denotes the FrameQBufMgr Id from which frame is allocated.
freeFrmQueueNo
Free quque No from which frame is allocated in FrameQBufMgr.
numFrameBuffers
Number of framebuffers in a frame.
C SYNOPSIS
| struct FrameQBufMgr.FreeFramePoolObj |
 |
Free Frame pool structure to keep track of the free frames in a frame pool
| XDCscript usage |
meta-domain |
var obj = new FrameQBufMgr.FreeFramePoolObj;
obj.numFrms = UInt32 ...
obj.freeFrms = UInt32 ...
obj.numFrmHdrBufs = UInt32 ...
obj.freeFrmHdrBufs = UInt32 ...
obj.frmHdrBufSize = UInt32 ...
obj.numBufsInFrame = UInt32 ...
obj.numDynamicHdrBufs = UInt32 ...
obj.freeDynamicHdrBufs = UInt32 ...
obj.numDynamicFrames = UInt32 ...
obj.freeDynamicFrames = UInt32 ...
obj.frmStartAddrp = UInt32 ...
obj.frmEndAddrp = UInt32 ...
obj.hdrBufStartAddrp = UInt32 ...
obj.hdrBufEndAddrp = UInt32 ...
obj.frmBufsStartAddrp = UInt32 ...
obj.frmBufsEndAddrp = UInt32 ...
C SYNOPSIS
| struct FrameQBufMgr.NotifyParams |
 |
Structure defining notification parameter structure
| XDCscript usage |
meta-domain |
var obj = new FrameQBufMgr.NotifyParams;
obj.watermark = UInt32 ...
obj.cbContext = Ptr ...
obj.cbClientHandle = Ptr ...
FIELDS
watermark
Minumum number of free frames required to generate
notification Same water mark for all the individual
freeFramePools in the set.
cbFxnPtr
Cacll back function.
cbContext
Context pointer that needs to be passed to call back
function.
cbClientHandle
Handle that needs to be passed as first arg to
call back.Ideally this should be callers client
handle.
C SYNOPSIS
| struct FrameQBufMgr.ShMem_InstNameServerEntryParams |
 |
Structure defining Additional specific parameters that name server maintains
alonh with the interface type
| XDCscript usage |
meta-domain |
var obj = new FrameQBufMgr.ShMem_InstNameServerEntryParams;
obj.sharedAddr = Ptr ...
obj.sharedAddrSize = UInt32 ...
obj.instGateMPAddr = Ptr ...
obj.frmBuf_regionId = UInt8 ...
obj.hdrBuf_regionId = UInt8 ...
obj.cliGateMPAddr = Ptr ...
FIELDS
sharedAddr
Virtual shared Region Address for control structure.
sharedAddrSize
Size of the shared memory for control structure.
instGateMPAddr
Instance gateMP shared address in
SharedRegion_SRPtr format.Valid only if it
is created internally.
memMgrType_HdrBufs
MemMgr type configured for Header buffers.
memMgrType_FrmBufs
MemMgr type configured for Frame buffers.
allocaterName_HdrBufs
Name of the HeapMemMp instance to be used
Header buffer allocation.
TODO: need to check if it is valid for
Tiler
allocaterName_FrmBufs
Name of the HeapMemMp instance to be used
frame buffer allocation.
TODO: need to check if it is valid for
Tiler
C SYNOPSIS
| config FrameQBufMgr.A_InvalidCreatorProcId // module-wide |
 |
Assert raised when creator processor id of the instance is not valid
| XDCscript usage |
meta-domain |
msg: "A_InvalidCreatorProcId: Invalid creator processor id"
};
C SYNOPSIS
| config FrameQBufMgr.A_InvalidInstNo // module-wide |
 |
Assert raised when Inst No of the instance is not valid
| XDCscript usage |
meta-domain |
msg: "A_InvalidInstNo: Invalid instance no"
};
C SYNOPSIS
| config FrameQBufMgr.A_invalidParams // module-wide |
 |
Assert raised when an invalid parameter(s) is passed into a function
| XDCscript usage |
meta-domain |
msg: "A_invalidParams: Invalid parameter"
};
C SYNOPSIS
| config FrameQBufMgr.A_nullHandle // module-wide |
 |
Assert raised when null handle is returned from modules
| XDCscript usage |
meta-domain |
msg: "A_nullHandle: Null Handle"
};
C SYNOPSIS
| config FrameQBufMgr.A_nullPointer // module-wide |
 |
Assert raised when a null pointer needs to be dereferenced
| XDCscript usage |
meta-domain |
msg: "A_nullPointer: Null pointer"
};
C SYNOPSIS
| config FrameQBufMgr.Attrs_STRUCT_PADDING // module-wide |
 |
Padding required for the Attrs structure
| XDCscript usage |
meta-domain |
C SYNOPSIS
| config FrameQBufMgr.CACHE_LINESIZE // module-wide |
 |
Cache line size
| XDCscript usage |
meta-domain |
FrameQBufMgr.CACHE_LINESIZE = UInt32 128;
C SYNOPSIS
| config FrameQBufMgr.E_CacheAlign // module-wide |
 |
Error raised when buffersize is not aligned to Cache line size
| XDCscript usage |
meta-domain |
msg: "E_CacheAlign: BufferSize is not Cache Aligned"
};
C SYNOPSIS
| config FrameQBufMgr.E_ClientNotifyMgrCreate // module-wide |
 |
Error raised when ClientNotifyMgr Create failed
| XDCscript usage |
meta-domain |
FrameQBufMgr.
E_ClientNotifyMgrCreate =
Error.Desc {
msg: "E_ClientNotifyMgrCreate: ClientNotifyMgr instance Create Failed"
};
C SYNOPSIS
| config FrameQBufMgr.E_ClientNotifyMgrOpen // module-wide |
 |
Error raised when ClientNotifyMgrOpen failed
| XDCscript usage |
meta-domain |
msg: "E_ClientNotifyMgrOpen: ClientNotifyMgrOpen instance Open Failed"
};
C SYNOPSIS
| config FrameQBufMgr.E_FrameQBufMgrCreateFail // module-wide |
 |
Error raised when internal FrameQBufMgr create failed
| XDCscript usage |
meta-domain |
FrameQBufMgr.
E_FrameQBufMgrCreateFail =
Error.Desc {
msg: "E_FrameQBufMgrCreateFail: Internal FrameQBufMgr instance create API failed"
};
C SYNOPSIS
| config FrameQBufMgr.E_FrameQBufMgrNotCreated // module-wide |
 |
Error raised when FrameQBufMgr is not created
| XDCscript usage |
meta-domain |
FrameQBufMgr.
E_FrameQBufMgrNotCreated =
Error.Desc {
msg: "E_FrameQBufMgrNotCreated: FrameQBufMgr instance is not created"
};
C SYNOPSIS
| config FrameQBufMgr.E_FrameQBufMgrNotFound // module-wide |
 |
Error raised when FrameQBufMgr is not Found in NameServer
| XDCscript usage |
meta-domain |
FrameQBufMgr.
E_FrameQBufMgrNotFound =
Error.Desc {
msg: "E_FrameQBufMgrNotFound: FrameQBufMgr instance is not found in NameServer"
};
C SYNOPSIS
| config FrameQBufMgr.E_FrameQBufMgrOpenFail // module-wide |
 |
Error raised when FrameQBufMgr open failed
| XDCscript usage |
meta-domain |
FrameQBufMgr.
E_FrameQBufMgrOpenFail =
Error.Desc {
msg: "E_FrameQBufMgrOpenFail: FrameQBufMgr instance open failed"
};
C SYNOPSIS
| config FrameQBufMgr.E_InstanceExists // module-wide |
 |
Error raised when an instance already exists
| XDCscript usage |
meta-domain |
msg: "E_InstanceExists: Instance already exists"
};
C SYNOPSIS
| config FrameQBufMgr.E_InvAddr // module-wide |
 |
Error raised when Insufficient shared addrprovided to create call
| XDCscript usage |
meta-domain |
msg: "E_InvAddr: Shared Addr provide to create call is NULL"
};
C SYNOPSIS
| config FrameQBufMgr.E_InvSize // module-wide |
 |
Error raised when Insufficient shared memory provided to create call
| XDCscript usage |
meta-domain |
msg: "E_InvSize: SharedMemory provided to create call is less than the instance shared memory requirements"
};
C SYNOPSIS
| config FrameQBufMgr.E_InvalidInterfaceType // module-wide |
 |
Error raised when an invalid interface type mentioned in params
| XDCscript usage |
meta-domain |
FrameQBufMgr.
E_InvalidInterfaceType =
Error.Desc {
msg: "E_InvalidInterfaceType: Invalid interface type"
};
C SYNOPSIS
| config FrameQBufMgr.E_InvalidParams // module-wide |
 |
Error raised when an invalid parameter(s) is passed into a function
| XDCscript usage |
meta-domain |
msg: "E_InvalidParams: Invalid parameter"
};
C SYNOPSIS
| config FrameQBufMgr.E_maxInstances // module-wide |
 |
Error raised when max instances limit is reached
| XDCscript usage |
meta-domain |
msg: "E_maxInstances: max instances limit reached"
};
C SYNOPSIS
| config FrameQBufMgr.MAXINSTANCES // module-wide |
 |
Maximum number of instances that can be created for this module
| XDCscript usage |
meta-domain |
FrameQBufMgr.MAXINSTANCES = UInt32 64;
C SYNOPSIS
| config FrameQBufMgr.MAX_NAMELEN // module-wide |
 |
Maximum length of the name strings
| XDCscript usage |
meta-domain |
FrameQBufMgr.MAX_NAMELEN = UInt32 32;
C SYNOPSIS
| config FrameQBufMgr.NOTIFY_RESERVED_EVENTNO // module-wide |
 |
Event Number to be used by FrameQBufMgr module
| XDCscript usage |
meta-domain |
FrameQBufMgr.NOTIFY_RESERVED_EVENTNO = UInt32 3;
C SYNOPSIS
| config FrameQBufMgr.nameServer // module-wide |
 |
Handle to the name server
| XDCscript usage |
meta-domain |
C SYNOPSIS
| config FrameQBufMgr.usedefaultgate // module-wide |
 |
If set to true FrameQBufMgr instances will use dafault gate set in
FrameQBufMgr.
If default gate is not set in FrameQBufMgr, it uses GateMP's default
gate. Set it to zero if FrameQBufMgr needs to create gate for a
instance (remoteProtect and localProtect flags should be valid in
params in this case)
| XDCscript usage |
meta-domain |
FrameQBufMgr.usedefaultgate = Bool false;
C SYNOPSIS
| metaonly config FrameQBufMgr.common$ // module-wide |
 |
Common module configuration parameters
| XDCscript usage |
meta-domain |
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
| metaonly config FrameQBufMgr.maxRuntimeEntries // module-wide |
 |
Maximum number of FrameQBUfMgr's that can be dynamically created
and added to the NameServer
| XDCscript usage |
meta-domain |
| metaonly config FrameQBufMgr.nameSrvPrms // module-wide |
 |
This Params object is used for temporary storage of the
module wide parameters that are for setting the NameServer instance
| XDCscript usage |
meta-domain |
| metaonly config FrameQBufMgr.tableSection // module-wide |
 |
Section name is used to place the names table
| XDCscript usage |
meta-domain |
FrameQBufMgr.tableSection = String null;
| metaonly config FrameQBufMgr.useNameServer // module-wide |
 |
Whether to have this module use the NameServer or not
| XDCscript usage |
meta-domain |
FrameQBufMgr.useNameServer = Bool true;
DETAILS
Currently defaulted to false because static creation of NameServer
instances is not supported.
| Instance Config Parameters |
 |
| XDCscript usage |
meta-domain |
var params = new FrameQBufMgr.Params;
// Instance config-params object
//
size: 0,
name: null,
openFlag: false
};
params.impParams = Ptr null;
// Pointer to implementation specific parameters
params.impParamsSize = UInt32 0;
// Pointer to implementation specific parameters
| config FrameQBufMgr.commonCreateParams // instance |
 |
| XDCscript usage |
meta-domain |
var params = new FrameQBufMgr.Params;
...
size: 0,
name: null,
openFlag: false
};
C SYNOPSIS
| config FrameQBufMgr.impParams // instance |
 |
Pointer to implementation specific parameters
| XDCscript usage |
meta-domain |
var params = new FrameQBufMgr.Params;
...
params.impParams = Ptr null;
C SYNOPSIS
| config FrameQBufMgr.impParamsSize // instance |
 |
Pointer to implementation specific parameters
| XDCscript usage |
meta-domain |
var params = new FrameQBufMgr.Params;
...
params.impParamsSize = UInt32 0;
C SYNOPSIS