SYS/Link Software Manifest


Legend

Package Name

The name of the application or files

Version

Version of the application or files

License

Name of the license or licenses that apply to the Package.

Location

The directory name and path on the media (or in an archive) where the Package is located. The location is the top-level directory for the package and is relative to the base installation directory for SYS/Link.

Delivered As

This field will either be “Source”, “Binary” or “Source and Binary” and is the form the content of the Package is delivered in.  If the Package is delivered in an archive format, this field applies to the contents of the archive. If the word Limited is used with Source, as in “Limited Source” or “Limited Source and Binary” then only portions of the Source for the application are provided.

Modified

This field will either be “Yes” or “No”. A “Yes” means TI had made changes to the Package. A “No” means TI has not made any changes.

Obtained from[1]

This field specifies where TI obtained the Package from. It may be a URL to an Open Source site, a 3rd party company name or TI. If this field contains a link to an Open Source package, the date it was downloaded is also recorded.

  

Manifest

Note: Replace MM.mm.pp.bb in the directory path below with the SYS/Link release version you are using.

Package Name

Version

License

Delivered As

Modified

 

SYS/Link  

MM.mm.pp.bb

New BSD

Source

No

Location

Source at: syslink_MM.mm.pp.bb_<ReleaseQualifier>.tar.gz

Obtained from[1]

TI

 


[1] Any links appearing on this manifest were verified at the time it was created. TI makes no guarantee that they will remain active in the future.