C64X+ Watchdog Interface
========================

The supported C64X+ SOCs use the same watchdog hardware as does the ARM-based
Davinci processors (davinci_wdt). This is a bare bones watchdog driver which
provides a /dev/watchdog device. The watchdog timer is initially disabled after
reset and boot. To load the watchdog driver:

  % modprobe davinci_wdt

The default expiry time of 60 seconds can be modified with the "heartbeat"
option when loading the module. For example, you can achieve a ten second
expriry time with:

  % modprobe davinci_wdt heartbeat=10

Loading the driver does not start the watchdog. To do that, you must open the
device file (/dev/watchdog). To reset the watchdog timer counter in order to
prevent it from expiring,for keepalive one must write to the device file. For
instance:

  % echo >/dev/watchdog

will reset the watchdog counter (and activate it if it was not already started).

On TMS320C6455 based boards, external circuitry is needed to respond to the
watchdog output signal. The default response to a watchdog expiration on other
SOCs is to do nothing. These other SOCs may be configured to take other actions
based on a kernel cmdline parameter:

      wdt_action=<local|nmi|delay,NNN|system>
       where:
           local     => perform megamodule reset
           nmi       => perform an NMI
           delay,NNN => nmi followed by delayed local reset
                        NNN is number of CPU/6 clocks to delay
           system    => system reset

The "nmi", "delay", and "system" options are only available on the TMS320C6472.

Board-specific code may provide an NMI handler by setting mach_nmi_handler to
the address of the handler. This should be done in c6x_board_setup_arch() which
if after mach_nmi_handler is set to the default handler. The handler prototype
is:

   extern void (*mach_nmi_handler)(struct pt_regs *regs);