C64X+ EDMA3 Interface
========================

This document describes the kernel interface to the EDMA3 controller. For
details on the actual operation of EDMA3, see the appropriate hardware manual.


Platform Device Interface
=========================

The EDMA driver requires a platform_device structure to describe details of its
configuration:

static struct platform_device edma_device = {
	.name			= "edma",
	.id			= 0,
	.dev.platform_data	= edma_info,
	.num_resources		= ARRAY_SIZE(edma_resources),
	.resource		= edma_resources,
};

The platform_data is an array (one per EDMA controller) of EDMA information
used to configure the EDMA controller:

static struct edma_soc_info edma_cc0_info = {
	.n_channel		= EDMA_NUM_DMACH,
	.n_region		= EDMA_NUM_REGIONS,
	.n_slot			= EDMA_NUM_PARAMENTRY,
	.n_tc			= EDMA_NUM_EVQUE,
	.n_cc			= 1,
	.queue_tc_mapping	= queue_tc_mapping,
	.queue_priority_mapping	= queue_priority_mapping,
};

static struct edma_soc_info *edma_info[] = {
	&edma_cc0_info,
};

The edma_soc_info struct provides the number of channels, regions, param slots,
and event queues available on the controller. Also, queue -> transfer controller
mapping and queue priority are provided.

The EDMA3 controller has a limited number of channels which may be shared with
other processors on the SoC. Furthermore, various SoC events may be used to
trigger DMA operations, but these events are assigned to specific channels. If
a specific driver needs to use specific DMA channels, those channels must be
reserved. This is done through the device driver resource list. For example:

static struct resource evm6474_rio_resources[] = {
	{
		.name	= "LSU",
		.start	= DMA_CIC_EVT6,
		.flags	= IORESOURCE_DMA,
	},
	{
		.name	= "ICCR",
		.start	= DMA_CIC_EVT5,
		.flags	= IORESOURCE_DMA,
	},
	{
		.name	= "RATE",
		.start	= DMA_CIC_EVT7,
		.flags	= IORESOURCE_DMA,
	},
};

static struct platform_device evm6474_rio_device = {
	.resource	= evm6474_rio_resources,
};

The above ensures that DMA channels for the given events will not be dynamically
assigned so that they will be available for the RIO driver.


API
===

------------------------------------------------------------------------------
int edma_alloc_channel(int channel,
		void (*callback)(unsigned channel, u16 ch_status, void *data),
		void *data,
		enum dma_event_q eventq_no)

 Allocate DMA channel and paired parameter RAM

    @channel: specific channel to allocate; negative for "any unmapped channel"
    @callback: optional; to be called on DMA completion or errors
    @data: passed to callback
    @eventq_no: an EVENTQ_* constant, used to choose which Transfer
	       Controller (TC) executes requests using this channel.  Use
	       EVENTQ_DEFAULT unless you really need a high priority queue.

This allocates a DMA channel and its associated parameter RAM slot.
The parameter RAM is initialized to hold a dummy transfer.

Normal use is to pass a specific channel number as @channel, to make
use of hardware events mapped to that channel.  When the channel will
be used only for software triggering or event chaining, channels not
mapped to hardware events (or mapped to unused events) are preferable.

DMA transfers start from a channel using edma_start(), or by
chaining.  When the transfer described in that channel's parameter RAM
slot completes, that slot's data may be reloaded through a link.

DMA errors are only reported to the @callback associated with the
channel driving that transfer, but transfer completion callbacks can
be sent to another channel under control of the TCC field in
the option word of the transfer's parameter RAM set.  Drivers must not
use DMA transfer completion callbacks for channels they did not allocate.
(The same applies to TCC codes used in transfer chaining.)

Returns an integer 'handle' for the channel which is used in further API
calls. If negative, the returned handle is an errno.


------------------------------------------------------------------------------
void edma_free_channel(unsigned channel)

 Deallocate DMA channel

    @channel: dma channel returned from edma_alloc_channel()

This deallocates the DMA channel and associated parameter RAM slot
allocated by edma_alloc_channel().

Callers are responsible for ensuring the channel is inactive, and
will not be reactivated by linking, chaining, or software calls to
edma_start().


------------------------------------------------------------------------------
int edma_alloc_slot(unsigned ctlr, int slot)

 Allocate DMA parameter RAM

     @slot: specific slot to allocate; negative for "any unused slot"

This allocates a parameter RAM slot, initializing it to hold a
dummy transfer.  Slots allocated using this routine have not been
mapped to a hardware DMA channel, and will normally be used by
linking to them from a slot associated with a DMA channel.

Normal use is to pass EDMA_SLOT_ANY as the @slot, but specific
slots may be allocated on behalf of DSP firmware.

Returns the number of the slot, else negative errno.


------------------------------------------------------------------------------
void edma_free_slot(unsigned slot)

 Deallocate DMA parameter RAM

    @slot: parameter RAM slot returned from edma_alloc_slot()

This deallocates the parameter RAM slot allocated by edma_alloc_slot().
Callers are responsible for ensuring the slot is inactive, and will
not be activated.


------------------------------------------------------------------------------
int edma_alloc_cont_slots(unsigned ctlr, unsigned int id, int slot, int count)

 Alloc contiguous parameter RAM slots
 The API will return the starting point of a set of
 contiguous parameter RAM slots that have been requested

    @id: can only be EDMA_CONT_PARAMS_ANY or EDMA_CONT_PARAMS_FIXED_EXACT
         or EDMA_CONT_PARAMS_FIXED_NOT_EXACT
    @count: number of contiguous Paramter RAM slots
    @slot: the start value of Parameter RAM slot that should be passed if id
           is EDMA_CONT_PARAMS_FIXED_EXACT or EDMA_CONT_PARAMS_FIXED_NOT_EXACT

If id is EDMA_CONT_PARAMS_ANY then the API starts looking for a set of
contiguous Parameter RAM slots from parameter RAM 64 in the case of
DaVinci SOCs and 32 in the case of DA8xx SOCs.

If id is EDMA_CONT_PARAMS_FIXED_EXACT then the API starts looking for a
set of contiguous parameter RAM slots from the "slot" that is passed as an
argument to the API.

If id is EDMA_CONT_PARAMS_FIXED_NOT_EXACT then the API initially tries
starts looking for a set of contiguous parameter RAMs from the "slot"
that is passed as an argument to the API. On failure the API will try to
find a set of contiguous Parameter RAM slots from the remaining Parameter
RAM slots


------------------------------------------------------------------------------
int edma_free_cont_slots(unsigned slot, int count)

 Deallocate DMA parameter RAM slots

    @slot: first parameter RAM of a set of parameter RAM slots to be freed
    @count: the number of contiguous parameter RAM slots to be freed

This deallocates the parameter RAM slots allocated by edma_alloc_cont_slots.
Callers/applications need to keep track of sets of contiguous parameter RAM
slots that have been allocated using the edma_alloc_cont_slots API.
Callers are responsible for ensuring the slots are inactive, and will not be
activated.


------------------------------------------------------------------------------
void edma_set_src(unsigned slot, dma_addr_t src_port,
				enum address_mode mode, enum fifo_width width)

 Set initial DMA source address in parameter RAM slot

    @slot: parameter RAM slot being configured
    @src_port: physical address of source (memory, controller FIFO, etc)
    @addressMode: INCR, except in very rare cases
    @fifoWidth: ignored unless @addressMode is FIFO, else specifies the
	        width to use when addressing the fifo (e.g. W8BIT, W32BIT)

Note that the source address is modified during the DMA transfer according to
edma_set_src_index().


------------------------------------------------------------------------------
void edma_set_dest(unsigned slot, dma_addr_t dest_port,
				 enum address_mode mode, enum fifo_width width)

 Set initial DMA destination address in parameter RAM slot

    @slot: parameter RAM slot being configured
    @dest_port: physical address of destination (memory, controller FIFO, etc)
    @addressMode: INCR, except in very rare cases
    @fifoWidth: ignored unless @addressMode is FIFO, else specifies the
                width to use when addressing the fifo (e.g. W8BIT, W32BIT)

Note that the destination address is modified during the DMA transfer according
to edma_set_dest_index().


------------------------------------------------------------------------------
void edma_get_position(unsigned slot, dma_addr_t *src, dma_addr_t *dst)

 Returns the current transfer points

    @slot: parameter RAM slot being examined
    @src: pointer to source port position
    @dst: pointer to destination port position

Returns current source and destination addresses for a particular parameter
RAM slot.  Its channel should not be active when this is called.


------------------------------------------------------------------------------
void edma_set_src_index(unsigned slot, s16 src_bidx, s16 src_cidx)

 Configure DMA source address indexing

    @slot: parameter RAM slot being configured
    @src_bidx: byte offset between source arrays in a frame
    @src_cidx: byte offset between source frames in a block

Offsets are specified to support either contiguous or discontiguous memory
transfers, or repeated access to a hardware register, as needed. When accessing
hardware registers, both offsets are normally zero.


------------------------------------------------------------------------------
void edma_set_dest_index(unsigned slot, s16 dest_bidx, s16 dest_cidx)

 Configure DMA destination address indexing

    @slot: parameter RAM slot being configured
    @dest_bidx: byte offset between destination arrays in a frame
    @dest_cidx: byte offset between destination frames in a block

Offsets are specified to support either contiguous or discontiguous memory
transfers, or repeated access to a hardware register, as needed. When accessing
hardware registers, both offsets are normally zero.


------------------------------------------------------------------------------
void edma_set_transfer_params(unsigned slot,
		u16 acnt, u16 bcnt, u16 ccnt,
		u16 bcnt_rld, enum sync_dimension sync_mode)

 Configure DMA transfer parameters

    @slot: parameter RAM slot being configured
    @acnt: how many bytes per array (at least one)
    @bcnt: how many arrays per frame (at least one)
    @ccnt: how many frames per block (at least one)
    @bcnt_rld: used only for A-Synchronized transfers; this specifies
               the value to reload into bcnt when it decrements to zero
    @sync_mode: ASYNC or ABSYNC

See the EDMA3 documentation to understand how to configure and link transfers
using the fields in PaRAM slots.  If you are not doing it all at once with
edma_write_slot(), you will use this routine plus two calls each for source
and destination, setting the initial address and saying how to index that
address.

An example of an A-Synchronized transfer is a serial link using a single word
shift register.  In that case, @acnt would be equal to that word size; the
serial controller issues a DMA synchronization event to transfer each word,
and memory access by the DMA transfer controller will be word-at-a-time.

An example of an AB-Synchronized transfer is a device using a FIFO. In that
case, @acnt equals the FIFO width and @bcnt equals its depth. The controller
with the FIFO issues DMA synchronization events when the FIFO threshold is
reached, and the DMA transfer controller will transfer one frame to (or from)
the FIFO.  It will probably use efficient burst modes to access memory.


------------------------------------------------------------------------------
void edma_link(unsigned from, unsigned to)

 Link one parameter RAM slot to another

    @from: parameter RAM slot originating the link
    @to: parameter RAM slot which is the link target

The originating slot should not be part of any active DMA transfer.


------------------------------------------------------------------------------
void edma_unlink(unsigned from)

 Cut link from one parameter RAM slot to another

    @from: parameter RAM slot originating the link

The originating slot should not be part of any active DMA transfer. Its link is
set to 0xffff.


------------------------------------------------------------------------------
void edma_chain(unsigned from, unsigned to)

 Chain one parameter RAM slot to another

    @from: channel originating the link
    @to: channel which is the link target

The originating channel should not be part of any active DMA transfer.


------------------------------------------------------------------------------
void edma_unchain(unsigned from)

 Unchain one channel from another

    @from: channel slot originating the chain

The originating slot should not be part of any active DMA transfer.


------------------------------------------------------------------------------
void edma_write_slot(unsigned slot, const struct edmacc_param *param)

 Write parameter RAM data for slot

    @slot: number of parameter RAM slot being modified
    @param: data to be written into parameter RAM slot

Use this to assign all parameters of a transfer at once.  This allows more
efficient setup of transfers than issuing multiple calls to set up those
parameters in small pieces, and provides complete control over all transfer
options.



------------------------------------------------------------------------------
void edma_read_slot(unsigned slot, struct edmacc_param *param)

 Read parameter RAM data from slot

    @slot: number of parameter RAM slot being copied
    @param: where to store copy of parameter RAM data

Use this to read data from a parameter RAM slot, perhaps to save them as a
template for later reuse.


------------------------------------------------------------------------------
void edma_pause(unsigned channel)

 Pause dma on a channel

    @channel: on which edma_start() has been called

This temporarily disables EDMA hardware events on the specified channel,
preventing them from triggering new transfers on its behalf


------------------------------------------------------------------------------
void edma_resume(unsigned channel)

 Resumes dma on a paused channel

    @channel: on which edma_pause() has been called

This re-enables EDMA hardware events on the specified channel.


------------------------------------------------------------------------------
int edma_start(unsigned channel)

 Start dma on a channel

    @channel: channel being activated

Channels with event associations will be triggered by their hardware events, and
channels without such associations will be triggered by software.

Returns zero on success, else negative errno.


------------------------------------------------------------------------------
void edma_stop(unsigned channel)

 Stops dma on the channel passed

    @channel: channel being deactivated

Any active transfer is paused and all pending hardware events are cleared. The
current transfer may not be resumed, and the channel's Parameter RAM should be
reinitialized before being reused.